Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pail

Pail
Sales Price: -
Review Rating: 4.62
8 Customer Reviews
5 star 6
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
For filtering waste oil
4
From Japan
On 2015-05-02 11:00:16
It is used for filtration of waste oil, it is easy to use a filter paper tightly caught.
This review is about item#77657063.
Subdivision of emulsion for pavement work
5
From Japan
On 2015-04-25 17:35:03
We are very satisfied with our first transaction, we have made it quickly and reliably. Regardless of the order item we are satisfied. If it can do, I am looking forward to the e-mail of products related to our company.
This review is about item#77657063.
For bamboo oil drainage, boiled the water outdoors with fire.
5
From Japan
On 2014-12-28 23:50:32
It was a solid build and just good size, it was very easy to use. Equivalent, I put on fire until it got hot, but there was no pain. As original use, even when using lid as a sealing air, packing is attached to the lid and sealability is outstanding. I think that if the price is a bit cheaper, I think that there is no choice but for this price as goods are solid.
This review is about item#77657063.
It is optimum for temporary storage of "Ceramic Sanohwa Ceramic Stove SG-4" for windbreak hoods.
5
From Japan
On 2014-12-17 20:37:14
I bought two pail cans. One is putting "Sanwa metal ceramic briquetting stove stove SG - 4" in this pail can. I think that it is the size suitable for this stove's hood. You can also use the Sanwa ceramic briquette stove more safely because the firepower can be stabilized and the guard can also be done. I think that the combustion efficiency also increases with the hood effect. I used a jacquard, pot, Dutch oven on the ring of the lid with a wire mesh of 30 cm in outer diameter. This is very convenient. In the other hand, ash of briquettes is processed in a fire pot and it is put out for collection of predetermined garbage, but it is used for temporary storage until then. Ash of briquettes is bulky so I think that a pail can of this size is just right. Cans, lids and rings are both good, inexpensive and thankfully used. For your information, please.
This review is about item#77657063.
Miscellaneous goods storage
5
From Japan
On 2014-09-10 13:21:23
I bought it referring to the review that the lid is good. It is so stiff that my child's mischief can be prevented. I only want a lid.
This review is about item#77657063.
It is convenient when there is no water supply facility when using the exterior construction
5
From Japan
On 2014-08-15 13:20:07
Since it was a place where there was no water supply used for installing the fence, it was handy when carrying water and carrying it
This review is about item#77657063.
Smoked
5
From Japan
On 2014-05-21 07:31:21
The price was cheap but the making was solid, making the lid was particularly good. I bought it at a cheaper price than I bought at a home center. Thank you
This review is about item#77657063.
To discard the fabric wiped with organic solvent.
3
From Japan
On 2013-11-05 13:42:10
I am glad that the lid is solid. I think that it was still better if there was a little smaller size.
This review is about item#77657063.
1
Customer Who Viewed This Item Also Viewed
Pail
Sealed Tank, Hanging Type
Sample
Individual Pail Cans 18L
Steel 20L Open Pail Can
Lid for sample
Empty Square Cans