Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Small Round Window

Small Round Window
Sales Price: 4.99 SGD
Review Rating: 4.00
12 Customer Reviews
5 star 6
4 star 2
3 star 2
2 star 2
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Attach to existing indoor door
2
From Japan
On 2017-12-18 23:17:12
Although the thickness of the door panel is up to 40 mm, On the design, there is also a thin part, it becomes about 20 mm. Then it becomes thick with this thickness, so it was cut and used. I also want you to make things that are thin.
This review is about item#9412453.
Light of the toilet
5
From Japan
On 2017-09-29 21:19:16
Because the toilet's electricity was on I attached it.
This review is about item#9412453.
Taking a light for a door
5
From Japan
On 2017-03-16 23:37:14
I installed it in the washroom door I forgot to turn off the fluorescent light
This review is about item#9412462.
To check the door light of the toilet
5
From Japan
On 2017-03-10 11:26:06
I was worried because the thickness of the door was thin and it was full of the lower limit of the thickness range of the product, but it works well. It seems that many of the old building doors are thin, it seems that thin items are required for the lower limit side about 5 mm.
This review is about item#9412453.
Harassment
5
From Japan
On 2017-02-24 15:13:15
The toilet tradition has never been lost, and Mr. Kami's words have been reduced by one. Good!
This review is about item#9412462.
The door of the toilet.
5
From Japan
On 2016-06-10 23:37:54
As a matter of fact, attaching this makes me forget to turn off the lights. As a disadvantage, of course, it seems that everything looks like a toilet door. (It is good to make it as a thing.) I think that it was good to install.
This review is about item#09412453.
Attach to toilet and washroom door
2
From Japan
On 2016-03-25 17:01:32
It was not possible to use because the minimum thickness of the product is 22 cm or more because it will be installed where the door thickness is only 1 cm. We cut the thickness of the product and modified it to less than 1 cm and installed it. I would like a product that can be attached even 1CM if possible.
This review is about item#09412487.
Preventing the forgetting to turn off lights in the basement
3
From Japan
On 2015-12-25 20:34:22
I will not be able to check chops
This review is about item#09412462.
Lighting in the toilet
3
From Japan
On 2015-12-22 14:51:28
I used it as a light in the door of the toilet. Product was not particularly problematic, but there is dissatisfaction with shipping. Purchase on the same day thankful that shipping fee, cash on delivery etc will be free, but because it became a separate packing, because it became a separate shipment, although the time also does not change very much, only the addition order of the same day arrived two days later. It did not work for only one part waiting · · ·. Why did you order the same item on the same day with a little time difference, so that delivery will be delayed by two days? Is it? Is it? Moreover, the shipping date is the same. It is no wonder.
This review is about item#09412444.
Attached to the wooden door of the internal toilet.
4
From Japan
On 2014-11-18 09:23:54
Because it is small, it will be light if it is a daylight white LED by all means, but weak enough it is enough because it is showing its function. If I can change the LED bulb to warm color I will try it next time. Because the hole saw of 24 to 25 mm is high, though it thought to draw an arc with a thin drill, it is troublesome, so if you do with a 29 mm hole saw of Daiso, if you tighten loosely, a gap can be formed about 1 mm about the top, but tightly fastened and fixed If possible, the gap will be gone. Or if you adjust the hole size by winding it on the main body with tape, more precision will rise. It is OK because it is not a wonderful gate so that we can get nearly 2000 yen at the hole saw.
This review is about item#09412444.
Light of the toilet
5
From Japan
On 2014-09-29 16:05:35
It is satisfactory enough.
This review is about item#09412453.
Light toilet lighting
4
From Japan
On 2013-02-22 21:38:06
Because there is a ring part made of all transparent material, I want you to handle such items as well (the visibility of the light is quite different). Cospa at DIY is good. Just drilling at 24 mm, we recommend drilling with 25 mm in margin, as the hole part is not closely attached to the flat surface even if even a little hole is distorted.
This review is about item#09412487.
1
Customer Who Viewed This Item Also Viewed
Digital Thermo-Hygrometer
BP12-E meter reading window
Small Round Window
Brightness for door
Picking up lights
Safety check Akarimado