Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of TW Plastic Case

TW Plastic Case
Sales Price: 2.99 SGD
Review Rating: 4.55
20 Customer Reviews
5 star 15
4 star 3
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 20 of 20 Reviews
Transmitter enclosure
5
From Japan
On 2018-05-25 16:27:22
It was just right size and it was very good. I would like a screw to fix the board etc. is also included, if possible.
This review is about item#88209633.
Self-made passive for car · audio passive · crossover · for network storage
5
From Japan
On 2018-05-03 17:23:26
Truly [Takachi] products, products can put confidence in the whole width. 350 Hz Cross Network Film · Con about 105 μF / 2.0 mH Because both pod cores and coils are large, they were all intriguingly intriguing but all parts fitted safely in the case. It is a purchase for the purpose of accommodating them, so it is appreciated that various sizes are finely available.
This review is about item#88209755.
As a case of electronic parts
4
From Japan
On 2018-04-26 14:28:43
Easy to process, you could do a hole drill freely with a hand drill or reamer. About 10 9V batteries were stored and used as a simple power supply.
This review is about item#88209886.
DC power supply for wireless receiver
5
From Japan
On 2018-04-08 14:39:46
I always patronize. I like it because it has good workability and less deformation.
This review is about item#88209791.
Weak electric printed circuit board and various parts for incorporation
5
From Japan
On 2018-03-19 21:23:33
Even if plug terminals etc. are attached and detached, they have sufficient strength, also easy to drilling, convenient and handy.
This review is about item#88209886.
Implementation of electronic equipment
5
From Japan
On 2018-01-30 18:18:46
The variety is also abundant and convenient. It is also easy to use with strength. It is easy to process.
This review is about item#88209764.
Hobby's electronic work
5
From Japan
On 2017-12-17 15:21:30
I can not see the universal board of soldered solder if it is put in the box!
This review is about item#88209834.
Base placement
5
From Japan
On 2017-08-31 14:37:00
It is used to produce a switch for relaying the connection cable of the tester. It is good to be able to choose a size that fits just small. Because it is inexpensive and has versatility, its use range is large depending on the size.
This review is about item#88209773.
Electronic circuit
5
From Japan
On 2017-08-19 21:50:44
Very easy to use, I am satisfied with buying. I also want to purchase.
This review is about item#88209852.
Prototype sensor P plate casing
4
From Japan
On 2017-05-29 02:59:31
There should be a type that is not a screw for tightening the lid
This review is about item#88209834.
We are planning to have switches and controllers
5
From Japan
On 2017-05-25 09:21:41
It is cheap and good. The texture of the case itself is not too bad. The speed controller of AC motor is scheduled to be built.
This review is about item#88209764.
Insertion of electronic circuit
5
From Japan
On 2017-05-23 14:58:18
It was just right size. After closing the lid it needed confidentiality and under was enough.
This review is about item#88209992.
Used to incorporate dimmer module
4
From Japan
On 2017-04-06 18:15:44
It was easy to process because it was plastic, but since the post for screwing the bottom plate is standing in the interior, the usable width is smaller than the apparent width, and since the dimming knob is attached to the shorter side, the board strikes the column and positions it It was difficult. Because the design is trapezoidal, since the side faces are diagonal, the way of using it as a built-in case of equipment is just the place where the appearance is now.
This review is about item#88209755.
Work
5
From Japan
On 2016-12-16 14:52:05
It is satisfying with this convenience, this quality, convenient size.
This review is about item#88209536.
Used as personal computer controller BOX of personal computer
5
From Japan
On 2016-08-17 18:04:35
Both size, ease of handling and weight are satisfied.
This review is about item#88209956.
Incorporating the base to connect the wires
5
From Japan
On 2016-06-23 17:49:27
It can be installed in a narrow place. Drilling is also easy with Holso. I will come in handy.
This review is about item#88209922.
IC circuit case
5
From Japan
On 2016-06-16 19:33:35
It is easy to process and just right size.
This review is about item#88209633.
It was used for red guiding.
5
From Japan
On 2016-02-23 18:54:27
There is neither possible nor impossible.
This review is about item#88209746.
Small electronic circuit
1
From Japan
On 2016-02-14 16:14:43
The evaluation is bad, although a gray color was ordered, a black object arrived. Will Mon Tarou grow up when it grows bigger? I thought.
This review is about item#88209755.
In a case of a little electronic work
3
From Japan
On 2014-10-10 19:37:39
Because it is an ABS resin close to raw (almost no modifier is contained), it is soft and vulnerable to heat. Just touch the soldering iron just to melt it. A boss stands for the screw fixing of the lid quite inside. When you want to put the circuit board etc at the last minute, there is only to remove the boss. I will think of another way to fix the lid. Care is required when using the inner side because the taper that becomes narrower becomes the bottom (the side is not vertical).
This review is about item#88209633.
1 2
Customer Who Viewed This Item Also Viewed
SW Plastic Case
Plamoul Accesories, Bent
Molded Case TB
PF type panel plastic case
LC-type hand type plastic case
SW-N Plastic Case
PR-type top cover desorption plastic box
SB-type plastic case
TWF type flange foot with flame-retardant plastic case
SY-type plastic case
SW-T flame-retardant plastic case
TWN Plastic Case
MB type aluminum case
Molded Box TB-30 Series
Molded Case TB-50