Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Commercial water-saving shower chestnut shower SW swing type

Commercial water-saving shower chestnut shower SW swing type
Sales Price: -
Review Rating: 4.40
5 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Replacement due to damage to the shower head
5
From Japan
On 2017-04-05 14:51:48
Anyhow the head was big and I was surprised. Even when washing the dishes, you can pour them all at once with a big shower. It seems that there is considerable water-saving effect and I am looking forward to it. Water-saving pieces were also attached, but there seems to be enough water saving effect even without it (package reference). There is no stress in use. Dare to say that the switching button of the shower does not move with one hand (because the body also turns sideways unless you hold down the main body) was a little marginal.
This review is about item#88830235.
Kitchen sink
3
From Japan
On 2016-11-29 16:14:12
It is very good as a water-saving shower, so it's good to have good water well. However, since the length of the swinging portion was 5.5 cm, I was not thinking about the height of the faucet, so the distance to the sink got closer and it was better for a slightly smaller size.
This review is about item#88830235.
kitchen
5
From Japan
On 2015-09-03 15:27:27
I think that it will be easy to use and save water
This review is about item#88830235.
Commercial kitchen
4
From Japan
On 2015-03-02 09:44:18
It is much bigger than the shower of the retrofit type for home use, easy to switch and easy to use. It is very different without attaching. I was a little puzzled because various parts were included.
This review is about item#88830235.
Wash dishes and pots in the kitchen
5
From Japan
On 2014-11-08 22:43:48
It was easy to set and we did not need much power, and I could easily install it even if I was a machine tone. It is satisfied to save water without leakage from the installation part. I was worried about whether the type of faucet would fit, but since I sold a faucet of the same type as the house on the same site, I could confirm and purchase with confidence. The neck pretense can also be 360 ​​° C in parallel, it can be turned by 360 ° C and it can also be turned 360 ° C so it is saved by washing the large pan even in a narrow washing space.
This review is about item#88830235.
1
Customer Who Viewed This Item Also Viewed
Switching Shower
Flow switching shower
G Type Rotary Shower Head 13
Swinging Kitchen Shower
Neck pretend kitchen shower
Kitchen shower
Sewing sink with original port
Kitchen shower
Kitchen Spray
Switching Shower
Rotary Shower
Shower Head for Sink