Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Chain Detacher

Chain Detacher
Sales Price: 61.99 SGD
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Repair shutter roller chain
5
From Japan
On 2016-10-01 16:30:38
It is very useful for replacing the roller chain, which is used for a general over-slider.
This review is about item#88475396.
Conveyor and stacker crane
5
From Japan
On 2015-06-17 14:22:25
It is compact, light and easy to use. You can use it even in narrow places. Is the pin easy to break, so is there a spare pin?
This review is about item#88475396.
Equipment Maintenance
4
From Japan
On 2015-02-16 00:10:54
Although there are opinions of some that it is hard to use, there is also opinion of equipment related work but it is an opinion from the experience but it is not saying that it is a good evaluation even if a good tool also has a habit It is also a habit and it pulls out the chain Sometimes it is difficult to correct the center while hitting it to the center, unlike writing it would have to do a few things. When turning, the force will be affected by the rotation direction and it will be misaligned. Personally I think that a simple structure is good.
This review is about item#88475396.
1
Customer Who Viewed This Item Also Viewed
Chain Cutter
Chain Rivet Extractor
For One Column Ck Type Chain Cutter
Chain Cutter CK Type, 2 Column
Chain Cutter Two Lines
Chain Cutter Set
Chain Cutter Set
Cutter Pin for CK Type
Chain Breaker
Single Row Spare Pin
Roller Chain Link
Chain Puller
Chain Pliers
Chain Cutters & Liberator
Chain Puller
Straight punch chain cutter
Chain Tool