Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Oil Pail

Oil Pail
Sales Price: 2.99 SGD
Review Rating: 3.71
17 Customer Reviews
5 star 4
4 star 7
3 star 4
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 17 of 17 Reviews
For dividing and mixing of water paint class
4
From Japan
On 2018-05-12 14:43:45
I think that the thickness of the upper lid is a bit weak and it hangs and it gets crooked like this
This review is about item#723948.
Excess paint storage after car paint toning
2
From Japan
On 2018-01-15 13:51:42
Even if minor toning is done, automobile repair paint always remains, so far it was stored in a plastic container, but because it solidifies inside and it is not suitable for long-term preservation, we purchase a metal made here did. Although it is excellent with respect to preservation, it is deformed just by opening the lid with poor cover. Although it is fine if it is used up at one time, since it is also used with a stroke, the degree of hermeticity is lowered while opening and closing it many times. Since 1 liter type lid is also sturdy it can be opened and closed many times. I do not want to raise the strength (especially the edge part) of the lid because the price may be higher.
This review is about item#723975.
Used for sample storage and shipping of oil
4
From Japan
On 2017-12-13 16:50:46
Although there are rusty parts in some places, for the price, it was a product that can withstand use enough to transport oily liquids.
This review is about item#723984.
Subdivision of paint
4
From Japan
On 2017-11-23 15:09:21
Good cost performance. It was nice to have a hold back.
This review is about item#723957.
When painting work
4
From Japan
On 2017-10-13 09:18:17
Isamu is used for subdividing paint. I'm thankful that the agitator fits perfectly . (Since genuine empty cans are expensive) (- _ -;)
This review is about item#723966.
Storage of paint and brush
5
From Japan
On 2017-10-10 18:00:57
Because it is inexpensive, it can be used easily as a consumable item. I will continue to purchase it from now on.
This review is about item#723948.
When painting work
4
From Japan
On 2017-05-11 12:50:52
It can be used without problems since there is no change from the can that is sold normally because paint enters.
This review is about item#00723957.
For toning of screen printing ink
5
From Japan
On 2017-02-26 16:52:46
We bought the can from the toning tones of 16 colors this time and the necessary ink amount. It was able to be used without difficulty for mixing with a large stirring machine.
This review is about item#723948.
For preservation of paint subdivisions
4
From Japan
On 2017-02-02 13:19:22
I bought it for the division preservation of oil finish paint for wood part. Hold the lid Bubbles return inside (brush ironing?) And it is strong. Since it is temporary storage thing, it is unknown how long it will have for long-term preservation, but I feel that it is solid for price.
This review is about item#723975.
Subdivision of paint
3
From Japan
On 2017-01-06 10:08:21
I bought a can and divided it into small pieces. It is not particularly good, bad or cheap at paint cans of foot, but it is appreciated to be sent in bulk. As we are almost in a disposable state, aside from usability, we will be saved if there is a handling of a cheaper one a little more.
This review is about item#723948.
For rust preventive coating
3
From Japan
On 2016-11-02 15:03:30
Other people were also written, but regrettable that the lid is very difficult to open
This review is about item#723948.
Subdivision of paint
1
From Japan
On 2016-09-29 19:45:29
There was a crushed can in a box that was packed cleanly. The box is strange although there is no collapsed place and the can is crushed why it is beautiful.
This review is about item#723957.
For paint storage after toning
3
From Japan
On 2016-08-05 17:41:12
It was hard to open the lid. I tried to open it little by little while turning with the driver, but the edge of the lid was soft and deformed.
This review is about item#00723966.
Storage
5
From Japan
On 2015-11-03 22:01:54
I am saved because I can buy a paint can's can
This review is about item#00723966.
Used for putting liquid for oily condition
4
From Japan
On 2015-10-22 10:20:55
It was weak to durability and the shape was easy to deform so I thought it would be fine if the material was strong.
This review is about item#00723966.
Woodworking
3
From Japan
On 2015-10-21 03:10:09
Refill and mix paint used in woodworking, and use it as a container to contain beeswax wax. There is no particular problem at the time of use.
This review is about item#00723975.
To divide methanol for removing dirt from a single can
5
From Japan
On 2015-04-02 20:38:26
It is convenient to carry because it has a handle
This review is about item#00723957.
1
Customer Who Viewed This Item Also Viewed
Pail
Round Can
Plain Cans
Paint pail tin can
Round Tin Cans
Square Oil Cans
Steel 20L Open Pail Can
Can
Oily for angle cans
Stain universal can
Color pail
Aqueous for angle cans
Round can for water