Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Floor jack 3.0t

Floor jack 3.0t
Sales Price: 119.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 5
4 star 0
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Tire exchange
3
From Japan
On 2017-07-04 21:38:42
The tire attached to the jack seems to be useless quickly but it was cheap so I think that the price is suitable
This review is about item#1465704.
Vehicle maintenance
5
From Japan
On 2017-04-28 15:07:41
Chevrolet Astro was able to be used without problems. I do not know the durability, but I am satisfied with my present situation.
This review is about item#1465704.
Tire change of my car
5
From Japan
On 2017-04-06 17:20:29
I was able to do work without stress, I expect how many years I can use without failing.
This review is about item#1465704.
Tire exchange
3
From Japan
On 2017-03-13 07:39:15
Although making is sloppy, since there are three, it is useful for shortening the time,
This review is about item#01465704.
When tires of a sales vehicle are exchanged
5
From Japan
On 2017-01-21 18:18:08
This price is 3t compatible, it is a very cost effective product.
This review is about item#1465704.
Used for tire change
5
From Japan
On 2017-01-11 18:57:41
In the past I bought a jack of 3500 yen and used it, but in 2 years the rise started to stop on the way, I purchased this jack this time. I did a demonstration of car tire exchange, but it is light and easy to use and good.
This review is about item#1465704.
Vehicle maintenance
5
From Japan
On 2014-10-26 21:15:33
Used for maintenance of 2000 cc sedan (normal car height). Initially, since the jack point was in the back, we had to insert the jack body all the way, the handle bar interfered with the bumper and could not jack up. Without having to use a bar, I fished it to a certain extent using a short bar, and I was able to work safely using the attached bar. If it was a big round item it would have worked without trouble, but we chose this product with emphasis on portability. For jacking up from the side, I used F - 26 - 1 of Daikin Industry which I purchased at the home center, but there seems to be a special item as well. And what I noticed after using it is that there is no need to raise both wheels in oil change but also that the jack gets in the way of oil discharge and that it is possible to replace oil without any jack up. I think that it is lighter and easier to handle if you choose a pantograph hydraulic jack unless you use a jack stand. I wrote it variously but I am very satisfied with this product.
This review is about item#01465704.
1
Customer Who Viewed This Item Also Viewed
Jack Attachment for Sides
High Lift Jack 2.25T
Garage Jack 3T
Oil-Pressure Lowdown Jack
Hydraulic Floor Jack 3 Ton
Low Down Car Corresponding Jack
Hydraulic Floor Jack
Hydraulic Floor Jack
Hydraulic floor jack 2.25t
Hydraulic lowdown garage jack 2.5t
Hydraulic Floor Jack (3t)
Floor Jack 2t