Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hex bit socket

Hex bit socket
Sales Price: 7.99 SGD
Review Rating: 4.75
4 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Mission oil change
5
From Japan
On 2016-12-11 21:51:59
Extreme mission oil drain is 10 mm hex and injection is the same. Especially the injection side connects the long extension and turns it around 60 cm so it will not turn unless it is a socket. It is an essential tool.
This review is about item#6950676.
Overhaul of front fork of DUCATI 900 S
5
From Japan
On 2016-09-29 20:22:43
Reaching to the bolt at a deep place, it has high rigidity, so you can use it with confidence. In addition, the cost performance is also high. Regular sockets use snap-ons in their nice appearance, but hex-bits are limited to koken.
This review is about item#6950518.
Motorcycle Maintenance
4
From Japan
On 2016-06-09 16:12:13
I am fluffy coke, I'm pretty cool. Hexagon socket head screwdriver with this size (small screw) has shallow hexagonal hole depth, hexagon hole with low hardness directly will have a hexagonal hole, it will be stupid. Since this bit can be used with confidence and it is a long type, work in a narrow place is useful as well.
This review is about item#06950387.
Motorbike remodeling
5
From Japan
On 2015-06-09 21:25:20
A shape that can apply torque with peace of mind.
This review is about item#06950563.
1
Customer Who Viewed This Item Also Viewed
Hexagon Socket, inch
Hexagon socket
Short Hexagon Socket
Torx bit socket
BA socket
Hex bit socket set
Torx bit
Surface socket
9.5SQ Socket
3/8
No.12 Rubber ring set