Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of High-spec line D

High-spec line D
Sales Price: 48.99 SGD
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
Motorcycle Restore
From Japan
On 2017-12-05 19:35:59
Yamaha SDR's rear brake has a hitch and we used 60 centimeters. It is truly a Nichirin product and it seems to be robust in steel banjo. Originally 55 centimeters fit, but Monotaro did not have it. Since the thickness of the banjo is the same as genuine, it was installed with a genuine union bolt with 1 mm thick copper washer. Is your touch too severe? The appearance is the best! It was too long
This review is about item#3998663.
Maintenance of the motorcycle
From Japan
On 2017-05-31 20:31:15
I had trouble with Yodobashi camera. As a result, I made it into a monotail.
This review is about item#3998706.
W650 for replacement
From Japan
On 2016-03-26 10:12:36
"03998715" is used for W 650 of the semi up-up handle. After replacement, we put in fluids, but since W has good accuracy of breeder bolt, we injected it from the bottom, it was immediately usable. The play of the brake is reduced a little, the touch is much better than the normal, and it is also very easy to use, not a gashic. The hose's texture is also good, and iron banjo is safe to use for a long time.
This review is about item#03998715.
Customer Who Viewed This Item Also Viewed
T5 wedge 12V LED bulb
High-spec line A
Sure System Line
Brake Hose
Pedal Rubber
Mesh Hose
Long Throttle Cable
Manifold Set
Front fender