Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of WELDCRAFT tungsten Rare Earth

WELDCRAFT tungsten Rare Earth
Sales Price: 28.99 SGD
Review Rating: 4.67
6 Customer Reviews
5 star 4
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Aluminum welding
5
From Japan
On 2018-02-12 22:43:04
For the first time, it was very difficult to weld aluminum on the second hand scaffold, but it was good that the large 2.4 could melt in.
This review is about item#4540104.
TIG welding (iron, SUS)
5
From Japan
On 2017-11-09 22:22:46
I usually use tritan, but I think it is more durable than tritanium. I often use pulse welding, but if it is tritan, the tip wears out over time, but I think that rare earth (purchased 2.4 mm) can be used for a long time and the number of re-polishing has decreased.
This review is about item#4540104.
Plumbing work
4
From Japan
On 2017-07-16 08:09:05
I think there is no problem. It is saved if it is a little lower price.
This review is about item#04540104.
TIG welding
5
From Japan
On 2017-02-22 19:42:46
Great! The concentration of the arc is too good and it lowers the voltage slightly! It is definitely the best compared with Tritan Lantern Celitan!
This review is about item#4540104.
DC TIG welding
4
From Japan
On 2016-10-30 21:41:17
I was able to use it well for welding iron and stainless steel. Because there was no work of aluminum, it is not used for interchange.
This review is about item#4540104.
Aluminum welding
5
From Japan
On 2016-03-06 17:43:43
I purchased it as a substitute for tritan, but it got a very good finish.
This review is about item#04540095.
1
Customer Who Viewed This Item Also Viewed
Cerium Tungsten Electrodes
Gear Tay
Alumina Gas Lens Nozzle
Alumina gas lens nozzle
E3 tungsten (Lantana)
WELDCRAFT tungsten 2% cerium
WELDCRAFT Electrode Rod
Gas lens WP-17,18,26,1726, for CS410
For large-diameter gas lens WP-17,18,26
WELDCRAFT Electrode Rod