Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wind block pants WB-3P

Wind block pants WB-3P
Sales Price: -
Review Rating: 4.40
5 Customer Reviews
5 star 4
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
At delivery
5
From Japan
On 2017-02-20 15:36:02
I like this with a pretty slim silhouette. Elasticity and heat retention are also sufficient.
This review is about item#5697003.
Light work, light exercise (golf) etc.
5
From Japan
On 2016-01-28 14:41:25
It was stylish and excellent wind protection and very easy to handle. The pocket on the right side was also easy to use, as there is no lid which cargo pants tend to have. I think that it is good enough to be useful for going out to golf. If it were to be improved, it would be better if the material was made lighter and waterproof could be provided.
This review is about item#05697012.
In a room without heating
2
From Japan
On 2016-01-27 20:21:21
I bought it by referring to the revue of motorists on motorcycle commuting but it is not as warm as I thought it is working wearing down pants on top I will certainly heat a hot hot sweat when doing intense move 165 cm 56 kg M size I bought it. The waist size is okay, but the feet are short. The result is quite large. · · · Trousers themselves are slim and slim feeling is good and feeling Good feeling I think that M size is impossible.
This review is about item#05697003.
Commuting by motorcycle
5
From Japan
On 2014-11-22 15:07:05
I commute by motorcycle 40 km (about 1 hour) one way with pass road. The other morning I could withstand 3 degrees Celsius although it was 3 degrees Celsius. (I like the kind of inner tights) I caught rain on the way back, but a windproof film? There was no flood caused by rain because there was a layer of rain. I think that the cost effect is high, but it is good if there is more color development. Army green and so on.
This review is about item#05697037.
I bought it for use on motorcycle commuting.
5
From Japan
On 2014-09-26 22:49:28
I bought it because the motorcycle commuting is a battle against the cold in the season when the outside temperature falls below 20 degrees, but at the outside temperature 15 degrees it can run without any cold at all. I will check if the cold of the wind can be prevented with the outside temperature falling in the future.
This review is about item#05697012.
1
Customer Who Viewed This Item Also Viewed
Adjust Cargo Pants
Neo Soldier Trousers
Bag rail
NEW micro pants 8226
Waterproof Winter Pants