Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Allen wrench

Allen wrench
Sales Price: 0.99 SGD
Review Rating: 4.50
6 Customer Reviews
5 star 4
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Car maintenance
4
From Japan
On 2018-04-12 15:13:07
Things I was looking for were found and I was able to use it very conveniently.
This review is about item#16402182.
Car maintenance
3
From Japan
On 2018-03-25 14:10:25
Writings are written, but licking is not a special feeling. However, it is harder to twist than cheaper articles and it seems to have durability.
This review is about item#16402365.
Motorcycle Maintenance
5
From Japan
On 2018-03-01 15:33:14
Both quality and price are satisfactory. Although it becomes a personal feeling, the wrench becomes unexpectedly worn. I guess preference is better for a little more.
This review is about item#16402322.
In order to remove the fixed cap hexagon socket button cap bolt with 2 mm across flats
5
From Japan
On 2017-05-25 16:59:57
It is used for a licked bolt of a hexagon socket in a recessed place. It is used for rough cure that lightly strikes the long axis side and shakes the short shaft side with a vise plier. It was cheap so I could use such a way without hesitation, but at this price, even this size firmly adopted the surface contact type, size notation is also printed. It is also a point that the long axis side is not a ball point.
This review is about item#16402347.
Machine maintenance
5
From Japan
On 2017-05-25 16:10:36
I often use a hexagon socket head bolt, but it is easy to rotate without dull corners.
This review is about item#16402182.
Car fan belt exchange
5
From Japan
On 2016-10-30 04:17:13
When removing the fan belt's tension pulley with a hexagonal wrench, it seemed like a tanning in the hand held KTC, so when I changed to Wera, I did not lick and I was able to remove the bolt easily. When dismounting it is a dish that can be relieved to the highest.
This review is about item#16402182.
1
Customer Who Viewed This Item Also Viewed
Allen wrench
Allen Long Miri set 7pcs.
Plastic bags input hex wrench
Hex key set
Allen Long 10 mm
Hexagon Short
Combination wrench
950PKS hex key