Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Insulation cup universe

Insulation cup universe
Sales Price: 10.99 SGD
Review Rating: 4.67
3 Customer Reviews
5 star 2
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
For coffee time
From Japan
On 2018-02-04 14:40:34
I do a coffee time when I am waiting for a fishing trip at a fishing spot, but the thin cup is good for the first one when the hands are cold, but the heat is reversed from the second ones. Even though I pass it hotly, I will cool down quickly, but I'm expecting it because it is a thick cup + heat resistant. I'm still unused at fishing spots ☆ I made four.
This review is about item#18289373.
When you drink coffee or tea at a company
From Japan
On 2016-12-23 15:21:57
Since it is troublesome to wash the cup every day, I would like to use a disposable cup to drink coffee or tea at the office. However, many paper cups and insert type cups are around 250 mL, which means that when we drip coffee and put it in, the amount is small and I am not satisfied. So I was looking for a big disposable cup, but I finally found this product. The same product was also on other mail order sites, but everything was out of stock, only monotail was able to be shipped. Try using it for 1 week, so it's as big as 402 mL so you can drink plenty, so it's quite satisfying. It's heat resistant and it is solid compared to ordinary paper cups. It is 50 bags including tax and 733 yen including taxes, which is a little expensive, is it about this from the viewpoint of capacity and making.
This review is about item#18289337.
For coffee or cereal
From Japan
On 2016-06-17 18:52:21
It is nice to see a little smoke of the purple gradation due to the surface material peculiar to the insulation cup. It is strong, so you can use it with confidence.
This review is about item#18289337.
Customer Who Viewed This Item Also Viewed
Recycled Paper Kraft Tape
Paper Cup Sparkle
Daily check cup
Ink Cartridge HP178XL
Heat Insulation Paper Cup
Paper Eco Spoon
Tote bag unbleached plain oversized
Nail clippers (New nail clipper)
Cup 9oz striped orange
Hot cup Snow White