Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Branch Line Coupler (Straight Line Type)

Branch Line Coupler (Straight Line Type)
Sales Price: 18.99 SGD
Review Rating: 4.23
13 Customer Reviews
5 star 7
4 star 3
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 13 of 13 Reviews
Permanent plumbing of factory
5
From Japan
On 2018-04-23 21:27:32
There is no air leak, it enters lightly, it is OK and it is OK without clicks.
This review is about item#19288614.
Used on branch of hose such as air blow gun / spray gun on factory premises equipment.
4
From Japan
On 2018-02-09 14:55:41
I purchase it multiple times. Two series of one-touch desorption type is easy to use, but since it will be directly attached to pipe piping in terms of structure, the method of fixing to the equipment and the structure will be limited. If auxiliary parts or mounting holes that can be fixed with screws or tie wraps etc. are processed, I think that the number of scenes to use will increase. Since it can not be helped, clamp the manifold block part with two 6 × 1/2 Bracket brackets and use it. Also, although you can see a review of "No coupla male is attached ...", it should have had a specification with "coupla male".
This review is about item#19288614.
Branch to the blow gun or spray gun as a permanent compressed air port of the press machine.
2
From Japan
On 2018-01-27 14:24:17
I changed the supply port to the side instead of the center, but I would like a hole for fixing. I would like to fix it to the operation panel, but since the coupler part protrudes more than the manifold part, a spacer is necessary. Also, there is no mounting hole etc, so you need to devise to fix it. At least it is more convenient to process the mounting holes ...
This review is about item#19288614.
For air hose connection in the garage
5
From Japan
On 2017-10-26 20:36:26
Due to the diversification of air hoses in the garage, we purchased along with air coupler expansion. It is cheap and convenient.
This review is about item#19288614.
Ideal for work using multiple air tools!
4
From Japan
On 2017-10-14 23:52:25
Three one-touch couplers are lined up, but when you dropped it from hand, there are times when the air hose is disconnected due to the nature of the coupler, so when switching hose troubles when you are out, it is better to change to a two-touch coupler go up.
This review is about item#19288623.
Use of air tools
4
From Japan
On 2017-02-11 17:47:26
Product has no problem, but it is regrettable that there is no male chuck.
This review is about item#19288614.
Used for branching from compressor
5
From Japan
On 2016-11-23 22:41:06
I used it for branching air from the compressor. With one touch connection, smooth fitting and removing. I am satisfied without leakage. For connection, "Stainless steel screwed hexagon nipple order code 07334092" was used. Regarding pneumatic equipment, since it is an amateur, I was worried about not knowing what to use and what to connect. It was good to have a type with screwed hexagon nipple. Also, if there is information such as a connection example (related parts list to use), it is glad to amateurs.
This review is about item#19288614.
For factory maintenance
5
From Japan
On 2016-08-27 20:59:31
It is attached to air piping and it is used. It is useful because it is cheaper than other brands.
This review is about item#19288614.
Air distribution
3
From Japan
On 2016-08-22 18:19:11
Depending on the socket on the other side, air leakage may occur
This review is about item#19288623.
Car maintenance
5
From Japan
On 2016-08-09 13:00:12
It is easy to use because the coupler is one touch.
This review is about item#19288614.
Place helium gas in multiple persons at the event
5
From Japan
On 2016-08-02 17:18:20
It seems easy to use although it is two weeks later in full swing.
This review is about item#19288648.
Used when using pneumatic instruments
3
From Japan
On 2016-05-27 17:49:26
I could use it normally
This review is about item#19288623.
Motorcycle Maintenance
5
From Japan
On 2016-01-16 17:57:32
One-touch coupler included is convenient. It is also good moderation.
This review is about item#19288614.
1
Customer Who Viewed This Item Also Viewed
Line Coupler 200L
Line Coupler 200 T Model
Male Plug
PU Plug
Small line coupler
PVC button tube
Quick coupling AL type
Safety breaker
Overhead Note label
Branch Coupling, Fixed
Coupling With Rotary