Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Bench drilling machine

Bench drilling machine
Sales Price: 369.99 SGD
Review Rating: 2.86
7 Customer Reviews
5 star 1
4 star 2
3 star 1
2 star 1
1 star 2
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Drilling operation
1
From Japan
On 2018-02-26 15:32:13
I have worked on a hand drill, but I bought a drill machine for the first time. Since the tightening of the tower is weak, it turns around (it is such a specification? Because accuracy of the vice is loose, it can not be firmly fixed (especially small size of 4 to 5 cm or less) After that, the accuracy of rotation of the drill chuck is bad, I regret that I should have used another model.
This review is about item#30386405.
Drilling of aluminum plate or thin iron plate etc.
1
From Japan
On 2017-05-31 23:49:34
Because this is a problem of the manufacturer, I am grateful for the correspondence of Mr. Monotarou but the first one was not able to install due to a tap failure of the steering wheel. Although Montalaro ordered fast exchange, the second one was an overall Whether the accuracy is poor or not, even when nothing is scraped off, even when you start lowering the steering wheel a little bit, Gun, noise and vibration are so terrible that something is scraping like something begins to emerge. For that reason I inspected each part but there is no looseness of screw etc. Also there is no core shake of chuck part, but this trouble is unchanged even if adjusting the belt. Since it is a drilling machine, it is natural that the sound comes out when cutting it, but it is honesty to be honest that such sounds and vibrations will come out before shaving. . .
This review is about item#30386405.
Drilling, rusting with a wire wheel
3
From Japan
On 2017-05-17 18:49:04
I am dissatisfied with pipe rigidity and elevator accuracy, but I think that it is unavoidable considering cost.
This review is about item#30386405.
Making parts for work tools
5
From Japan
On 2017-04-18 14:48:50
It used to be used a bit earlier than the drillboard, but it was a bit expensive but it was really nice because the performance of several stages was high.
This review is about item#30386405.
For any drilling
4
From Japan
On 2017-02-24 22:39:09
It is the first drill as a desktop type. I bought it because it is a model that can raise and lower the table with a handle even at a low price. Motor power is somewhat unsatisfactory when the drill diameter becomes thick, but on the contrary it does not burden on the drill bit, and if we hold it for a long time, we are grasping as a better one. It is a product you want to use for a long time.
This review is about item#30386405.
Drilling with DIY
2
From Japan
On 2016-11-07 10:44:59
I bought a drill machine for the first time. I studied variously with DIY beginners, but I thought that this level was enough, but I bought it, but I was sorry that there was no drilling power as I thought it was. As you can see, it seems better to try it on the actual machine before purchasing.
This review is about item#30386405.
Production of original equipment
4
From Japan
On 2016-10-24 21:37:42
I bought it because it has a handle attached to the elevator and it is convenient for processing a single item of different shape. The taper part of the spindle was rusted with parts confirmation before assembly. I rusted with sandpaper and attached the chuck. I'm glad I had paper of reasonable count. Assembly is easy and completed in about 20 minutes. We performed hole drilling on the aluminum plate, but it was able to be used without problems. I think that cost performance in this class is sufficient. The improvement point is to ensure rust prevention of parts at the time of shipment.
This review is about item#30386405.
1