Chemical Anchors
Chemical anchors are adhesive anchors that fix gold screws and deformed steel bars using chemical reactions. The capsule containing the solvent is inserted into a hole made in concrete, etc., and the capsule is destroyed by driving a gold screw, a sized iron, or a deformed steel rod, etc., causing a chemical reaction of the solvent to fix the anchor. It takes a while for each product to fix. In addition, it is also important to obtain sufficient fixing strength for concrete holes to carefully remove dust and other dust. Products with short capsules that can be used even with a small thickness, such as concrete, are available.
Other Related Pages
- No Brand For chemical anchors (Stainless steel)Used for chemical anchorsMaterial Stainless steel (SUS304) Tip Angle (°) 45 Type Single-sided cut
- Nihon Decoluxe Chemical Anchor R Type (Standard Type)The embedding machine becomes lighter and the work load is reduced. Anchor muscle embedding time has been improved by approximately 20%. It does not contain 13 volatile organic compounds (VOCs) specified by the Ministry of Health, Labor and Welfare. By adopting non-styrene resin, unpleasant odors... Read MoreMaterial Modified vinyl ester resin
- No Brand For chemical anchors Cut into pieces (Iron / Unichrome plating)Used for chemical anchorsTip Angle (°) 45 Material Iron unichrome plating Type Single-sided cut
- Asahi KASEI AR Chemical Setter SUPER LL APSince the main ingredient is epoxy acrylate resin, which has excellent alkali resistance, there is almost no decrease in fixing strength due to aging. Since it has high initial rigidity against tensile force and excellent toughness, it can be widely used for structural members. It is a glass-seal... Read MoreSpecification Rotating / hitting type
- SANKO TECHNO Wire brush for adhesive anchorMetal wire type that demonstrates stable strength. Compatible with all types of adhesive anchors.
- Asahi KASEI EA-500S (Resin Set)(Main agent) The main component is non-styrene epoxy acrylate, which has less odor and improves the environment at the construction site. In addition, by adding thixotropy, liquid dripping during ceiling construction has been eliminated. (Curing agent) A curing agent with good storage stability t... Read MoreMaterial (Main agent) Epoxy acrylate resin Trusco Part No. 328-5472
- Asahi KASEI Adhesive anchor AR chemical setter HP anchor (rotating / hitting type film tube)Excellent adhesion due to high-performance epoxy acrylate resin. The granular curing agent is dispersed throughout the capsule, eliminating uneven mixing with the resin when bolting, and achieving reliable curing. Seismic retrofitting work. For dam construction, etc. * The maximum tensile load is... Read MoreSpecification Rotating / hitting type
- Asahi KASEI AR chemical setter AP short typeBy using "epoxy acrylate resin" as the main agent, it exhibits excellent adhesion. Demonstrates excellent alkali resistance. High initial rigidity and excellent toughness. Concrete, fence / soundproof wall installation, tunnel construction, dam construction, rockfall prevention net inst... Read MoreIngredient Main agent: Epoxy acrylate resin Specification Rotating / hitting type Type Short type
- Asahi KASEI AR chemical setter (short size)A sealed resin capsule anchor that contains epoxy acrylate resin, which has excellent alkali resistance, strong adhesion strength, and almost no change over time, as the main ingredient, and a curing agent and aggregate in a glass tube at a fixed ratio. Since epoxy acrylate resin is used as the m... Read More
- Nihon Decoluxe Chemical anchor R type (short type)The embedding machine becomes lighter and the work load is reduced. Anchor muscle embedding time has been improved by approximately 20%. It does not contain 13 volatile organic compounds (VOCs) specified by the Ministry of Health, Labor and Welfare. By adopting non-styrene resin, unpleasant odors... Read MoreMaterial Modified vinyl ester resin
- Asahi KASEI EA-500 (Resin Set)Two-component mixed injection type with built-in all power (Main agent) The main component is non-styrene epoxy acrylate, which has less odor and improves the environment at the construction site. In addition, by adding thixotropy, liquid dripping during ceiling construction has been eliminated. ... Read MoreMaterial (Main agent) Epoxy acrylate resin
- Nihon Decoluxe Chemical anchor PG type (Chem punch)Designed with consideration for the health of building users and enforcers. We use modified vinyl ester resin that does not use styrene, which is included in 13 volatile organic compounds (VOCs) that cause sick house syndrome, as defined by the Ministry of Health, Labor and Welfare. There is no s... Read More
- UNIKA Resin A injection typeIt is an injection type adhesive anchor. We can handle various bolts and deformed reinforcing bars. L-shaped and U-shaped lines can be constructed. Uses epoxy acrylate resin with high alkali resistance. Fixation to concrete, stone, ALC, hollow base material. Foundation work for steel frames, etc.... Read More
- Asahi KASEI AR Chemical Setter MU typeJust by driving it, it exerts a strong fixing force. L-shaped and U-shaped lines can be constructed. Has excellent alkali resistance. Fixation of concrete blocks. Soundproof wall mounting. For tunnel construction, etc. * The maximum tensile load is the value when the concrete strength is Fc21N / ... Read MoreSuitable Material Concrete block Specification Driving type Ingredient Main agent: Epoxy acrylate resin
- Osaka Spirit Chemical cutting (iron / dove)Surface Treatment Dove Material Ironfrom S$3.99Min. 2 days
- Nihon Decoluxe EL350N cartridgeConstruction using modified vinyl ester resin that does not use "styrene" as a raw material, which the Ministry of Health, Labor and Welfare warns of "suspicion of carcinogenesis" and "risk of adverse effects on fertility or foetation" as hazard information. It does ... Read MoreSet Contents 1 EL-350 cartridge, 2 EL nozzles
- Maeda Kosen "Bolt Mate Epo EP-450" 300ml bottle typeAn injection-type adhesive post-construction anchor that mixes and installs a room-temperature curing type low-viscosity epoxy resin main agent and curing agent on-site. To stir and mix, just hold the main agent container in your hand and shake it, and no special equipment is required. It has a l... Read MoreCapacity (mL) Main agent: 206 / curing agent: 94 Included Accessories 1 base bottle, 1 hardener bottle Mass (g) 418 Applicable Standard JAIA F ☆☆☆☆ compatible product Trusco Part No. 467-5444
- SANKO TECHNO Sankowa brushThe wire part makes small scratches on the surface of the concrete hole to improve the adhesive strength of the adhesive anchor. A brush for cleaning chips in the holes * When selecting a product, be sure to pay attention to the applicable drilling diameter. * Be sure to wear leather gloves when ... Read MoreDrilling diameter (mm) (Conformity) 19.0-20.0 Mass (g) 103.5 Brush Length (mm) 130 Outer Diameter (mm) 19 Overall Length (mm) 465 Trusco Part No. 859-6108 Material (Brush Part) Metal Specification Sankowa brush Material (Handle) woodfrom S$22.99Min. 2 days
- Asahi KASEI EA-500 exclusive mixing nozzleThe 12 spirals (blades) ensure that the main agent and curing agent are kneaded.from S$58.99Min. 2 days
- Nihon Decoluxe Evolock GL450It meets the epoxy resin physical property standard values specified by NEXCO (former Japan Highway Public Corporation). Epoxy resin is the main component, and stable adhesive strength can be obtained due to its strong adhesive strength. Lean construction method: Since it is a cartridge type, an ... Read MoreTime can be Used (minutes) (5℃)120、(10℃)90、(20℃)40、(30℃)25、(35℃)15 Curing Time (hours) (5℃)24、(10℃)16、(20℃)8、(30℃)5、(35℃)4 Capacity (mL) 450from S$66.99Min. 2 days
- N Pat Perfix spike capsule (adhesive post-installation adhesive anchor)Highly corrosion-resistant vinyl ester resin that does not contain styrene is used as the main agent. Stepped glass is used for all sizes to ensure that the glass tube is crushed and that the resin and hardener are mixed more smoothly.
- UNIKA Resin A mixing nozzle (3)Contains 3 mixing nozzles for both GE type and PE type.Mass (g/set) 31 Trusco Part No. 363-3128 Applicable cartridge GE-165・GE-410・PE-400N Material Resin
- Osaka Spirit Chemical cutting (stainless steel)Material Stainless steel
- A.Y. Fastener Chemical Insert (Steel)Anchor method that combines an insert with an internal thread and a chemical anchor (resin fixing material). The attachment can be tightened with commercially available bolts like an internal screw anchor. You can freely choose the length of the bolt according to the thickness of the attachment. ... Read Morefrom S$7.49Min. 2 days
- UNIKA Resin A HC-U type (implanted type)Bolts and reinforcing bars can be cut into small pieces for construction. The unique glass tube shape reduces the number of hammer hits. Using vinyl ester resin with high alkali resistance, it can be stored for a long time before construction. Foundation work such as steel frames, road work, tunn... Read MoreSpecification Driving type Material Main agent: Vinyl ester resin
- Asahi KASEI EA-500 (base kit)A great value set with a storage bag. (Main agent) The main component is non-styrene epoxy acrylate, which has less odor and improves the environment at the construction site. In addition, by adding thixotropy, liquid dripping during ceiling construction has been eliminated. (Curing agent) A curi... Read MoreMaterial (Main agent) Epoxy acrylate resin
- KFC SartiteAchieves strength, excellent workability, and economy that are not inferior to conventional resin capsule anchors. Since it is a capsule type, it is easy to install without weighing, kneading, or injecting work. The water ratio is properly controlled just by immersing it in water, and stable perf... Read Morefrom S$34.99Min. 2 days
- A.Y. Fastener Chemical insert (stainless steel)Anchor method that combines an insert with an internal thread and a chemical anchor (resin fixing material). The attachment can be tightened with commercially available bolts like an internal screw anchor. The length of the bolt can be freely selected according to the thickness of the attachment.... Read MoreMaterial Stainless steelfrom S$13.99Min. 2 days
- Nihon Decoluxe EL mixing nozzleThe spiral structure allows the main agent and curing agent to be mixed reliably.from S$45.99Min. 2 days
- Nihon Decoluxe GLN NozzleThe spiral structure allows the main agent and curing agent to be mixed reliably. * If the drilling diameter is 19 mm or less and the drilling depth is 180 mm or more, be sure to attach the attached extension tube before injecting the resin. * When the extension nozzle is attached, the perforatio... Read MoreSet Contents Mixing nozzle, extension tube, 10 each Outer Diameter (Φmm) (Mixing) 18 Length (mm) (Mixing) 170from S$56.99Min. 2 days
- SANKO TECHNO Eagle anchor EG type steel metric screwNemeji anchor for AR chemical setter (EA-500 / 500S / 500W / EX-350 / 400L). It maximizes the ability of the adhesive resin and firmly fixes it in the concrete hole. It is possible to adjust the non-landing and attach / detach the attachment, which is unique to the Nemeji type. Bench installation... Read Morefrom S$6.99Min. 2 days
- Osaka Spirit Chemical cutting (iron / dove) (small box)Surface Treatment Dove Material Ironfrom S$3.59Min. 3 days
- SANKO TECHNO Eagle anchor EG type Stainless steel metric screwMaterial Stainless steel
- Nihon Decoluxe GLG GunWhen the trigger is released, the resin discharge stops. A lightweight and easy-to-use manual gun.from S$449.90Min. 2 days
- N Pat Perfix resin capsule (organic capsule-type adhesive anchor)Anchor system that has excellent durability and shows high physical properties by using unsaturated polyester resin that cures quickly at room temperature and is stable, and uses the highest-ranked screw-based unsaturated polyester resin as the main agent. Is established. * RC-12, RC-16, RC-20, R... Read Morefrom S$44.99Min. 6 days
- Nihon Decoluxe EL dedicated gunWhen the trigger is released, the resin discharge stops. A lightweight and easy-to-use manual gun.from S$299.90Min. 2 days