Well-balanced performance with good mechanical strength, heat resistance, abrasion resistance, chemical resistance, and machinability. By polymerizing and molding the main raw material nylon monomer under atmospheric pressure, the characteristics of nylon are improved, and it has excellent featur... Read More
Thickness Tolerance (mm) 0~+1.0 Surface Resistance (Ω) 1013Color Blue Type Cutting board Material MC nylon (MC901) Length Tolerance (mm) ±0.3 Width Tolerance (mm) ±0.3
This is a basic grade of MC nylon with improved mechanical strength, thermal properties, and chemical properties compared to general 6 nylon. It has excellent mechanical strength and durability compared to conventional nylon resin. It is a self-lubricating material with excellent sliding performa... Read More
Thickness Tolerance (mm) 0~+1.0 Width Tolerance (mm) 0~+15.0 Length Tolerance (mm) 0~+20.0 Color Blue Material MC nylon Type MC901
The MC602ST has improved machinability compared to the conventional MC601ST, especially reduces damage to the blade due to the filler, and extends the life to stabilize and maintain a good finished state. The filling material has been improved to improve the ease of cutting compared to the conven... Read More
Surface Resistance (Ω) 1013Length (mm) 1200 Width (mm) 600 Material MC nylon Type MC602ST
This is a basic grade of MC nylon with improved mechanical strength, thermal properties, and chemical properties compared to general 6 nylon. It has excellent mechanical strength and durability compared to conventional nylon resin. It is a self-lubricating material with excellent sliding performa... Read More
Thickness Tolerance (mm) 0~+1.0 Width Tolerance (mm) 0~+15.0 Length Tolerance (mm) 0~+20.0 Material MC nylon Type MC900NC Color Natural color
A special lubricant has been added to the base of MC901 to further improve slip performance and wear resistance. It is a "stick slip countermeasure product" suitable for solving problems such as the machine not moving smoothly and vibrations occurring. MC901 is one of the materials with... Read More
Thickness Tolerance (mm) 0~+1.0 Width Tolerance (mm) 0~+15.0 Length Tolerance (mm) 0~+20.0 Length (mm) 1200 Width (mm) 600 Material MC nylon Type MC703HL Color Purple
Special graphite is added to the base of MC901 to improve weather resistance, wear resistance, and slip characteristics. The product color of MC801 with the addition of special graphite is metal black. It blocks ultraviolet rays and shows weather resistance. Withstands long-term outdoor use. It h... Read More
Thickness Tolerance (mm) 0~+1.0 Width Tolerance (mm) 0~+15.0 Length Tolerance (mm) 0~+20.0 Color Dark gray Material MC nylon Type MC801
The antistatic characteristics and heat resistance in the high resistance range have been improved compared to the conventional MC501CD R6. Demonstrates heat resistance up to 150 ° C. It has antistatic performance with a volume specific resistance of 108 to 1010 Ωcm. Improvements have been made t... Read More
Thickness Tolerance (mm) 0~+1.0 Width Tolerance (mm) 0~+15.0 Length Tolerance (mm) 0~+20.0 Surface Resistance (Ω) 106~109Length (mm) 1200 Width (mm) 600 Color Black Material MC nylon Type MC501CDR9
Based on MC901, carbon-based filler is added to add conductive performance. It can also be used in places where it is difficult to make resin due to the generation of static electricity. The volume intrinsic resistance is as low as 1 to 102 Ωm. The filler of MC501CD is evenly dispersed, and the r... Read More
Width Tolerance (mm) 0~+15.0 Length Tolerance (mm) 0~+20.0 Length (mm) 1200 Width (mm) 600 Color Black Material MC nylon Type MC501CDR2
Volume specific resistance value 10 2 to 10 4 Ω ・ cm, which is a very low resistance value. The resistance value is constant in all parts, so you can use it with confidence even after machining. Even if the surface is worn, the resistance value does not change, and the resistance value does not ... Read More
This is a basic grade of MC nylon with improved mechanical strength, thermal properties, and chemical properties compared to general 6 nylon. It has excellent mechanical strength and durability compared to conventional nylon resin. It is a self-lubricating material with excellent sliding performa... Read More
MC Nylon is a large engineering plastic manufactured by the casting method. In addition to strong mechanical strength and excellent wear resistance, it is also highly elastic and self-lubricating. High mechanical strength / Excellent mechanical strength and durability compared to conventional nyl... Read More
MC Nylon is a large engineering plastic manufactured by the casting method. In addition to strong mechanical strength and excellent wear resistance, it is also highly elastic and self-lubricating. High mechanical strength / Excellent mechanical strength and durability compared to conventional nyl... Read More
MC Nylon is a large engineering plastic manufactured by the casting method. In addition to strong mechanical strength and excellent wear resistance, it is also highly elastic and self-lubricating. High mechanical strength / Excellent mechanical strength and durability compared to conventional nyl... Read More
It is a high-tech material that combines the excellent sliding performance of MC nylon with antistatic performance. The half-life is 2 seconds or less due to the electrostatic damping characteristics (compliant with JIS L 1094). It is non-filler (non-carbon), and contamination by additives is min... Read More
Width Tolerance (mm) 0~+15.0 Length Tolerance (mm) 0~+20.0 Length (mm) 1200 Width (mm) 600 Color Ivory Material MC nylon Type MC500ASR11
Based on MC901, carbon-based filler is added to add antistatic performance. It can also be used in places where it is difficult to make resin due to the generation of static electricity. The volume intrinsic resistance is as low as 1 to 104 to 106 Ωm. The filler of MC501CD is evenly dispersed, an... Read More
Color Black Type MC501CDR6 Length Tolerance (mm) 0~+20.0 Material MC nylon Width Tolerance (mm) 0~+15.0 Length (mm) 1200 Width (mm) 600