Motorcycle
Other Related Pages
- KIJIMA Oil-resistant two-layer pipe hose (compatible with gasoline)Two-layer structure using oil-resistant rubber inside * Cannot be used for injection vehicles.Oil resistance temperature (℃) 100
- KIJIMA Helmet lock (general purpose)A helmet lock that comes in handy when you're on the go. By locking the helmet while shopping or sightseeing, you will be able to act lightly. * Please use M6 countersunk bolts for mounting. * Can be used as a repair part for the helmet lock dedicated to each KIJIMA model. * When manufacturin... Read More
- KIJIMA Helmet LockA convenient helmet lock is attached to the left tandem step. It is installed without any discomfort without spoiling the image of the car body.
- KIJIMA Heat-Resistant Sticker (Aluminum Sheet)The heat resistant temperature of the adhesive is 150 ° C or less. Please avoid using it for high-pitched parts such as exhaust pipes. * The heat resistant temperature of the adhesive is 150 ° C or less. Please avoid using it in high temperature parts such as exhaust pipes.Heat Resistance Temperature (℃) 150
- KIJIMA Small turn signal lamp (aluminum die-cast)A type of blinker that can be crimped on a shaft-shaped stay * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able to compensate you.Type #680 Lens Color Amber Attached Valve Without S bulb
- KIJIMA Fuel jointSince it can be split and joined with one touch, workability is improved when removing the fuel tank etc. by interrupting the fuel line! When splitting, the built-in valve of the main body closes to prevent the outflow of gasoline. (W stopper type has a built-in valve on the insert side)Specification Resin body W stopper
- KIJIMA Turn signal ASSY FR / RL* This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able to compensate you.Color Amber
- KIJIMA Back supportBag support that prevents entanglement when attaching the side bag. Set with a black finish so as not to break the unique Bobber style. Considering practical use, the left side is set as a single unit.Suitable for Bonneville Bobber / Left Color Blackfrom S$119.90Min. 7 days
- KIJIMA Tandem gripIntroducing a tandem grip that can be installed without breaking the style of the Z900RS / CAFE, which is a revival of the old Z style to the present day, and is convenient for loading luggage. The side grip is designed to be as close to the seat surface as possible in order to increase the sense... Read MoreSuitable for Z900RS Material Steel
- KIJIMA BIG Square Mirror (for new vehicle certified vehicles)Excellent visibility !! For both left and right. * This product is an important safety part, so be sure to outsource the replacement work to a certified maintenance company. If you replace it by yourself, you will be responsible for it and we will not be able to compensate you.Type Left and right combined use
- KIJIMA Fuel jointSince it can be split and joined with one touch, workability is improved when removing the fuel tank etc. by interrupting the fuel line! When splitting, the built-in bubble of the main body closes to prevent the outflow of gasoline. (W stopper-type has a built-in bubble on the insert side)Material Resin bodyfrom S$46.99Min. 7 days
- KIJIMA Slim gripIntroducing a new electronic throttle compatible model in the slim grip series that is closer to genuine and easier to grip than genuine! Grip left and right throttle pipes included.from S$63.99Min. 7 days
- KIJIMA Bag supportA new lineup for Super Cub C125 is available for bag support that prevents entanglement when attaching side bags! Demonstrates functional effects while maintaining the image of the car body. Plating specifications that have a high dress-up effect even by itself. Set as a left and right set and le... Read MoreMaterial Steel chrome finish Color Platingfrom S$99.90Min. 6 days
- KIJIMA 405-238 +++ Engine Guard + BlackIntroducing an engine guard that can handle minor falls such as standing up! A well-thought-out shape that has been repeatedly verified for the actual state of a fall. Clamp type fog lamps and pegs can also be attached, making it useful for touring. Steel black finish Pipe diameter: 25.4mmSuitable for Rebel 250/500 + 17Y-from S$229.90Min. 7 days
- KIJIMA Heat / Oil Resistant Double Layer Pipe Hose (Gasoline Compatible) with ClipA two-layer structure that uses oil-resistant rubber on the inside and heat-resistant neoprene on the outside protects the hose from heat sources such as engines. * Cannot be used for injection vehicles.Specification With clip Heat Resistance Temperature (℃) 120 Oil resistance temperature (℃) 100
- KIJIMA Hose Conversion JointA replacement joint used when the inner diameter of the hose is different when replacing the tank or captor. Available in aluminum and nylon.Specification With clip
- KIJIMA Heat / Oil Resistant Double Layer Pipe Hose (Compatible with Gasoline)A two-layer structure that uses oil-resistant rubber on the inside and heat-resistant neoprene on the outside protects the hose from heat sources such as engines. * Cannot be used for injection vehicles.Heat Resistance Temperature (℃) 120 Oil resistance temperature (℃) 100
- KIJIMA Hose Power Band (Steel: Trivalent Chromate)Arch type that is easy to spread with pliers etc.
- KIJIMA Gasket SheetFreely cut with a cutter etc. to match the genuine cover. Asbestos is not used. * We recommend that you ask a maintenance company to replace this product. Compensation may not be possible if the replacement work is done individually.Heat Resistance Temperature (℃) 180
- KIJIMA Gasoline filter (metal fiber)Intermediate performance type that has both filtration capacity and flow rateSpecification -
- KIJIMA Gasoline filter L typeThe use of a fine basket filter improves the filtration capacity, and the magnet type collects iron powder that can damage the cylinder, enabling more perfect filtration.
- KIJIMA Hose Clip A Type (Stainless Steel)A type hose clip. Please use it for lines that do not apply pressure.Material Stainless steel
- KIJIMA Stainless Muffler BandMore tightening torque can be applied compared to conventional bands.Material (Bolt) Steel Material (band) Stainless steel
- KIJIMA Copper WasherBe sure to replace it when replacing the brake hose, etc. The same copper as genuine is used to maintain high confidentiality.
- KIJIMA Silicone Cord 7mmUses 7 copper core cables with excellent conductivity! Excellent insulation of pure silicone rubber and super glass fiber prevents electric leakage! Excellent weather resistance.
- KIJIMA Oil filter conventional element (no magnet)An even better new feature has been added to the conventional high quality Kijima oil filter. A special design that takes the oil flow rate into consideration and a powerful donut-shaped magnet inside the filter effectively absorbs sludge (iron powder) mixed in the oil. The mounting method is the... Read More
- KIJIMA Silent Glass WoolThe muffling effect can be improved by replacing it when the muffling effect deteriorates due to aging.Included Accessories Stainless wire Heat Resistance Temperature (℃) 600
- KIJIMA Gasoline Filter (Nylon Mesh)The use of a fine basket filter improves the filtration capacity, and the magnet type collects iron powder that can damage the cylinder, enabling more perfect filtration.Specification Red Color Red
- KIJIMA Hose power bandA new black pattern has been added to the hose power band that applies force evenly to prevent the hose from coming off.Material Steel Color BK
- KIJIMA Hose Clip B Type StainlessThe hose clip B type, which has a shape that is easy to pick up, is now available by changing the material to stainless steel. Made of stainless steel, which is more resistant to rust and more durable than conventional piano wire, you can use it for a longer time with peace of mind.
- KIJIMA High protection filmA guard film that protects the car body from scratches and rust for a long period of time. A single-sided adhesive film for car bodies that uses a transparent acrylic adhesive on a base material with excellent gasoline resistance and wear resistance. It has excellent adhesion and fits well on sim... Read More
- KIJIMA ConnectorA T-shaped connector that is convenient for branching fuel lines and oil lines. Made of resin Water, gasoline, oil * Because it is not metal, it cannot be used in places with high temperatures or pressure.
- KIJIMA Coupler housing, waterproof typeThe coupler is convenient when there are many connections and disconnections of water wiring. 1 pair of male and femaleSpecification HM090
- KIJIMA One Way Valve Ball TypeUsed for gasoline tank breathers to minimize the outflow of gasoline in the event of a fall. (In the race, it is required to be installed by MFJ rules.) * Cannot be used for fuel lines.Material Aluminum Finish Anodized
- KIJIMA Gasoline filterThe use of a fine basket filter improves the filtration capacity, and the magnet type collects iron powder that can damage the cylinder, enabling more perfect filtration.
- KIJIMA Wire lock drain boltDrain bolts whose regulation is fixed by wire in the race. Made of steel for strength. The strong magnet at the tip of the bolt also has an excellent cleaning function to remove sludge such as iron powder in oil.Included Accessories Copper washer, wire for wiring
- KIJIMA Oil resistant / pressure resistant / water resistant / weather resistant hose 1. 5MPaHose with excellent oil/pressure/water resistance on the inside and rubber with excellent weather resistance on the outside. It has a pressure resistance of 1.5 MPa, and can handle temperatures of -40°C to +100°C for oil and 0°C to +60°C for water. Supports external temperatures from -40°C to +70... Read MoreMaterial (Reinforcing layer) Synthetic fiber Maximum Operating Pressure (MPa) 1.5 Withstand Pressure (MPa) 1.5
- KIJIMA Release tie wrapIdeal for places where tightening and detachment are repeated frequently, such as temporary fixing of parts. It can be removed.Color Black
- KIJIMA Oil resistant hose pinkPlease use it in places where heat is not applied, such as fuel lines. Not suitable for hot or hot areas. Also, it cannot be used for injection vehicles.Specification With clip Operating Temperature Range (℃) -38~60