Oils / Fuels
Oil / fuel system refers to parts of motorcycle equipment such as oil filters, various hoses and joints. The demand for oil filters for motorcycles is the highest, and it seems that there are many people who change filters when changing oil. The best selling hose is a two-layer hose with oil-resistant rubber inside. In addition to oil resistance, there is also a heat and oil resistant two-layer pipe hose, which is characterized by protecting the hose from the heat of the engine and so on. Since rubber products harden due to the weather and cold / warm conditions, try to replace them regularly.
Other Related Pages
- MonotaRO Oil filter for motorcyclesHigh quality motorcycle oil filter supervised by a Japanese manufacturer. With O-ring and gasket. For motorcycles *Never use it with anything other than an oil filter. *Please be sure to check the "genuine part number" as the type differs depending on the model and year even if it is th... Read More
- Union Sangyo (UNION) Oil Filter for Two-Wheeled VechicleThe best filter paper is made by highly efficient folding method, which prolongs the life of oil and engine. The Malaysian factory, one of the main factories of the union industry, acquired the international standard "ISO9001" certification for quality systems in 1999, and manages the q... Read More
- KIJIMA Oil-resistant two-layer pipe hose (compatible with gasoline)Two-layer structure using oil-resistant rubber inside * Cannot be used for injection vehicles.Oil resistance temperature (℃) 100
- DAYTONA Super Oil Filter for MotorcyclesIncrease the creases of the filter by about 20% to expand the filtration area. Efficiently removes foreign matter in the oil and reduces the burden on the engine. The excellent performance supported by the filtration performance test is a proof of domestic production manufactured under strict qua... Read More
- DAYTONA Fuel filter for motorcycleShutting out foreign substances such as dust and rust in the gasoline tank in advance is the first step to take care of the engine and make it last longer. Installed in the middle of the fuel hose from the gasoline tank. The transparent body allows you to check the degree of dirt immediately! * I... Read More
- DAYTONA One way valve setBrake air bleeding tool that uses a one-way valve mechanism to prevent backflow. It is lightweight and has excellent durability because it uses a spring-loaded valve with a small aluminum body. A hose with an inner diameter of Φ5 is attached for inserting the nipple. * Box wrench is not included.... Read More
- KITACO (K-CON) nippleA nipple that can be used as an outlet for oil coolers, case breathers, etc.
- K&N oil filterA high-performance oil filter from K & N that uses a proven K & N filter. By increasing the excellent filtration performance and oil flow rate, the pressure loss due to the filter is reduced and the engine performance is improved. Filtration effect By impregnating cellulose material with ... Read More
- KIJIMA Fuel jointSince it can be split and joined with one touch, workability is improved when removing the fuel tank etc. by interrupting the fuel line! When splitting, the built-in valve of the main body closes to prevent the outflow of gasoline. (W stopper type has a built-in valve on the insert side)Specification Resin body W stopper
- KIJIMA Fuel jointSince it can be split and joined with one touch, workability is improved when removing the fuel tank etc. by interrupting the fuel line! When splitting, the built-in bubble of the main body closes to prevent the outflow of gasoline. (W stopper-type has a built-in bubble on the insert side)Material Resin body Suitable Hose Inner Diameter (Φmm) 8from S$46.99Min. 7 days
- DAYTONA Oil drain washerA high-grade drain bolt gasket with an antistic coating on the surface. It is widely used by 4-wheel manufacturers. Cannot be used with Daytona Oil Clean Bolt at the same time. Please use a special product.Thickness (mm) About 1.7
- KITACO Super Fuel Hose SETA transparent tube with high gasoline resistance. Even if dust or water gets in, you can immediately see the inside. The green hose is medium quality, making it ideal for carburetor breathers and fuel tank breathers. Since the pink hose is soft, it does not harden even in winter and is ideal as a... Read MoreLength (m) 1 Included Accessories 5 hose clips
- KIJIMA Heat / Oil Resistant Double Layer Pipe Hose (Gasoline Compatible) with ClipA two-layer structure that uses oil-resistant rubber on the inside and heat-resistant neoprene on the outside protects the hose from heat sources such as engines. * Cannot be used for injection vehicles.Specification With clip Oil resistance temperature (℃) 100 Length (m) 1 Heat Resistance Temperature (℃) 120
- MonotaRO Fuel (gasoline) filter for motorcyclesSince it is transparent, you can easily check the degree of dirt visually. It can be easily installed by measuring the inner diameter of the fuel hose from the gasoline tank and selecting the one that matches the dimensions of the insertion part on the filter side. As a replacement fuel filter fo... Read MoreSpecification Paper filtration specifications
- EXCEL Oil filter for motorcycleExcel oil filter with a history of 50 years on four wheels. Reliable technology. * Gaskets may not be usable depending on the model.Recycled paper use mark Conformity RoHS directive (corresponding to 10 substances) Correspondence
- KIJIMA Hose Conversion JointA replacement joint used when the inner diameter of the hose is different when replacing the tank or captor. Available in aluminum and nylon.Specification With clip
- KITACO (K-CON) Fuel HoseA two-layer hose that uses NBR (nitrile rubber) for the inner layer. Has excellent heat resistance, cold resistance, oil resistance, and gasoline resistance. * Cannot be used for injection vehicles.Length (m) 1 Color Black
- Vesrah oil filterBesura is a Japanese manufacturer with 55 years of history and accumulated technology. The product is produced in Japan and has the same specifications as the genuine product, so you can use it with confidence. * O-rings may not be included depending on the product number. For details, please che... Read More
- NTB Fuel HoseIt has a double structure and has excellent oil resistance.Length (m) 1
- KIJIMA Heat / Oil Resistant Double Layer Pipe Hose (Compatible with Gasoline)A two-layer structure that uses oil-resistant rubber on the inside and heat-resistant neoprene on the outside protects the hose from heat sources such as engines. * Cannot be used for injection vehicles.Heat Resistance Temperature (℃) 120 Oil resistance temperature (℃) 100 Length (m) 1
- NTB Oil FilterLong-lasting car with excellent filter effect. Obtained ISO9022 certification.
- DAYTONA Drain bolt gasketWhen removing the drain bolt for oil change etc., it is recommended to replace the gasket at the same time. Can be used for normal drain bolts, etc. Cannot be used with Daytona Oil Clean Bolt at the same time. Please use a special product.
- DAYTONA Oil-resistant rubber gasoline hoseHigh quality is achieved by using synthetic rubber (excellent in gasoline resistance) on the inside and polyethylene rubber (excellent in weather resistance) on the outside. Includes 5 hose clips. * Cannot be used for gasoline hoses for injection vehicles. * Cannot be used for brake fluid.Included Accessories Hose clips: 5 Withstand Pressure (MPa) 1 Length (m) 1
- MonotaRO Magnet oil filter for motorcyclesBy incorporating a magnet, the iron powder removing power is improved compared to conventional products. Iron powder contained in the oil may damage the engine. As the oil passes through the filter, it protects the important engine by removing iron powder with a magnet. For motorcycles * Never us... Read More
- KIJIMA Gasoline filter (metal fiber)Intermediate performance type that has both filtration capacity and flow rateSpecification -
- KIJIMA Gasoline filter L typeThe use of a fine basket filter improves the filtration capacity, and the magnet type collects iron powder that can damage the cylinder, enabling more perfect filtration.
- KIJIMA Oil filter conventional element (no magnet)An even better new feature has been added to the conventional high quality Kijima oil filter. A special design that takes the oil flow rate into consideration and a powerful donut-shaped magnet inside the filter effectively absorbs sludge (iron powder) mixed in the oil. The mounting method is the... Read More
- ALBA Fuel hoseRubber products harden due to climate and temperature differences. We recommend regular replacement. * Please install under the guidance of a skilled and specialized technician.Length (m) 1 Color Black Manufacturer General purpose Material Rubber
- K&N Oil FilterK & N's high-performance oil filter has gained tremendous trust as a high-flow air filter. By increasing the excellent filtration performance and oil flow rate, the pressure loss due to the filter is reduced and the engine performance is improved.
- KIJIMA Gasoline Filter (Nylon Mesh)The use of a fine basket filter improves the filtration capacity, and the magnet type collects iron powder that can damage the cylinder, enabling more perfect filtration.Maximum Outer Diameter (mm) 21 Dimension D (mm) 21 Dimension B (mm) 32 Dimension L (mm) 60 Overall Length (mm) 60 Specification Red Color Red
- ZETA Drain Bolt with MagnetA strong magnet is press-fitted into the tip of the bolt to collect a small amount of iron powder contained in engine oil. Equipped with a wiring hole to prevent loosening. M8 bolts are made of stainless steel. M10 and M12 bolts are made of aluminum.Screw Length (mm) 15 Material Aluminum Applicable bolt size M12 Teeth Spacing P1.5
- KIJIMA ConnectorA T-shaped connector that is convenient for branching fuel lines and oil lines. Made of resin Water, gasoline, oil * Because it is not metal, it cannot be used in places with high temperatures or pressure.
- KITACO Almidren boltThis aluminum drain bolt uses the finest aluminum for aircraft and is commercialized with aluminum that has been further heat-treated. The tensile strength is about twice as strong as the aluminum alloy bolts that use 5056 materials that are usually on the market. Furthermore, the finish is a sur... Read More
- DAYTONA 3WAY fuel cockON / OFF / RES 3WAY type. Hose inner diameter: Φ6 * If you do not use 3WAY type (39253) RES, please block it.
- KIJIMA One Way Valve Ball TypeUsed for gasoline tank breathers to minimize the outflow of gasoline in the event of a fall. (In the race, it is required to be installed by MFJ rules.) * Cannot be used for fuel lines.Overall Length (mm) 43.5 Dimension (mm) 6 Material Aluminum Finish Anodized
- KIJIMA Wire lock drain boltDrain bolts whose regulation is fixed by wire in the race. Made of steel for strength. The strong magnet at the tip of the bolt also has an excellent cleaning function to remove sludge such as iron powder in oil.Included Accessories Copper washer, wire for wiring
- KIJIMA Gasoline filterThe use of a fine basket filter improves the filtration capacity, and the magnet type collects iron powder that can damage the cylinder, enabling more perfect filtration.