Inverters / Other Related Supplies
Other Related Pages
- Watty Float Switch (for Water and Chemicals)Reed switch type ultra-compact, Japan's smallest class Food Sanitation Law compliantMaximum Switching Current 0.5A Number of Control Points 1 Applicable Voltage (V) Maximum AC100 / DC100 Operation ON when the liquid level rises Detection Method Reed switch type Electric wire used UL1007 AWG24 Applicable Liquid Water (standard liquid)
- Riko Float SwitchA reed switch is enclosed inside, and the switch operates by the magnetic force of the magnet inside the float. If you set the float in the opposite direction, it will turn on ascending (reversible).As ONE Part Number 1-4069-01 Contact Resistance (mΩ) 150 Contact Capacity 50W DC/AC Maximum Switching Current DC/AC0.5A Maximum switching voltage (V) DC/AC300 Dielectric strength between contacts (V) DC500 Material PP (polypropylene) Insulation Resistance (MΩ) over 100
- Mitsubishi Electric High Frequency Brake ResistorYou can improve the usage rate of regenerative braking. * For 15K, use a configuration in which two 18Ω units are connected in parallel. * For 22K, configure two 13Ω units connected in parallel. * For H15K, connect two 18Ω units in series. (The resistor is described as FR-ABR-15K. Same resistor a... Read More
- Mitsubishi Electric Line Noise FilterThis is a noise filter for suppressing radio noise and line noise radiated from the power supply side or output side of the inverter. * The FREQROL-A700 and F700 (P) series 55K and below have a built-in equivalent product (zero-phase reactor) on the input side.
- Mitsubishi Electric Inverter Option DC Reactor FR-HEL SeriesDue to the miniaturization, the mounting area is smaller than the conventional model.
- Mitsubishi Electric Parameter Unit Connection Cable for InverterCable for connecting the operation panel and parameter unit. * Not applicable to conventional series such as FREQROL-A200 and Z200 series.Length (m) 5 Suitable Model FR-A500, E500 series
- Toshiba Schneider Inverter Inverter option* We do not deliver to private homes (detached houses / apartments). * Depending on the delivery location, the delivery date may be postponed and additional shipping charges may be incurred. * Since it will be delivered by a large vehicle of 4 tons or more, we may ask the customer to pick up the ... Read Morefrom S$37.99Min. 2 days
- Mitsubishi Electric Attachment compatible attachmentWith this attachment, it can be mounted as it is using the mounting holes for the conventional model FREQROL-A024 / A044 series. This is convenient when you want to replace the existing conventional model with the FREQROL-E700 series. * If an attachment is used, the depth dimension after installi... Read Morefrom S$64.99Min. 2 days
- Mitsubishi Electric Inverter Option AC Reactor FR-HAL SeriesDue to the miniaturization, the mounting area is smaller than the conventional model.
- Mitsubishi Electric For Cooling Fan FR-E720-15K* The compatible body (FR-E720-15K) has two cooling fans. If you need one, please purchase two.Suitable Model FR-E720-15Kfrom S$39.99Min. 2 days
- Fuji Electric Braking ResistorIt is used to improve braking ability when the vehicle is started or stopped frequently or when the moment of inertia is large.from S$74.99Min. 3 days
- Mitsubishi Electric Inverter option for FR-A800 + setup software + FR-Configurator2Specification Inverter setup softwarefrom S$179.90Min. 2 days
- ESCO 0- 120 ℃ / 0-0.6MPa / Φ110mm Water height meter (Horizontal type)Esco Part No. EA729PA-5from S$159.90Min. 2 days
- Mitsubishi Electric Parameter unit with battery packA parameter unit that allows parameter setting without connecting a power supply to the inverter.from S$459.90Min. 2 days
- Hitachi Industrial Equipment Systems Input side radio noise filter (capacitor filter)It connects directly to the power supply terminal of the inverter to reduce the radiated noise emitted from the electric wire. Reduces radio interference to radios and televisions.from S$97.99Min. 7 days
- Hitachi Industrial Equipment Systems Braking resistor Small typeMass (kg) 0.27 Rated Capacity (W) 120from S$199.90Min. 7 days
- Hitachi Industrial Equipment Systems DC reactor (for harmonic suppression, power coordination, power factor improvement)Suppresses the harmonics generated on the inverter input side. It also helps improve power factor.from S$299.90Min. 7 days
- ESCO 0-120 ℃ / 0-0.3MPa / Φ88mm Water height gauge (Horizontal type)Esco Part No. EA729PA-1from S$149.90Min. 6 days
- Hitachi Industrial Equipment Systems Radio noise filter (zero-phase reactor)Installed on the input side and output side of the inverter to reduce the radiation noise emitted from the electric wire. It reduces radio interference to radios and TVs, and prevents malfunctions of measuring instruments and sensors.from S$119.90Min. 7 days
- FLON CHEMICAL Fluorine resin level gauge B type NR0177 seriesIt is a liquid level gauge made of all fluororesin. Has excellent chemical resistance and heat resistance. Since the pipe uses PFA pipe, it is visible. There is no need to worry about breaking like a glass tube.from S$469.90Min. 16 days
- Mitsubishi Electric Inverter Option Mounting Compatible Attachment FR-A5AT SeriesMounting Compatible Panel 1from S$64.99Min. 104 days
- ESCO 0-120 ℃ / 0-0.3MPa / Φ110mm Water height meter (Horizontal type)Esco Part No. EA729PA-4from S$159.90Min. 6 days
- Fuji Electric Option for single-phase 100V inputPower Supply 3-phase 200Vfrom S$97.99Min. 10 days
- OMRON SYSDRIVE inverter JX series / MX series / RX series Digital operatorSuitable Model SYSDRIVE JX / MX / RX seriesfrom S$89.99Min. 6 days
- ESCO 0- 120 ℃ / 0-0.6MPa / Φ162mm Water height gauge (Horizontal type)Esco Part No. EA729PA-8
- Hitachi Industrial Equipment Systems Braking resistor Medium capacity typefrom S$539.90Min. 7 days
- Watty Water Level Sensor Float Type HL Series for Water / Chemical Solution Detectionfrom S$119.90Min. 13 days
- Toshiba Schneider Inverter Input ReactorThe input reactor is used to improve the input power factor on the inverter power supply side, reduce harmonics, or suppress external surges. Installed when the power supply capacity is 500 kVA (Note) or more and the power supply capacity is 10 times or more the inverter capacity, or when a disto... Read Morefrom S$199.90Min. 9 days
- Mitsubishi Electric Inverter Option Dedicated Separate Reactor FR-XCL Seriesfrom S$299.90Min. 49 days