All Category

Synthetic Slings

A fiber sling is a fiber sling that is used to hang heavy objects on a crane. Mainly made of polyester or nylon, it is more flexible than metal wire slings, and is suitable for slinging transported objects that do not like scratches such as wood, plastic, copper, aluminum products, and machine parts. Choose an appropriate sling according to the items to be transported, and store the sling in a place where it will not be affected by heat or chemicals. In addition, it is important to observe the degree of wear firmly and strive for maintenance safety.
View : Grid List
Filter

Items 1 - 40 of 722

Set Ascending Direction
  1. Sling Belt Z Type (JIS4 Grade, Both Ends Eye Type)
    Tamura Sogyo Sling Belt Z Type (JIS4 Grade, Both Ends Eye Type)
    A strong belt sling of JIS highest grade (4th grade). Using strong polyester yarn, it has excellent features such as tensile strength, durability, abrasion resistance, and low elongation. There is a white core thread inside, making it easy to understand the disposal standard when the belt is worn... Read More
    Type  Eye shape on both ends  Accuracy Grade  JIS Class 4  Material  Polyester 
    Rating:
    97%
    from S$26.99
    Min. 2 days
  2. AQ sling ⅣE (4 grade, both ends eye type)
    Houshou AQ sling ⅣE (4 grade, both ends eye type)
    Workability is outstanding with the twill weaving method that is particular about softness. It is thick and has excellent durability. Entering a limit display line that shows the timing of disposal. The belts are color-coded according to the maximum working load for easy management. Slinging work... Read More
    Accuracy Grade  4th grade  Belt Thickness (mm)  9~10  Type  Both ends eye type  Specification  JIS+B+8818+4 grade equivalent product  Material  Polyester 
    from S$25.99
    Min. 4 days
  3. Polyester Sling
    MonotaRO Polyester Sling
    Since it uses polyester yarn, it is a sling that is strong in tensile strength and elongation. It is a product-friendly sling that does not easily get peculiar even when bent. Ideal for slinging products that do not like scratches on wire slings such as copper, aluminum, plastic, and wood product... Read More
    Type  Eye shape on both ends  Material  Polyester 
    Rating:
    88%
    from S$13.99
    Min. 2 days
  4. Sling Belt (JIS3 Grade, Both Ends Eye Type)
    TRUSCO Sling Belt (JIS3 Grade, Both Ends Eye Type)
    Moderate elongation softens the impact. The green side (used side) and the orange side (outer side) are color-coded. (Due to the structure of the belt sling, the durability differs between the green surface (used surface) and the orange surface (outer surface), so use it correctly on the green su... Read More
    Eye Thickness (mm)  Type  Eye shape on both ends  Accuracy Grade  JIS3 grade  Material  Nylon (inside: polyester)  Operating Temperature (℃)  under 100 
    Rating:
    87%
    from S$25.99
    Min. 2 days
  5. Blue sling (JIS3 grade, both ends eye shape)
    TESAC Blue sling (JIS3 grade, both ends eye shape)
    Polyester absorbs almost no water and has good light resistance, making it an ideal material for outdoor use. In order to eliminate the difficulty of understanding the apparent dimensions, we have separated the design for each size. This keeps things organized and makes inventory management easie... Read More
    Color  Blue  Type  Eye shape on both ends  JIS Standard  JIS B 8818 standard product  Operating Temperature (℃)  under 100 
    Rating:
    94%
    from S$299.90
    Min. 2 days
  6. Polyester sling light JIS1 grade, both ends eye shape
    Maruzen Orimono Polyester sling light JIS1 grade, both ends eye shape
    Since it uses tough synthetic fibers, it has excellent tensile strength, durability, weather resistance, and antiseptic properties. There is a usage limit sign that shows the guideline for disposal at a glance. For general slinging work.
    Belt Thickness (mm)  Type  Eye shape on both ends  JIS Standard  JIS B 8818 standard product  Specification  JIS B 8818 standard product  Accuracy Grade  JIS1 grade  Material  Polyester  Operating Temperature (℃)  under 100 
    Rating:
    97%
    from S$13.99
    Min. 2 days
  7. Sling Soft type Endless
    MonotaRO Sling Soft type Endless
    A soft type sling whose surface is covered with nylon. As it is a flexible soft type, it is easy to fit various suspended loads. In addition, it is a lightweight and easy-to-use product that is less prone to habits than wires even when bent. For steel, stone, landscaping, wooden products, etc. * ... Read More
    Belt Width (mm)  40  Belt Thickness (mm)  Type  Endless 
    Rating:
    93%
    from S$13.99
    Min. 2 days
  8. Tough Sling P Type (Both Ends Eye Type)
    Tamura Sogyo Tough Sling P Type (Both Ends Eye Type)
    Light, easy to bend and easy to handle, it improves the efficiency of slinging work. Using strong polyester yarn, it has excellent features such as tensile strength, durability and abrasion resistance, and low elongation. The length and width are easy to understand by color-coding the eye part an... Read More
    Material  Polyester 
    Rating:
    92%
    from S$26.99
    Min. 2 days
  9. Round sling (JIS standard product, endless type)
    TRUSCO Round sling (JIS standard product, endless type)
    A sling with a structure in which a bundle of strong polyester yarn is wrapped with a surface cloth made of nylon, which has excellent wear resistance. It is flexible and fits gently on any suspended load. In addition, it fits well and has excellent load stability. Even if it is bent, it does not... Read More
    Type  Endless  JIS Standard  JIS B 8811 standard product 
    Rating:
    97%
    from S$23.99
    Min. 2 days
  10. Power sling KP-1 type (JIS ⅢE type)
    KONDOTEC Power sling KP-1 type (JIS ⅢE type)
    Install an eye on the end of the sling. The most versatile type. The eyes are sewn to protect them, and hooks can be easily attached and detached. It has a built-in safety line that tells you when to replace it. Since the date of use is attached to the inner side of the sewn part of the eye, plea... Read More
    RoHS directive (corresponding to 10 substances)  Correspondence  Accuracy Grade  JIS3 grade 
    Rating:
    84%
    from S$23.99
    Min. 2 days
  11. Inca round sling endless type (HN)
    Taiyo Seiki Iron Works Inca round sling endless type (HN)
    The "Inca Round Sling" is a soft sling in which fibers are bundled and covered with a surface cloth. Since it is a light and soft material, it fits flexibly into objects that are difficult to hang, and you can use it with confidence without damaging the suspended load. Inca round slings... Read More
    RoHS directive (corresponding to 10 substances)  Correspondence  Type  Endless  Material  Super high-strength polyester yarn 
    Rating:
    82%
    from S$97.99
    Min. 7 days
  12. Reinforcing pad (magic tape removable type)
    TESAC Reinforcing pad (magic tape removable type)
    With Velcro, it can be easily attached anywhere. For angular products, we recommend using a corner pad.
    RoHS directive (corresponding to 10 substances)  Correspondence 
    Rating:
    80%
    from S$12.99
    Min. 2 days
  13. Lock Sling "Sigma" A-1 JIS4 Grade, Both Ends Eye Type
    Meidai Lock Sling "Sigma" A-1 JIS4 Grade, Both Ends Eye Type
    3-layer structure. 6 layers of strong construction with 2 layers of 3-ply woven belts, even if one layer on the surface wears out, the remaining layers can ensure safe strength. Usage limit marking. Warning signs are indicated by white core threads in both the thickness and width directions. Beca... Read More
    Material  100% polyester  Type  Eye shape on both ends  Specification  JIS B 8818 4 grade  JIS Standard  JIS B 8818 standard product  Accuracy Grade  JIS Class 4 
    Rating:
    100%
    from S$26.99
    Min. 2 days
  14. 4-point hanging sling
    O.H. Industrial 4-point hanging sling
    A 4-point hanging sling that uses a belt sling for the forged ring. * Do not use at a suspension angle of 120 ° or more. It is recommended to use within 60 °. * The maximum working load shown is the value when the suspension angle is 0 °.
    Belt Color  Blue  Type  Forging safety  Material (Catch)  S45C  Specification  With safety lever (hook) 
    Rating:
    67%
    from S$379.90
    Min. 2 days
  15. Bluesling software E type (both-eye type)
    TESAC Bluesling software E type (both-eye type)
    RoHS directive (corresponding to 10 substances)  Correspondence  Type  Eye shape on both ends 
    Rating:
    91%
    from S$25.99
    Min. 2 days
  16. Corner Pads for Belt Sling (Cylindrical Type)
    TRUSCO Corner Pads for Belt Sling (Cylindrical Type)
    Since it is a tubular belt, it can be passed through afterwards. For protecting the belt sling when lifting angular luggage * If a suspended load with an edge slides sideways, the effect of the corner pad may be almost eliminated.
    Type  Tubular 
    Rating:
    60%
    from S$9.59
    Min. 2 days
  17. Corner pad with velcro (magic tape removable type)
    TRUSCO Corner pad with velcro (magic tape removable type)
    Since it can be removed with Velcro, it can be installed in any position immediately. For protecting the belt sling when lifting angular luggage. * If a suspended load with an edge slides sideways, the effect of the reinforcing cylinder may be almost lost.
    Material  Belt: nylon  Type  Made by magic 
    Rating:
    92%
    from S$22.99
    Min. 2 days
  18. Belt sling / NBⅢE
    O.H. Industrial Belt sling / NBⅢE
    JIS B 8818 Ⅲ grade (eye type on both ends) A belt woven with polyester yarn is sewn into a three-layer structure. Slinging work
    Belt Color  Blue  Belt-End Finish  Eye sewing  JIS Standard  JIS B 8818 standard product  Accuracy Grade  JIS3 grade  Material (Belt)  Polyester 
    Rating:
    97%
    from S$26.99
    Min. 2 days
  19. Wide Soft Sling
    TRUSCO Wide Soft Sling
    Wide type of soft sling Flat like a belt sling, gentle on products, and soft like a soft sling. It has excellent tensile strength and durability, and is a durable specification. Since it is wider than the belt sling with the same suspension load, the contact area with the suspended load is wider,... Read More
    Belt Thickness (mm)  Type  Eye shape on both ends 
    Rating:
    100%
    from S$27.99
    Min. 2 days
  20. Round sling RE type
    KITO Round sling RE type
    An endless sling in which a strong polyester yarn wire is covered with a rope-shaped spring and a protective sheet. Since it is a flexible rope, it fits freely in a wide range of packaging, has less slippage, and has excellent load stability. The strength is held by the core thread, and if the ou... Read More
    Type  Endless 
    Rating:
    60%
    from S$34.99
    Min. 2 days
  21. Batter cylinder type
    Tamura Sogyo Batter cylinder type
    A friction-resistant nylon pad. Belt protection when safely hanging objects with sharp corners or rough surfaces.
    Material  Nylon  Type  Tubular 
    Rating:
    60%
    from S$12.99
    Min. 2 days
  22. Mysterious belt
    Matsuura Industry Mysterious belt
    You can easily move large items such as furniture and refrigerators in the office or at home. For rearranging furniture and archives
    Load capacity (N)  (Maximum recommended pair) 3430 
    Rating:
    100%
    from S$65.99
    Min. 2 days
  23. Blue sling soft N type (endless type)
    TESAC Blue sling soft N type (endless type)
    Scratches and load slippage are less likely to occur. Since the colors are separated according to the load, you can easily select the sling according to the suspended load. If the outer cloth is torn and the white core thread inside is visible, it is the limit of use, so replace it immediately. P... Read More
    Material  Cloth: Nylon / Core: Polyester  RoHS directive (corresponding to 10 substances)  Correspondence  Type  Endless 
    Rating:
    100%
    from S$48.99
    Min. 2 days
  24. Both ends eye type sling belt 50mm width (Ⅲ grade JIS standard product)
    allsafe Both ends eye type sling belt 50mm width (Ⅲ grade JIS standard product)
    Since the original fabric of the sling belt has a "three-layer structure", it has achieved strength and safety. The raw thread uses ultra-high cooperation polyester, which is most suitable for fiber slings, and combined with our unique sewing processing technology, it has improved tensi... Read More
    Maximum Working Load (t)  1.6  Belt Width (mm)  50  Belt Thickness (mm)  Type  Eye shape on both ends  Material  Super high strength polyester 
    from S$49.99
    Min. 2 days
  25. Inca Lifting Sling JIS
    Taiyo Seiki Iron Works Inca Lifting Sling JIS
    Since it is made of fiber, it can be used in a wide range of work sites such as lifting work for those who dislike scratches, slinging work for general heavy objects, and horizontal pulling work for loads. Belt sling for general sling work. * Please use below the working load. * Since it is a tex... Read More
    Type  Eye shape on both ends 
    Rating:
    93%
    from S$38.99
    Min. 2 days
  26. Belt Sling BSL Type (III Grade)
    KITO Belt Sling BSL Type (III Grade)
    A belt sling with a moderate width and extremely high stability. Since the eye parts on both ends are squeezed, slinging work is easy. Moreover, because it is covered with a protective sheet, it has excellent durability. Comes with a limit sign that shows the usage limit. The red core thread is w... Read More
    Type  Eye shape on both ends  JIS Standard  JISB8818  Color  Light green  Material  Polyester 
    Rating:
    92%
    from S$299.90
    Min. 13 days
  27. Sling Rope, 500kg
    TRUSCO Sling Rope, 500kg
    Uses tough polyester yarn as the core yarn Since burrs do not appear like wires, the eye part and the main body, which are easy on the hands, are integrated, so the eye part does not come off. Will not hurt Painted products that are troublesome when lifting and lowering pipes and steel pipes * Fo... Read More
    Operating Load (ton)  0.5  Breaking Load  3.2t  Operating Load (kg)  500:(TRS5-15~-40) 800:(TRS8-15~-40)  Type  Eye shape on both ends 
    Rating:
    87%
    from S$29.99
    Min. 2 days
  28. Polyester Sling
    KITO Polyester Sling
    A belt sling with an appropriate width and extremely high stability. Since the eye parts on both ends are squeezed (depending on the size of the belt), slinging work is easy. Moreover, because it is covered with a protective cloth, it has excellent durability. If you see the red limit sign, it is... Read More
    Belt Thickness (mm)  Color  Light green  Material  Polyester 
    from S$23.99
    Min. 2 days
  29. 2-Point Libert Sling
    O.H. Industrial 2-Point Libert Sling
    A two-point hanging sling that uses a belt sling for the forged ring.
    Belt Color  Blue  Type  Forging safety 
    from S$199.90
    Min. 2 days
  30. Protection corner
    KITO Protection corner
    Use the protective corner to protect the sling and prevent side slip in the case of a slanted load or a suspended load with a rough surface. Various types are available according to the model and size, so you can choose according to the sling.
    Thickness (mm)  5.8 (when two sheets are stacked) 
    from S$9.59
    Min. 2 days
  31. Sling Rope, 800kg
    TRUSCO Sling Rope, 800kg
    Uses tough polyester yarn as the core yarn Since burrs do not appear like wires, the eye part and the main body, which are easy on the hands, are integrated, so the eye part does not come off. Will not hurt * For items with corners, use a corner pad such as a reinforcing pad.
    Operating Load (ton)  0.8  Breaking Load  5.0t  Type  Eye shape on both ends 
    Rating:
    100%
    from S$36.99
    Min. 2 days
  32. Polypower EC-2 type
    H.H.H. Mfg. Polypower EC-2 type
    The cores are connected. The endlessly wound core bears the weight, and even if it is thin, it is strong. It can be used at intervals between wire ropes, and there is no risk of injury due to twisting or strands. If you see the blue sign, replace it. * Length refers to the length of folding in half.
    Rating:
    80%
    from S$39.99
    Min. 2 days
  33. Belt sling Ⅲ E type
    H.H.H. Mfg. Belt sling Ⅲ E type
    Made of super strong polyester yarn, it has excellent durability. Abrasion resistance is improved by special resin processing. Elongation is reduced by the material and weaving method. * There is a white thread in the core. Stop using when you see the white thread.
    Type  Eye shape on both ends  Material  Polyester 
    from S$29.99
    Min. 2 days
  34. Safety Power Rope, 6mm
    TRUSCO Safety Power Rope, 6mm
    The main material, Dyneema SK-60, is the lightest ultra-high-strength, high-elasticity fiber of all high-performance fibers. It is an advanced material with excellent UV resistance and chemical stability in addition to excellent mechanical properties. The main material, Dyneema SK-60, is light en... Read More
    Rope Diameter (Φmm)  Type  Eye shape on both ends 
    Rating:
    100%
    from S$59.99
    Min. 2 days
  35. Nylon soft sling
    ESCO Nylon soft sling
    Supple and gentler design than belts. Softer than conventional belts, it is supple and fits perfectly on suspended objects. It is difficult to place scratches and slippage. Colors are separated according to load. Please choose the sling according to the suspended load. Also, if you can see the wh... Read More
    Type  Eye shape on both ends  Material  Nylon 
    from S$44.99
    Min. 2 days
  36. Belt sling / NBⅢE
    O.H. Industrial Belt sling / NBⅢE
    This sling is a JIS8818ⅢE (eye type on both ends) general-purpose type, and is the JISⅢ grade with the largest working load when a belt woven with polyester yarn is sewn in three layers. The belt is a little softer than Apix IIIE. Know the usage limit, Safe with a signal !! * If you can see the w... Read More
    Rating:
    100%
    from S$23.99
    Min. 2 days
  37. Polyester Sling Belt Sling BSH Type
    KITO Polyester Sling Belt Sling BSH Type
    A moderately wide belt sling with extremely high safety. Slinging work is easy. Because it is covered with a protective cloth, it is extremely durable. *When the red limit sign is visible, the usage limit is reached.
    Belt Thickness (mm)  Type  Eye shape on both ends  Standard  JIS B 8818  Accuracy Grade  JIS IV grade  Color  Light green  Material  Polyester 
    from S$85.99
    Min. 18 days
  38. Rock sling Belt sling Corner pad (through 1) E type Tubular
    Meidai Rock sling Belt sling Corner pad (through 1) E type Tubular
    A corner pad for belt slings that is resistant to friction due to special resin processing. If the white thread is exposed due to fraying, change the position of the contact surface before use. * Usable temperature 100 ° C or less * Not for chemical resistance. * Please be sure to use it for angu... Read More
    Material  100% polyester  Overall Length (mm)  500  Type  Tubular 
    from S$17.99
    Min. 2 days
  39. A sling belt
    TOYO SAFETY A sling belt
    Both ends ring type (with a tough protective sheet on the hanging part) The material is super strong polyester fiber. It has little elasticity and can work stably even on heavy objects. A danger signal if cracks or wear occur up to the black lines at both ends that indicate the limit of use. * Fo... Read More
    Accuracy Grade  JIS3 grade 
    from S$32.99
    Min. 4 days
  40. Sling Belt, Polyester
    TRUSCO Sling Belt, Polyester
    Excellent dimensional stability due to low elongation. Since the sewing on one side is double, it is soft and ideal for hanging chalk. Since it uses tough synthetic fibers, it has excellent tensile strength, durability, weather resistance, and antiseptic properties. Surface-processed steel materi... Read More
    Maximum Working Load (t)  0.8  Eye dimensions (mm)  210  Belt Width (mm)  25  Belt Thickness (mm)  Type  Eye shape on both ends  JIS Standard  JIS B 8818 standard product  Material  Polyester 
    Rating:
    80%
    from S$26.99
    Min. 2 days
View : Grid List
Filter

Items 1 - 40 of 722

Set Ascending Direction