Non-Packaged
Other Related Pages
- MonotaRO Genroku Disposable Chopsticks 100 Sets Non-PackagedIt is the most common and cheap split chopstick that is easy to split because it has a groove in the split. Using Vietnamese afforestation material (MO material), it is stronger than aspen material and is easy to crack. In addition, the surface is also characterized by having few stains and strea... Read MoreMaterial Reforestation materials (MO materials) Mass (g) 410 Type Genroku Accuracy Grade Class 1-2
- MonotaRO 100 bamboo cut chopsticks nakedThe top of the split chopsticks (handle side) is cut diagonally. High-quality chopsticks often used for restaurants and hospitality. Because it is made of bamboo, it has strong strength and has the property of repelling oil. * Bamboo may smell when opened, but there is no problem with the quality... Read MoreMaterial bamboo Mass (g) 550 Type Natural cutting
- Daiwa Bussan Soot bamboo chopsticksDisposable chopsticks with plenty of 100 sets. Also for business use. Please be assured that disposable chopsticks do not contain antifungal agents (OPP, TBZ, DP, imazalil, etc.) and chlorine bleach.Material bamboo Type Natural chopsticks
- TORADA Japanese chopsticksThe chopsticks are divided into one and have a high-class feel. Each set has a white band at the center, making it ideal for a little hospitality.Specification With poly Material bamboo Type Egg chopsticks
- Daiwa Bussan Four Season Shirasagi Genroku Chopsticks (Nude)Chamfered corners that are strong and hard to break, making it easy to holdMaterial Birch Type Genroku chopsticksfrom S$7.69Min. 2 days
- Meikai Aspen MarshalMaterial Aspen Size 8 inch Type Genroku chopsticks
- HEIKO Aspen Marshal Chopsticks 500Value-added soft and light material For business use such as cafeteriasMaterial Aspen Type Genroku chopsticks
- MASUKI Japanese chopsticksIt is a common type of split chopstick with the largest distribution volume. It is a great value pack with roses, so it is ideal not only for business use but also for everyday use. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Pleas... Read MoreMaterial White Yang Type Genroku chopsticks
- Daiwa Bussan ECO plantation material chopsticks (bare)Material Natural wood Type Genroku chopsticks
- MASUKI Bamboo Chopsticks Carbonized BrownCompared to ordinary bamboo chopsticks, it has a luxurious feel. No chemicals such as fungicides, insect repellents and bleaches are used. It has a smoked scent. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery... Read MoreMaterial bamboo Type Natural chopsticksfrom S$8.19Min. 2 days
- Daiwa Bussan With knot Bamboo tempura chopsticksHard to break and breaks cleanlyMaterial Bamboo Type Natural chopsticksfrom S$2.99Min. 2 days
- ASTEP Disposable chopsticks Bamboo Tenka Naked TaperedIt is a standard disposable chopstick for events and food stalls.Material bamboo Type Natural chopsticksfrom S$13.99Min. 2 days
- MASUKI Japanese chopsticksIt is a common type of split chopstick with the largest distribution volume. It is a great value pack with roses, so it is ideal not only for business use but also for everyday use. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Pleas... Read MoreMaterial Birch Type Genroku chopsticks
- YANAGI PRODUCTS 100cm bamboo chopsticksIt is a split chopstick with the upper part cut diagonally. It is a great value pack with roses, so it is ideal for business use and everyday use. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be pos... Read MoreMaterial bamboo Type Natural chopsticksfrom S$6.49Min. 2 days
- MASUKI Disposable Chopsticks Hakuyo Genroku Tensoge(Diagonal Cut) 8 InchIt is a split chopstick with the upper part cut diagonally. It is a great value pack with roses, so it is ideal for business use and everyday use. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be pos... Read MoreMaterial White Yangfrom S$11.99Min. 2 days
- YANAGI PRODUCTS ChopsticksIt is a split chopstick with thin ends. It is a great value pack with roses, so it is ideal for business use and everyday use. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no... Read MoreMaterial bamboo Type Rikyu chopsticksfrom S$6.79Min. 5 days
- Daikoku Industry Sugi Sugi Tenka chopsticksMaterial Cedar Size 9 inch Type Natural chopsticksfrom S$19.99Min. 7 days
- YANAGI PRODUCTS 100 bamboo chopsticksIt is a split chopstick with a square upper part. It is a great value pack with roses, so it is ideal for business use and everyday use. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if t... Read MoreMaterial bamboo Type Twin chopsticksfrom S$6.49Min. 5 days
- Daiwa Bussan Environmentally friendly chopsticks Bamboo poly shutout chopsticksSpecification Knotted, 1 square chopstick Material Bamboofrom S$1.99Min. 6 days
- ESCO 210mm Bamboo chopsticks (100 sets)Material bamboo Mass (g) (Per kite) 7.3from S$8.89Min. 3 days
- Shinwa Cypress Chopsticks (Nude) Yoshino's Cypress ChopsticksDisposable chopsticks made from thinned cypress wood from Yoshino. A top-cut type that is ideal for hospitality.Material Natural wood Type Natural chopsticksfrom S$3.39Min. 6 days
- PackStyle PS 8 Sunn Chopstick 4.2 Navy Blue New2 to 3 grade mixed ・ White and good-looking chopsticks. Thickness: 4.2mmMaterial Birch wood Type Genroku chopsticksfrom S$149.90Min. 5 days
- PackStyle PS Shiraki Margin 8 inch 4.5 Thick Black New1st and 2nd grade mixed ・ You are fully satisfied with the thickness and material. Thickness: 4.5mmMaterial Aspen Type Genroku chopsticksfrom S$189.90Min. 5 days
- EBM Discount chopsticks white aspenType Genroku chopsticks Material Aspen maker part number 5582020from S$339.90Min. 4 days
- EBM Japanese chopsticks bamboo soup AMaterial bamboo Type Twin chopsticksfrom S$249.90Min. 4 days
- Daiwa Bussan Disposable Spoon 100 Pieces for Business UseDisposable type.Material polystyrene RoHS directive (corresponding to 10 substances) Correspondencefrom S$9.79Min. 2 days
- Daiwa Bussan Soot Bamboo Tenka Chopsticks (Unwrapped) 100 SetsHigh-class chopsticks made from smoked bamboo.Material bamboo Type Natural chopsticks RoHS directive (corresponding to 10 substances) Correspondence
- Daiwa Bussan Business Prosperity Fork 100 pcsFor food courts, food stalls, events, camping, outdoor activities, etc.Material polystyrene RoHS directive (corresponding to 10 substances) Correspondencefrom S$9.79Min. 10 days
- Daiwa Bussan Prosperous business + Genroku chopsticks (naked) 200 setsChopsticks that are strong and hard to break, suitable for everyday use.Material Birch Type Genroku chopsticks RoHS directive (corresponding to 10 substances) Correspondencefrom S$15.99Min. 9 days
- SHIMOJIMA Chopsticks Aspen GenrokuIt is a standard disposable chopstick for events and food stalls.Material Aspen Type Genroku chopsticks Manufacturer Product Code 004636302
- Daiwa Bussan Green Select Knotted Bamboo Chopsticks NakedDurable bamboo disposable chopsticks We use fast-growing bamboo. Knots are also used effectively. We use managed forest resources. (FSC certified) *Store in a dry place. Depending on the storage location, bamboo may become moldy. *Please be aware that when chopsticks are broken, hangnails may rem... Read MoreMaterial bamboo Type Natural chopsticks FSC-certified Authentication FSC certification number C154418from S$4.99Min. 9 days