An oil-resistant bag that is just the right size to hold one side dish such as French fries, croquettes, and minced meat cutlets. Please use it for eating at side dishes such as supermarkets, local festivals and events, and sightseeing spots. Machi: 35mm when unfolded
Due to the use of strong oil and water resistant paper, it will not seep out even if fried food or other oily food is added. It can be used for a wide range of purposes such as tempura, croquettes, side dishes, oil confectionery, french fries, bread, and others.
An oil-resistant bag that is just the right size to hold one side dish such as French fries, croquettes, and minced meat cutlets. Please use it for eating at side dishes such as supermarkets, local festivals and events, and sightseeing spots.
Color Plain Size S Manufacturer Product Code 004162100
Due to the use of strong oil and water resistant paper, it will not seep out even if fried food or other oily food is added. It can be used for a wide range of purposes such as tempura, croquettes, side dishes, oil confectionery, french fries, bread, and others.
Perfect for fried chicken, croquettes, tempura, donuts, french fries, fried chicken, etc.! It is a size and shape that you can easily eat a small amount. Since it uses oil-resistant and water-resistant paper, it can handle oil-resistant materials.
* Products shipped directly from the manufacturer... Read More
Absorbs excess oil with oil resistant paper. Even if you put heated food in it, steam will pass through it, so it will not be sticky due to moisture.
For donuts, croquettes, potatoes, fried bread, fried chicken, etc.
It is a convenient cup that can be used as a lid when you put chicken and potatoes that are very active in various events such as cultural festivals, bazaars, festivals, and fairs. You can purchase it in units of 50, so it is also recommended for people related to restaurants.
Since it uses oil-resistant and water-resistant paper, it can handle oil-resistant materials. It is a size and shape that you can easily eat a small amount. By putting gussets on both sides and cutting out the upper part of the front of the bag in a round shape, the contents are easy to put in an... Read More
Roasted sweet potato for roasted sweet potato Roasted sweet potato pack bag paper
If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery loca... Read More
An oil resistant bag for french fries. It can be used for eating at side dishes such as supermarkets, local festivals and events, and sightseeing spots. An oil-resistant bag that is just the right size to hold one side dish such as croquette and minced meat cutlet in addition to french fries. The... Read More
Material Oil resistant Basis Weight (g/m2) 50 RoHS directive (corresponding to 10 substances) Correspondence
A cup-type snack carton for potatoes, chicken, popcorn, etc. You can also make a square type by folding the four fold lines on the inside. There is a cut on the back of the body where you can insert a pick. Inner oil resistant finish (because it is made of paper, oil may bleed). No microwave