Glass Cups
Other Related Pages
- CAPTAIN STAG Double Stainless Barrel Type Mega JugsMaterial stainless steel Capacity (L) 1.0 product name/ type Beergrass
- M-CONS Plastic Silver Wine (Stacking)Plastic silver cup series stackableproduct name/ type wine glassfrom S$8.39Min. 2 days
- Libbey Libbey Chicago Tall Highball GlassLibby Tumbler & Barwear CHICAGO Chicago SeriesTypes of tableware Western tablewarefrom S$44.99Min. 2 days
- ADERIA Craft Beer GlassesBeer glass series where you can fully enjoy the taste of craft beer.Material Full surface ion tempered glass product name/ type Shot glassfrom S$11.99Min. 2 days
- HARIO Twin rock glassA double glass. Hard to condense. The mouthpiece is made of a single layer, so it is easy to drink.Type For hot water Material Heat resistant glass Opening Diameter (Φmm) 82 product name/ type Shot glass Types of tableware Western tablewarefrom S$29.99Min. 11 days
- ADERIA SON.hyx crystal glass Snifter 170 C372Opening Diameter (Φmm) 43 Maximum Diameter (Φmm) 70from S$119.90Min. 29 days
- Libbey Libbey Stemless Red Wine GlassLibby Stemware STEMLESS Stemless SeriesDiameter (Φmm) 98 product name/ type wine glass
- TKG MLV diamond glassThe brilliance of the multi-sided cut creates a sense of luxury. Make your drink more luxurious.Material High grade polycarbonate product name/ type Rock glass Heat Resistance Temperature (℃) -30~110 Dishwasher Commercial or home use
- ADERIA Craft Beer Master RichOpening Diameter (Φmm) 69 product name/ type Shot glassfrom S$13.99Min. 3 days
- Schott Zwiesel Finesse Champagne EP 298ccA series with beautiful stems of pulling legs that extend in a flowing manner. A slightly warped line from the bottom creates convection and brings out the aromas of various wines.Material Glass Maximum Diameter (Φmm) 75 product name/ type Champagne glassfrom S$229.90Min. 7 days
- Toyo-Sasaki Glass San Ace on the RockSpecification Oral physical enhancement Material Soda-lime glass product name/ type Shot glassfrom S$48.99Min. 7 days
- Schott Zwiesel Banquet Spirits 75ccThe strongest class in the world. Strong impact and scratches, and shine continues. As a reliable product with design and functionality, it is used in hotels and restaurants in more than 120 countries around the world.Material Glass Maximum Diameter (Φmm) 47 product name/ type Rock glassfrom S$86.99Min. 6 days
- ARC Openup EphevancentA new world opens up in the "magic curve" wine tasting where the fusion wine of material and design, selected to master the color, aroma and taste, smiles. State-of-the-art new material Kwarx. Kwarx. Absolute transparency Kwarx. (Kwarx.) Represents the original color of the wine inside,... Read MoreMaterial Crooks Diameter (Φmm) 72 product name/ type Shot glassfrom S$199.90Min. 3 days
- BORMIOLI LUIGI Atelier stemless whiteAtelier series Made in Italyproduct name/ type Shot glassfrom S$87.99Min. 3 days
- Toyo-Sasaki Glass Authentic Shochu Dora Ekubo on the RockSpecification Oral physical enhancement Material Soda-lime glass product name/ type Shot glassfrom S$76.99Min. 7 days
- ADERIA H / AX Coolel High Coolel 38Specification Oral physical enhancement Opening Diameter (Φmm) 64 Maximum Diameter (Φmm) 64from S$33.99Min. 6 days
- BODUM Bodam Assam Tea Glass SetMaterial Heat resistant glass / stainless steel product name/ type Shot glass Types of tableware Western tablewarefrom S$56.99Min. 3 days
- COCORO White mat Fuchiuchi gold-coated saddle-type via (large)product name/ type Shot glassfrom S$48.99Min. 3 days
- Schott Zwiesel Pure RieslingFeaturing a strikingly beautiful bowl line, the Pure series unleashes its abilities by swirling. This series is recommended as a glass that allows you to feel the aroma and bouquet in a well-balanced manner. We have 9 types of glass lines, so you can enjoy all types of wine and enjoy the variatio... Read MoreSeries pure Maximum Diameter (Φmm) 76 product name/ type Shot glassfrom S$229.90Min. 7 days
- Lehmann Glass Lehmann LalmanGlasses for wine by wine professionals. Founded in the Lehmann Champagne region, the glass brand Enomast series Oenology + Must (required) with the experience and knowledge of sommeliers and chefs. It was named the glass that is indispensable for tasting wine. It is an ideal form that has been ca... Read Moreproduct name/ type Shot glassfrom S$299.90Min. 3 days
- Toyo-Sasaki Glass Thin ice thin on the rockSpecification Full ion reinforcement Material Soda-lime glass product name/ type Shot glassfrom S$76.99Min. 7 days
- ADERIA Mini Glass W WhiskeyOpening Diameter (Φmm) 49 Maximum Diameter (Φmm) 49 product name/ type Shot glass
- SALUS Sato Kinzoku Kogyo Picardy TumblerMaterial Heat-resistant tempered glass
- ADERIA AX Spada SpadaA standard item of water glass. Since it can be stacked, it can be stored compactly.Specification Oral physical enhancement Opening Diameter (Φmm) 68 Maximum Diameter (Φmm) 68 Function Stackable Types of tableware Western tableware
- Libbey Libbey Perception Wine GlassLibby Stemware PERCEPTION Perception Series The bowl and stem are integrally molded in a one-piece structure. It is strong against impact and has excellent durability compared to general stemware. There is almost no damage due to twisting that tends to occur during cleaning.product name/ type wine glassfrom S$59.99Min. 2 days
- HARIO Heat-resistant Hot GlassHot glass made of heat-resistant glass. Easy to use with a simple design. You can reheat it in the microwave.Type For microwave oven Material Heat resistant glass Types of tableware Western tableware
- ADERIA Ulster Old 8A long-selling product manufactured since 1968. A beautiful tumbler with a strong cut-like design.Opening Diameter (Φmm) 79 Maximum Diameter (Φmm) 79from S$26.99Min. 2 days
- Libbey Libbey Embassy Poco Grande GlassLibby Stemware EMBASSY Embassy Series The bowl and stem are integrally molded in a one-piece structure. It is strong against impact and has excellent durability compared to general stemware. There is almost no damage due to twisting that tends to occur during cleaning.Color Clear Types of tableware Western tableware
- Libbey Libbey Chicago Old Fashioned GlassLibby Tumbler & Barwear CHICAGO Chicago Seriesproduct name/ type Shot glass Types of tableware Western tablewarefrom S$39.99Min. 2 days
- INAO INAO Tasting GlassA glass for wine professionals certified by INAO to taste a variety of wines of different varieties and origins under the same conditions. The definition of INAO glass is that it has legs and is tulip-shaped in a bowl with a capacity of 5 to 8 ounces. It is easy to swirl and has a shape that allo... Read MoreMaterial Non Red Crystal Maximum Diameter (Φmm) 67 product name/ type Shot glass
- TKG JB polycarbonate champagne fluteLighter than glass. Mainly for champagne, wine, etc.Material Polycarbonate product name/ type Champagne glass Heat Resistance Temperature (℃) 100from S$7.89Min. 2 days
- Bormioli Rocco New calix oldBormioli Rocco The history of Bormioli Rocco is the history of glass. Since the establishment of the first factory in Parma in 1825, we have always incorporated innovations in machinery, materials and design in its development. With excellent skills that integrate the knowledge and passion of anc... Read MoreMaterial Full tempered glass product name/ type Shot glass Types of tableware Western tableware
- ADERIA Thin Beer GlassLight-blown beer glass is a glass that pursues a smooth mouthfeel that allows you to directly taste the taste, sharpness, and aroma of beer. It is easy to hold a moderate constriction, and you can use it with attachment for a long time with a simple form that you will not get tired of. In additio... Read MoreSpecification Full ion reinforcement Dishwasher Commercial or home use
- ARC Island shotProducts with the tempered glass mark are fully tempered "tempered glass" that is hard to break. Arcoroc Tumblers Island SeriesMaterial Soda-lime glass Diameter (Φmm) 38 product name/ type Shot glassfrom S$59.99Min. 2 days
- Toyo-Sasaki Glass Aroma floatSpecification Oral physical enhancement Material Soda-lime glassfrom S$67.99Min. 2 days