Stainless steel double tableware series The double hollow structure with excellent heat and cold insulation makes it difficult to transfer heat to the outside. It is an excellent container that does not easily cool hot items and does not easily condense even if cold items are put in it. It's ... Read More
Mass (g) 360 Types of tableware Japanese tableware
A series of stainless steel containers that are familiar in Korea. It is hygienic, light and durable !! The cold noodle bowl is a versatile product that is used not only for cold noodles but also for bibimbap, yukgaejang, and other soups.
Material 18-10 stainless steel Size Φ190×65 Mass (g) About 1000
Warm with IH. Economical to use with a small IH cooking heater. You can enjoy warm soup tsukemen until the end in a full-fledged pottery tsukemen bowl. Efficiently warm from the bottom of the tsukemen bowl with a carbon heating element.
For cost reduction !! Eco & Healthy Bowl You can significantly reduce soup even with a seemingly ordinary bowl. The size of the appearance is the same as that of a regular bowl, but it is processed to reduce the capacity. Since the amount of soup used is small, it also leads to cost reduction.
Material melamine Heat Resistance Temperature (℃) 120
Animals driving a locomotive with vegetables and fruits. Even in the short time of eating, we will bring you a very peaceful and enjoyable time. With a shape that is excellent in stacking and stability when stored, consideration is given to efficient draining.
Eating out, hospitals, kindergartens... Read More
Warm with IH. Economical to use with a small IH cooking heater. You can enjoy warm soup tsukemen until the end in a full-fledged pottery tsukemen bowl. Efficiently warm from the bottom of the tsukemen bowl with a carbon heating element.
It is a hand-carved container with a taste. The calm colors make you feel the taste, and you will want to enjoy the food slowly.
Eating out, hospital, welfare
Material melamine Conform to Dishwasher, disinfection storage
A double-sided glaze Chinese noodle bowl that does not easily get oily. Red phoenix, blue dragon. The sacred beasts, Suzaku and Seiryu, which have been said to be auspicious since ancient times in China, are drawn on the noodle bowl. The arrangement makes you feel the image of Japanese, and it is... Read More
Capacity (L) 1.1 Microwave × Dishwasher ○ Types of tableware Chinese tableware
A variety of full-scale reinforced porcelain. Even though it is simple, it has a sense of grade and is a strong ally for various dishes.
Eating out / welfare / hotel