Rice Net & Cloth
Other Related Pages
- Iguchi Rice NetDoes not stick. It reduces the time and effort of washing the pot. Helps save water. Can be used repeatedly by washing with water.Material 100% polyester
- EBM Cooking Rice Net (Made by Tetoron)The rice doesn't stick and it's easy to wash in the kettle. A very convenient energy-saving net.Material Tetoron Heat Resistance Temperature (℃) 240
- Kanemitsusangyo Hokka other netThere is no sticking of rice, and washing in a kettle is speedy. Since there is no sticking or burning of rice in the kettle, rice loss is reduced and it is economical. Since it is easy to wash the kettle, the work time is reduced and the water charge is economical. The cooked rice is more delici... Read MoreMaterial 100% polyester (strong yarn)
- TKG Benlinnet softwareEasy-to-use soft type.Material Ester (Tetron yarn) Heat Resistance Temperature (℃) 150~180
- Nagoya Kogei Rice Bag Net for Commercial UseMaterial Polyester Heat Resistance Temperature (℃) 240
- TOKYO MEDICAL Rice guardFeatures. It quickly passes through the steam (steam) from the cooked rice, and the inner surface of the container becomes condensed water. Rice guard's water-absorbent paper absorbs condensed water to prevent backflow and control the moisturization of rice. It keeps the deliciousness of fres... Read MoreMaterial Paper, polyethylene, non-woven fabric Quantity (Sheets) 250from S$339.90Min. 2 days
- Altan Cooking rice netFor 5 squares. It has excellent heat resistance, so it can be used for a long time. The net prevents the rice from sticking and makes it easy to clean the container. [How to use] Wet the net with water. Spread the rice cooker net on the rice cooker. Put the rice in it and cover it with a net to w... Read MoreMaterial Kuraray yarn (100% polyester)from S$21.99Min. 2 days
- SANBELM For steamed cloth 2-3 mass NAIt is made of unbleached 100% cotton fabric, so you can use it with confidence.Material 100% cotton
- Yoshida Orimono Rice togi rice bagIf you put rice in a rice-cooking bag or rice-cooking bag, you can remove impurities, cracked rice, and small grains of rice from the mesh. You can cook rice by draining it while it is in the net and putting it in the rice cooker as it is. There is little burning or sticking to the pot, and it is... Read Morefrom S$49.99Min. 2 days
- SANBELM For sambermu steamed cloth 4 mass NAIt is made of unbleached 100% cotton fabric, so you can use it with confidence.Material 100% cotton
- FP Miyakohimo Cooking rice netThe blue lineup is suitable as a countermeasure against foreign matter contamination. Since it is a raw yarn made of chemical fibers, it does not easily fade.Material Polyester Color Blue Heat Resistance Temperature (℃) 250from S$16.99Min. 3 days
- KANDA Kankuma Rice CrossThere is no sticking of stubborn rice, making it easier to wash in a kettle. Since the rice does not stick or burn, there is little loss of rice and it is economical. Since it is easy to wash the pot, there is no loss of work time. Since it is easy to wash the kettle, the water bill is also econo... Read MoreMaterial Tetoron Heat Resistance Temperature (℃) 250from S$27.99Min. 4 days
- MT Torimatsu Cooking rice master NetronMaterial Polyester Heat Resistance Temperature (℃) Melting point: 255from S$29.99Min. 3 days
- KANDA Commercial cooking rice bag netMix Rate (%) 100% polyester Heat Resistance Temperature (℃) 240from S$56.99Min. 5 days
- MT Torimatsu RD rice cooking netYou can put rice in the net and transfer the rice as it is.Material Polyester Heat Resistance Temperature (℃) 200~250from S$21.99Min. 3 days
- Arcland Sakamoto Hikari net for cooking riceThere is no stubborn sticking of rice, and washing in a kettle is speedy. Since there is no sticking or burning of rice in the kettle, rice loss is reduced and it is economical. Since it is easy to wash the kettle, the work time is reduced and the water charge is economical. The cooked rice is mo... Read Morefrom S$29.99Min. 5 days
- EBM Everhot Takumi 5 go, lid typeCapacity 5 go (MAX) Power Consumption (W) 50 Power Supply Single phase 100V (50Hz, 60Hz) Warm Keeping Temperature Approx. 36 to 42 ° C maker part number 1647920from S$669.90Min. 4 days
- White Thumb ENDO Hikari NetDecide on labor-saving rice cooking. Eliminates sticking and burning.Material Toray Tetronfrom S$29.99Min. 8 days
- Tokyo Katsushika Welfare Cooking rice bag (100 pieces)If you use a large pot, you can serve many people at once. Approximately 150g of polished rice and water are packed in a bag, and the rice is cooked just by boiling it in hot water for about 20 minutes.Material Polypropylenefrom S$199.90Min. 8 days
- Yamaya Bussan Simple rice cooker bag <Obukuro no Trick> for 100gIt is a mysterious bag that cooks rice just by putting rice in a bag without polishing and boiling it for about 20 minutes. The bran that adheres to the surface of the rice is discharged through the small holes in the bag and cannot enter the bag again.Material Polyester nonwoven fabricfrom S$139.90Min. 8 days
- Iguchi Rice net blue 100 x 100 cmForeign matter contamination countermeasure product It is easy to find lint in case of emergency. Food Sanitation Law compliant products * Boil for about 5 minutes before using for the first time. * Please wash with hot or cold water before each use.Material Polyesterfrom S$26.99Min. 2 days
- SNCOM MultinetConvenient item. It can be used for various purposes.Material Polyester resinfrom S$35.99Min. 8 days
- EBM Everhot Takumi 5 Go Edo lid typeCapacity 5 go (MAX) Power Consumption (W) 50 Power Supply Single phase 100V (50Hz, 60Hz) Warm Keeping Temperature Approx. 36 to 42 ° C maker part number 1647930from S$679.90Min. 4 days
- TOKYO MEDICAL Rice guard 50 piecesBy setting it in the rice container, the rice does not stick to the container, and you can reduce the time and effort to wash the container. The water absorption layer absorbs the moisture of the rice (condensed water consisting of it) and prevents the rice from becoming messy. For restaurants, r... Read MoreColor WhiteDiscontinued
- Akebono industry Rice knitThe popular "rice pita clip" that can be drained quickly has become a fashionable knit pattern. I will not spill the rice. For draining wakame seaweed and shredded cabbage. Comes with a hook that can be hooked.Discontinued
- MARUZEN KIKAKU Plump rice miniAll you have to do is put the fluffy rice in the center of the surface of the rice filled with water in the rice cooker and cook it. The rice is cooked so that you can appreciate the deliciousness of each grain of rice. Perfect for rice balls and sushi rice. Also, even when it cools down, it stil... Read MoreMaterial CeramicDiscontinued
- MARUZEN KIKAKU Plump rice (2)All you have to do is put the fluffy rice in the center of the surface of the rice filled with water in the rice cooker and cook it. The rice is cooked so that you can appreciate the deliciousness of each grain of rice. Perfect for rice balls and sushi rice. Also, even when it cools down, it stil... Read MoreMaterial CeramicDiscontinued
- Kuraray Kuraflex Woo rice sheetIt is a sheet that absorbs moisture and keeps the deliciousness of rice for 12 hours when the rice is standing and shining. 1) The steam from the cooked rice passes through the Wu rice sheet and hits the heat insulation case to condense dew. 2) Condensed water drips, is absorbed by the pulp layer... Read MoreMaterial NW Pulp80/PP20Discontinued
- MARUZEN KIKAKU New plump riceAll you have to do is put the fluffy rice in the center of the surface of the rice filled with water in the rice cooker and cook it. The rice is cooked so that you can appreciate the deliciousness of each grain of rice. Perfect for rice balls and sushi rice. Also, even when it cools down, it stil... Read MoreMaterial CeramicDiscontinued
- KANDA Woo rice packGazette bag shape Eslen container Suitable for deep SP-20D.Specification With lid Material PP + insulation Capacity (L) 11Discontinued
- Kuraray Kuraflex Woo rice packIt is a sheet that absorbs moisture and keeps the deliciousness of rice for 12 hours when the rice is standing and shining. 1) The steam from the cooked rice passes through the Wu rice sheet and hits the heat insulation case to condense dew. 2) Condensed water drips, is absorbed by the pulp layer... Read MoreMaterial NW PP60/Pulp40 Quantity (Sheets) 200Discontinued
- MARUZEN KIKAKU Plump rice for business useAll you have to do is put the fluffy rice in the center of the surface of the rice filled with water in the rice cooker and cook it. The rice is cooked so that you can appreciate the deliciousness of each grain of rice. Perfect for rice balls and sushi rice. Also, even when it cools down, it stil... Read MoreMaterial CeramicDiscontinued