Oil Jugs / Oilers / Spray Bottles
Oil mugs are tools intended for pouring oil such as gasoline, light oil, kerosene, and machine oil. Although mainly intended for oil, there are types that are used as coolant and water replenishment. The oil supply port is useful for preventing wide-mouth type oil mugs from spilling. The one with lid has the advantage that dust and dust are difficult to enter, and there is also a type with a nozzle cap with a net to prevent foreign substances from entering the liquid. There are long nozzle types and noise holders for convenient storage. Polyethylene oil mugs are cheap and mainstream, but there are also products with better heat resistance and somewhat expensive but durable iron oil mugs.
Other Related Pages
- MonotaRO Oil Dispenser with Long NozzleWith a super long nozzle of 530 mm in length, you can easily work in places that were difficult to reach before. The long nozzle, which is difficult to store after use, also comes with a nozzle holder, so it can be stored compactly and the floor will not be dirty and the liquid will not be wasted... Read MoreMaterial Polyethylene Classification of the Hazardous Non-dangerous goods
- MonotaRO Spray Bottle for SolventYou can easily spray the undiluted solution of organic solvent. It is convenient when using a large amount such as parts cleaner. Eliminates the cost and hassle of disposing of aerosol cans. The spray pattern can be adjusted by rotating the cap at the tip of the nozzle, and when the cap is fully ... Read MoreMaterial Head: PP, Bottle: HDPE, Packing: VITON Scale 100mL unit Bottle Diameter (Φmm) 100 Classification of the Hazardous Non-dangerous goods
- FURUPLA Jet Oiler Baby Type (Lubricant Oil Can)A soft, thick bottle with excellent resilience. Suitable for water and chemicals as well as oil.Material Polyethylene Memory Yes Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- MonotaRO Spray Refiller Easy Refillable Replaceable TypeIt can be easily used by simply adding liquid material and injecting compressed air. The nozzle is a 2-way method that can be used in both folded and extended states. The 100mm long nozzle is convenient in narrow places or in deep places. Since it is a liquid material refill type, unlike conventi... Read MoreValve Opening Pressure (kPa) 630
- FURUPLA DIA Spray Bottle ClearAs it is a clear bottle, the liquid inside can be seen well. You can switch between fog and direct sunlight with the cap.Classification of the Hazardous Non-dangerous goods
- Ribot Special filling spray can 300mLA filling spray can for a filling machine dedicated to brakes and parts cleaners. It can be blown upside down.Specification Upside down injection possible Classification of the Hazardous Non-dangerous goods Feature Upside down injection possible
- ESCO 180ml pump oiler (flexible nozzle steel)Material Steel Capacity (L) 0.18 Nozzle flexible Classification of the Hazardous Non-dangerous goodsfrom S$48.99Min. 2 days
- YAMAZAKI (CONDOR) Sprayer with flexible tubeA sprayer with a tube that can be connected directly to the mouth of a plastic container. Spray spray * Do not use strong acid chemicals, light petroleum, chemicals with strong dissolving power, or solvents.Material Sprayer: PP, Flexible tube: PVC Color Red Mass (g) 146 Classification of the Hazardous Non-dangerous goods
- EPOCA TEC-ONE1000 VITONEquipped with a strong chemical resistant tank and a gasket of Baitton rubber [[(R)]], it is a spray for professionals with excellent acid resistance and weather resistance. It can be adjusted from mist to jet. Ideal for automobile-related work and outdoor use. For cleaning work related to automo... Read MoreMass (g) 399 Classification of the Hazardous Non-dangerous goods 2018 Trusco page 10 0822
- DAHLIA The spray DX long nozzle (pendulum hose type)Can be sprayed at any angle "Pendulum type hose" is adopted. You can spray at any angle. A single spray produces twice as much mist as a regular spray, making work easier. You can freely change the way the fog comes out by turning the nozzle cap. Alcohol disinfection (absolute ethanol c... Read MoreMass (g) 198 Classification of the Hazardous Non-dangerous goodsfrom S$26.99Min. 2 days
- DAHLIA Dariya fully automatic sprayMaterial Made of brass Classification of the Hazardous Non-dangerous goodsfrom S$229.90Min. 4 days
- Koga Chemical Mfg. Oil JugWe have various sizes according to the application. Ideal for changing coolant and oil.Material Polyethylene Memory Yes Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- MonotaRO Oil jug Long nozzle With lidWith a lid, it is difficult for dust and dirt to enter, and the ultra-long nozzle with a length of 530 mm makes it easy to work even in places where it was difficult to put in until now. Ideal for replenishing or replacing low-viscosity oils, coolants, and water such as gasoline, light oil, keros... Read MoreMaterial Polyethylene Capacity (L) 5 Bottom Diameter (mm) 205 Classification of the Hazardous Non-dangerous goods
- MonotaRO Canyon Spray Bottle Swivel TypeIt has a special patented structure and is highly durable because the important parts are completely sealed. By using the bellows tube and weight, it is possible to spray continuously from any angle such as [sideways] and [upside down], and there is no worry of bending and clogging. In addition, ... Read MoreMaterial PP, PE, LLDPE (body) Scale 50mL unit Classification of the Hazardous Non-dangerous goods
- FURUPLA Jet Oiler 400mL TypeA soft, thick bottle with excellent resilience. Suitable for water and chemicals as well as oil. In addition to oil, water, chemicals, adhesives, etc.Material Polyethylene Mass (g) 50 Memory Yes Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- FURUPLA Jet Oiler Super TypeSuitable for water and chemicals as well as oil. A soft, thick bottle with excellent resilience.Material Polyethylene, brass Mass (g) 36 Type Super type Memory Yes Bottom Diameter (mm) 58 Nozzle shape Straight Classification of the Hazardous Non-dangerous goods
- FURUPLA All Plastic Oiler Sewing Machine Type● A soft, thick bottle with excellent resilience. ● Suitable for water and chemicals in addition to oil.Material Polyethylene Type Sewing machine type Color Blue Mass (g) 7 Memory Yes Classification of the Hazardous Non-dangerous goods
- AZ AZ mixed weighing tank deluxeYou can easily make mixed gasoline from 10: 1 to 100: 1. You can easily make a 25: 1 mixed fuel simply by matching the heights of gasoline and two-stroke engine oil. For mixing mixed fuels, etc.Included Accessories Bellows nozzle Classification of the Hazardous Non-dangerous goods
- Koga Chemical Mfg. Super Long NozzleA long nozzle for Furukawa Yakuhin Kogyo's oil jug. It can also be used for Monotaro's long nozzle oil jug. With a length of 530 mm, it can easily reach places that cannot be reached with a standard nozzle. With dripping prevention cap.Included Accessories Dripping prevention cap Material Polyethylene Memory None Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- TRUSCO Long nozzle for spray made of PP30 cm PP replacement nozzle. "When spraying cleaning agents and lubricants into elongated holes, etc. Spray compatible products: ALP-AC, BP, BPS, BPSJ, CL, TC (cleaning agent), ALP-TS, MTS-420SP (cutting agent), ALP-AR, S2, SL, WO, TFP-420SP-U, -M, PTFE-420SP (oil spray type) "Material Polypropylene (PP) Mass (g) 2.0 Classification of the Hazardous Non-dangerous goods
- MonotaRO Hand Spray PE BottleCan be sprayed in two patterns, straight (rod-shaped) and wide (mist-shaped) * Since tap water is used for inspection at the time of manufacturing inspection, water may remain in the main body, but there is no problem in use. * Cannot be used for hot water above 40 ° C. * Cannot be used for solve... Read MoreMaterial (Nozzle) PP, (Bottle) PE Color (Nozzle) Red, (Bottle) White Suitable Fluid Water
- FURUPLA Jet Oiler New Super Brass Nozzle● A soft, thick bottle with excellent resilience. ● Since the nozzle is brass, it has a heat resistant effect.Material Polyethylene, brass Type New super type Memory Yes Nozzle shape Bend ahead Classification of the Hazardous Non-dangerous goods
- AZ Stainless nozzleClassification of the Hazardous Non-dangerous goods
- TRUSCO Spray Bottle, Cost EffectiveAn economy type spray that can be used widely from water to disinfectant. If you turn the nozzle, it can handle everything from jets to diffusion and fog. Viscous liquids and solvents cannot be used. * Cannot be used for solvent-based liquids.Color Black Discharge Amount 1cc Classification of the Hazardous Non-dangerous goods
- FURUPLA Jet Oiler 300mL TypeA soft, thick bottle with excellent resilience. Suitable for water and chemicals as well as oil.Material Polyethylene Mass (g) 37.5 Memory Yes Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- FURUPLA Jet Oiler Pistol TypeMaterial Polypropylene, polyethylene Color yellow Memory Yes Bottom Diameter (mm) 95 Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- FURUPLA Jet oiler portable oilpiperExcellent resilience with a soft thick bottle. Please pull out the brass pipe to use it. After use, if you insert the pipe to the bottom, the oil will not spill, so it is convenient to carry.Material Polyethylene, brass Color yellow Memory Yes Classification of the Hazardous Non-dangerous goods
- TRUSCO Long nozzle for spray (stainless steel)A 30 cm stainless steel replacement nozzle. When spraying a cleaning agent or lubricant into an elongated hole.Material Stainless steel Mass (g) 2.0 Head Diameter (Φmm) 22.8 Classification of the Hazardous Non-dangerous goods
- GA (Green Ace) Free bond containerRefill container for bonds. The bond can be stretched evenly on the spatula. It can be used for many purposes. Press the side of the container and the adhesive will come out. The sides are soft and easy to push. For those who want to reduce the amount of adhesive consumed. For those who want to e... Read MoreMaterial LDPE Color Natural Memory None Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- NIPPEI KIKI NIPPEI Pistol OilerA very long-lasting oiler made of aluminum die-cast.Classification of the Hazardous Non-dangerous goods
- AZ Plastic nozzleIt can be attached to a spray with a stem outer diameter of 4 mm. To the spray nozzleClassification of the Hazardous Non-dangerous goods
- FURUPLA Poly Jug● Easy-to-grip handle. ● Convenient for transferring liquids. ● A nozzle that can inject in a well-balanced manner.Material Polyethylene Memory Yes
- Mizuho Kasei PP Ointment ContainerWide caliber polypropylene container with no internal protrusions. Nearly the entire amount can be taken out even in paste form, and it can be used as a sample container with an inner plug. For storage and storage of liquids * Liquids that are not suitable for polyethylene and polypropylene canno... Read MoreSpecification With inner plug Scale None Material (Cap) Polypropylene (PP) Heat Resistance Temperature (℃) 80 Hazardous Class Other ones Material (inner plug) Polyethylene (PE) Classification of the Hazardous Designated combustibles Name of The Hazardous Synthetic resins
- BOLL OilerSemi-transparent with cap and scale, the contents can be seen and the tip nozzle is thin, so it can be easily injected even in narrow places.Classification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
- TRUSCO Mixing weighing tankIn addition to 25: 1, 50: 1, 10: 1 to 100: 1 mixed gasoline can be made. If you want to make it in a ratio of 25: 1, you can easily make it just by matching the height of gasoline and 2-cycle engine oil. Tank for mixing mixed gasoline * Gasoline sold separatelyMaterial Polyethylene (PE) Color White Mass (g) 620 Capacity (L) 5 Classification of the Hazardous Non-dangerous goods
- ESCO Plastic OilerMaterial Polyethylene Classification of the Hazardous Non-dangerous goods
- DAHLIA DAHLIA Spray BottleA refreshing mist with a quick blow! A light, easy and easy-to-use spray. You can freely change the way the fog comes out by turning the nozzle cap. It can be diluted with alcohol disinfection (80% or less of absolute ethanol) before use. * Chemical resistant materials are used, but acidic chemic... Read MoreClassification of the Hazardous Non-dangerous goods
- TRUSCO Colorful JugIt is convenient because it can be color-coded for each oil type. As it is a wide mouth type, it is convenient without spilling when refueling. It has a scale. It can be attached to a long nozzle (530 mm) as an option sold separately. Suitable for transferring machine oil, etc.Included Accessories Nozzle (160mm) Material Polyethylene (PE) Classification of the Hazardous Non-dangerous goods
- SANSYO Oil JugThe nozzle (total length 230 mm) bends freely, making it easy to inject. The nozzle cap has a net to prevent foreign matter from entering.Material PE Classification of the Hazardous Non-dangerous goods
- GA (Green Ace) Free bond container 750gClassification of the Hazardous Non-dangerous goods RoHS directive (corresponding to 10 substances) Correspondence
Filter by categories