All Category

Electric Winch Ropes

View : Grid List
Filter

30 Item(s)

Set Ascending Direction
  1. Cremona S rope
    JEFCOM (DENSAN) Cremona S rope
    Uses ester to prevent slipping and has good workability (easy to tie) With both eye processing that stretches little and sinks in water If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if th... Read More
    RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$189.90
    Min. 2 days
  2. DBP rope
    Portable Winch DBP rope
    Portable Winch Recommended rope For forestry
    Rope Specification  Double braided polyester rope 
    Rating:
    100%
    from S$299.90
    Min. 2 days
  3. Rope for electric winch Tetron cross (8 pcs)
    PROMATE Rope for electric winch Tetron cross (8 pcs)
    A strong rope that can be sized according to the application. Both ends eye processing. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the deliver... Read More
    Dimensions (Diameter Φmm)  12  Breaking Load (kN)  23 
    Rating:
    100%
    from S$279.90
    Min. 2 days
  4. Nylon 8 cross rope
    JEFCOM (DENSAN) Nylon 8 cross rope
    Kink ・ There is no return. Powerful with 8 strokes. With both eye processing. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery locatio... Read More
    RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$219.90
    Min. 4 days
  5. Super line rope UC
    Takagi Super line rope UC
    It is a rope that has almost the same strength as a wire rope and is hard to stretch. Has excellent electrical insulation. It is a waterproof type. As a limit display rope, as a rope for wire drawing * 1m cut product.
    Length (m)  Specification  Non-rotating structure  Color  Orange 
    Rating:
    100%
    from S$4.69
    Min. 2 days
  6. Line jet blow Lead rope
    JEFCOM (DENSAN) Line jet blow Lead rope
    Lead rope (rope for wire index)
    Length (m)  200  RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$99.90
    Min. 3 days
  7. Electric winch rope nylon
    PROMATE Electric winch rope nylon
    A strong rope (three-strike) that responds to the size according to the application If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery lo... Read More
    Overall Length (m)  30 
    from S$249.90
    Min. 2 days
  8. Rope for electric winch Tetoron cloth (12)
    PROMATE Rope for electric winch Tetoron cloth (12)
    A strong rope that can be sized according to the application. If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, the delivery d... Read More
    from S$269.90
    Min. 5 days
  9. Tetron rope
    JEFCOM (DENSAN) Tetron rope
    12-stroke kink with double eye processing that does not return If the delivery destination is a private house (detached house / apartment house), the shop name is required. Please note that delivery may not be possible if there is no store name. * Depending on the delivery location, the delivery ... Read More
    Dimensions (Φ × m)  10×50  Breaking strength (kN)  19.6  Specification  Breaking strength (kN) /19.6  RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$339.90
    Min. 4 days
  10. 12mm x 50m Tetoron rope (both eye processing)
    ESCO 12mm x 50m Tetoron rope (both eye processing)
    from S$329.90
    Min. 6 days
  11. Flat rubber rope
    TASCO Flat rubber rope
    Dimension (mm)  20×750~900 
    from S$27.99
    Min. 5 days
  12. 12mmx30m Tetoron rope (both eye processing)
    ESCO 12mmx30m Tetoron rope (both eye processing)
    * Please use an appropriate safe load for work with continuous load. (1/6/1/10 of breaking load)
    Rope dimensions (diameter Φmm x length m)  12×30  Mass (kg)  About 3.3  Breaking load (kN [kgf])  23(2350)  Specification  8 strikes 
    from S$239.90
    Min. 4 days
  13. 14mmx30m Tetoron rope (both eye processing)
    ESCO 14mmx30m Tetoron rope (both eye processing)
    * Please use an appropriate safe load for work with continuous load. (1/6/1/10 of breaking load)
    Breaking load (kN [kgf])  30.5(3110)  Rope dimensions (diameter Φmm x length m)  14×30  Mass (kg)  About 4.4  Specification  8 strikes 
    from S$289.90
    Min. 4 days
  14. Unilon G rope
    JEFCOM (DENSAN) Unilon G rope
    Higher strength than conventional cross-structured ropes. Good wear resistance and less likely to cause local wear damage. Lower elongation than nylon rope. There are few kinks because it is composed of 6 strands on each side. Flexible and easy to work with. With both eye processing.
    RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$449.90
    Min. 16 days
  15. 14mmx100m  Tetoron rope (both sides eye processing)
    ESCO 14mmx100m Tetoron rope (both sides eye processing)
    Rope dimensions (diameter Φmm x length m)  14×100  Breaking load (kN [kgf])  30.5(3110kgf)  Mass (kg)  About 14.5 
    from S$779.90
    Min. 5 days
  16. Super line rope UD
    Takagi Super line rope UD
    It floats on water and has about 10 times more wear resistance than aramid fiber. It is the lightest, ultra-high strength, and highly elastic fiber among high-performance fibers. It has excellent light resistance and can withstand outdoor use. It is lighter than wire rope and has no rust, so it i... Read More
    Length (m)  Packaging  Band winding  Color  Dark green 
    from S$6.49
    Min. 8 days
  17. 14mmx200m Tetoron rope (both eye processing)
    ESCO 14mmx200m Tetoron rope (both eye processing)
    Esco Part No.  EA628MD-144 
    from S$1,499.00
    Min. 4 days
  18. 16mmx200m Tetoron rope (both eye processing)
    ESCO 16mmx200m Tetoron rope (both eye processing)
    Esco Part No.  EA628MD-164 
    from S$1,899.00
    Min. 4 days
  19. 12mmx100m Tetoron rope (both sides processed)
    ESCO 12mmx100m Tetoron rope (both sides processed)
    * Please use an appropriate safe load for work with continuous load. (1/6/1/10 of breaking load)
    Breaking load (kN [kgf])  23(2350)  Mass (kg)  About 11.0  Specification  8 strikes  Rope dimensions (diameter Φmm x length m)  12×100 
    from S$589.90
    Min. 4 days
  20. For safety rope 3kg
    TASCO For safety rope 3kg
    from S$24.99
    Min. 5 days
  21. New super tech rope
    JEFCOM (DENSAN) New super tech rope
    Introducing a super strong rope with high heat resistance and high strength, with even higher strength! High strength that surpasses Kevlar rope. The breaking strength of Φ10mm is 53.9kN, which is more than twice that of Tetoron rope. It does not harden even when it gets wet, and keeps its supple... Read More
    Breaking strength (kN)  34.3  Dimensions (Φ × m)  8×100  RoHS directive (corresponding to 10 substances)  Correspondence 
    from S$1,999.00
    Min. 34 days
  22. Nylon cross rope (for eight-stroke / electric winch)
    ESCO Nylon cross rope (for eight-stroke / electric winch)
    The strongest nylon cross rope in general fiber materials. It is shock resistant, flexible, easy to handle, and has excellent wear resistance. Since it is a cross-knitted rope, it is difficult to kink and it is easy to handle because there is no untwisting. (Electric) For winch ropes, cargo handl... Read More
    from S$199.90
    Min. 4 days
  23. 12mmx200m Tetoron rope (both eye processing)
    ESCO 12mmx200m Tetoron rope (both eye processing)
    Esco Part No.  EA628MD-124 
    from S$1,199.00
    Min. 4 days
  24. SuperMax Rope for Forestry Winch
    DAIKO SuperMax Rope for Forestry Winch
    An ultra-high-strength rope using Dyneema, ideal for single-pull winches. The burden on the body is greatly reduced, and the efficiency of lumber collection work is improved. Single-body winch, lumber collection work, etc. * Do not use in an environment with a high temperature of 80 ° C or higher.
    from S$1,299.00
    Min. 5 days
  25. 16mmx  50m  Tetoron rope (both sides eye processing)
    ESCO 16mmx 50m Tetoron rope (both sides eye processing)
    Rope dimensions (diameter Φmm x length m)  16×50  Breaking load (kN [kgf])  38.5(3930kgf)  Mass (kg)  About 9.5 
    from S$539.90
    Min. 5 days
  26. 16mmx30m Tetoron rope (both sides processed)
    ESCO 16mmx30m Tetoron rope (both sides processed)
    * Please use an appropriate safe load for work with continuous load. (1/6/1/10 of breaking load)
    Rope dimensions (diameter Φmm x length m)  16×30  Breaking load (kN [kgf])  38.5(3930)  Specification  8 strikes  Mass (kg)  About 5.7 
    from S$349.90
    Min. 4 days
  27. 14mmx50m Tetoron rope (both eye processing)
    ESCO 14mmx50m Tetoron rope (both eye processing)
    * Please use an appropriate safe load for work with continuous load. (1/6/1/10 of breaking load)
    Mass (kg)  About 7.3  Rope dimensions (diameter Φmm x length m)  14×50  Specification  8 strikes  Breaking load (kN [kgf])  30.5(3110) 
    from S$439.90
    Min. 4 days
  28. Ikura cross rope
    IKURA SEIKI Ikura cross rope
    Length (m)  50 
    from S$219.90
    Min. 6 days
  29. Super tow rope
    PROMATE Super tow rope
    Equivalent to wire rope, about 2.5 times stronger than nylon rope. It is about 1/4 lighter than a wire rope, and has a blade structure that does not rotate the rope. Resistant to wear and tensile fatigue. Good weather resistance, corrosion resistance, and chemical resistance. Good electrical insu... Read More
    Dimensions (Diameter Φmm)  Overall Length (m)  100  Mass (kg)  About 5.3  Breaking Load (kN)  32.5 
    Discontinued
  30. [With discount] Nylon 8 cross rope
    JEFCOM (DENSAN) [With discount] Nylon 8 cross rope
    Kink ・ There is no return. Powerful with 8 strokes. With both eye processing. * For the breaking strength of each rope, set an appropriate safety factor according to the environment in which it is used. * Delivery to private homes is not possible.
    Rope Length (m)  50  Commodity condition  * Reasonable (unused / unopened)  Breaking strength (kN)  27.5  Rope Diameter (Φmm)  12 
    Discontinued
View : Grid List
Filter

30 Item(s)

Set Ascending Direction