With the various equipment supported by the hanging bolts as they are, additional work can be done to share the hanging bolts of the support material.
* Please do not install only one side of the angle with a long hole. Please use one set on both sides. There is a risk of falling. * The surface t... Read More
It is a support bracket that fixes the main girder to the ductor of the support material at the rising point along the wall surface.
* When using the cover as the bottom plate, please use SRU1C. * The surface treatment of electrogalvanized products will be changed from colored chromate (hexavalen... Read More
By attaching the ductor channel to the cable rack, the box can be installed and the wiring connection on the secondary side can be made near the rack. You can install the ductor channel after laying the cable. The ductor channel can be attached to either the open side or the back side of the cabl... Read More
It is a metal fitting that fixes the separator to the child girder of the rack.
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please n... Read More
* When using the cover as the bottom plate, please use NQRU1C. * S-QRS4 has a different body shape. * The surface treatment of electrogalvanized products will be changed from colored chromate (hexavalent) to trivalent chromate. The color of the exterior changes from gold to silver. There is no pr... Read More
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read More
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read More
Three channels can be rack, pipe, and cable support. It is a simple bolt and nut tightening work that does not require welding.
* Due to environmental friendliness, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color will change from a color ... Read More
When used in combination with the cover clamp (CVC □), it makes an electrical connection between the rack and the cover. The ground bond wire between the covers can be omitted. When installing the cover clamp, simply tighten the hexagon bolt (dent) to obtain an electrical connection.
* Due to env... Read More
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read More
There is no need for on-site processing of the metal fitting mounting part.
* Due to environmental friendliness, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color will change from a color close to gold to a color close to silver) Please not... Read More
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read More
When used in combination with hanging brackets (SRH1N, NRH1, QRH1, etc.), the bottom surface of the bottom plate becomes flat, and construction with excellent aesthetics can be performed. A standard rack cover can be used as the bottom plate. It can also be used for the joint metal fittings of th... Read More
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read More
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read More
Please use it as an auxiliary material for Tough Lock 60 TAFT B- □. Use this when the steel sleeve is not installed at the floor penetration part or when the support plate is treated as a backing plate at the wall penetration part.
* For TAFTBS and TAFTBS1, the standard opening size is 200,300 mm... Read More
* In consideration of the environment, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color changes from a color close to gold to a color close to silver) Please note that it may be mixed depending on the product because it will be switched se... Read More
Used to support cables.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
Suitable for Cable (Φ45mm or less) Material Steel Mounting Hole Spacing 500~1000
It can be fixed with one touch from the upper side of the separator.
* Support at least 4 straight parts per separator. * Please support at least 3 places in the branch rack.
There is no need for on-site processing of the metal fitting mounting part.
* Due to environmental friendliness, the plating process will be changed from hexavalent chrome plating to trivalent chrome plating. (The color will change from a color close to gold to a color close to silver) Please not... Read More
Specification DH8N / Electrogalvanizing treatment Type Melamine resin baking finish