A lightweight strap that fits perfectly to any caliber and greatly improves the efficiency of duct work. Although it is durable, it can be cut with scissors. Since it is an elliptical hole, it can be used with any fastener. (Stops sold separately)
Suspension band for duct
* Stoppers are sold sepa... Read More
It can be piped in any direction with respect to the base material (ductor channel).
* Bolts and middle nuts are sold separately. Please prepare a hexagon bolt with a length of 25 mm.
* Make a drain hole (Φ10) in the ductor channel installed in the direction perpendicular to the roof slope. Rainwater may collect and rust may occur. * Do not install in the direction in which the load (W) is applied to the base material cross support bracket. There is a risk of dropping out. * K... Read More
It can be used for various types of ducts. Each size is marked around the case, so you can measure the length with a guide and cut it to just the right size. It is convenient to carry and inventory management can be reduced.
Duct tightening band
* Clamp is sold separately.
Material Stainless steel (SUS430) Tensile Strength (N/mm2) 450
It is a metal fitting for attaching lighting equipment etc. to the interior duct body.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
A metal fitting for attaching equipment such as a switch box to the interior duct body.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
It is a connecting bracket for the interior duct body. Since it can be connected inside the interior duct body, the finish is beautiful. It can be easily installed by simply fitting the interior duct and tightening the screws.
*We cannot deliver products directly from the manufacturer to individu... Read More
It is used to protect cables when connecting from interior ducts to walls, attics, etc. The cable will not be damaged. It can be cut and used freely according to the thickness of the wall / ceiling material, and it is easy to install.
*We cannot deliver products directly from the manufacturer to ... Read More
Suitable for Wall / ceiling thickness (up to 45mm)
When the interior duct is used with the opening facing downward, it is used to temporarily fix the cable hanging down during wiring.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguishe... Read More
It is a connecting bracket for the plastic duct body. It can be easily connected by simply fitting it into the side groove of the plastic duct and tightening the screw.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the ... Read More
A fixture that directly attaches the interior duct body to the construction material with wood screws. It can be easily installed by simply tightening screws using the knock holes in the interior duct, resulting in a neat finish. There is no protrusion in the interior duct, and wiring after const... Read More
On the floor side, no glue remains even if it is peeled off, so it sticks to the PVC sheet floor such as vinyl tiles. Ideal for wagon malls. Even if the floor side is peeled off, it can be used again. * Rinse off dust and dirt with a neutral detergent, dry it, and then use it again.
*We cannot de... Read More
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
It can be easily attached to moldings, plastics, metals, glass, etc. The strong type is ideal for sticking to the wall. The peelable type can be peeled off later, leaving no glue on the sticking surface.
*Avoid using or storing in places with high temperatures or where it is easy to get wet. * Ca... Read More
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
Specification For skirting duct (PHD-95T) Material Plastic Color Chocolate
*We cannot deliver products directly from the manufacturer to individual homes. *Please note that this includes cases where the building name cannot be distinguished from the exterior of the building.
Specification For skirting duct (PHD-95T) Material Plastic Color Chocolate
It can be easily attached to moldings, plastics, metals, glass, etc. The strong type is ideal for sticking to the wall. The peelable type can be peeled off later, leaving no glue on the sticking surface.
*Avoid using or storing in places with high temperatures or where it is easy to get wet. * Ca... Read More