All Category

Blocks for Wiring Ducts

Other Related Pages

View : Grid List
Filter

32 Item(s)

Set Ascending Direction
  1. Day One Block (Roof Exposed Piping Block)
    NEGUROSU DENKO Day One Block (Roof Exposed Piping Block)
    MKB □ uses a hot dip galvanized ductor channel. S-MKB □ uses a stainless steel ductor channel. The block is waterproof and has excellent water repellency and is less likely to deteriorate. By extending the channel 3 mm from the top of the block and improving drainage, the piping material is less ... Read More
    Material  (Block part) Mortar 
    Rating:
    80%
    from S$29.99
    Min. 2 days
  2. Block for rooftop exposed piping (with rubber base)
    NEGUROSU DENKO Block for rooftop exposed piping (with rubber base)
    The rubber base is attached directly to the bottom of the block using an adhesive. Please use it on the rooftop with a waterproof coating that cannot be installed directly on the Day One block. MKBGB □ uses a hot dip galvanized ductor channel. S-MKBGB □ uses a stainless steel ductor channel. By e... Read More
    Color  (Rubber base) Black  Dimension (mm)  30×110×3t 
    Rating:
    80%
    from S$29.99
    Min. 2 days
  3. World Dactor (Foundation block for angle mount)
    NEGUROSU DENKO World Dactor (Foundation block for angle mount)
    It can be easily used as the basis of an angle piping stand. The angle material can be securely fixed by the mounting bracket on the top of the main body and the attached bolts. The block is waterproof and has excellent water repellency and is less likely to deteriorate. * Do not tilt or shake du... Read More
    from S$29.99
    Min. 2 days
  4. World Ductor (Nut nut for temporary fixing)
    NEGUROSU DENKO World Ductor (Nut nut for temporary fixing)
    After attaching to the ductor channel, it can be temporarily fixed, saving the trouble of holding down the middle nut. Since it can be temporarily fixed, it can slide freely according to the support interval after installation. * Due to environmental friendliness, the plating process will be chan... Read More
    Rating:
    100%
    from S$35.99
    Min. 2 days
  5. World Ductor (Fundamental base block)
    NEGUROSU DENKO World Ductor (Fundamental base block)
    Insert embedded type block. It can be used for many purposes as a foundation for various piping mounts. The block is waterproof and has excellent water repellency and is less likely to deteriorate. * Do not tilt or shake during or after construction. The block may be damaged.
    Mass (kg) 
    from S$29.99
    Min. 2 days
  6. Day One Block (Rubber Base for Day One Block)
    NEGUROSU DENKO Day One Block (Rubber Base for Day One Block)
    Please use it on the rooftop with a waterproof coating that cannot be installed directly on the Day One block. It is concave so that the day one block does not shift. It can also be used when using Day One blocks side by side in series. * The black color of the rubber base may stain depending on ... Read More
    Color  Black  Material  Ethylene propylene rubber 
    from S$6.49
    Min. 2 days
  7. World Ductor (with base block rubber base for mounting)
    NEGUROSU DENKO World Ductor (with base block rubber base for mounting)
    The rubber base is attached directly to the bottom of the block using an adhesive. Please use it when the paint film is waterproofed and the block cannot be installed directly. Insert embedded type block. It can be used for many purposes as the basis of various piping stands. The block is waterpr... Read More
    Mass (kg) 
    Rating:
    100%
    from S$36.99
    Min. 2 days
  8. D-One block (Rubber base for foundation block)
    NEGUROSU DENKO D-One block (Rubber base for foundation block)
    Please use it on the rooftop with a waterproof coating that cannot be installed directly on the foundation block. It is concave so that the foundation block does not shift. * The black color of the rubber base may stain depending on the condition of the floor. When storing at the site, lay a shee... Read More
    Color  Black  Material  Ethylene propylene rubber 
    from S$5.99
    Min. 2 days
  9. Day One Block (Roof Exposed Piping Block with Rubber Base)
    NEGUROSU DENKO Day One Block (Roof Exposed Piping Block with Rubber Base)
    The rubber base is attached directly to the bottom of the block using an adhesive. Please use it on the rooftop with a waterproof coating that cannot be installed directly on the Day One block. MKBGB □ uses a hot dip galvanized ductor channel. S-MKBGB □ uses a stainless steel ductor channel. By e... Read More
    Material  Block part: Mortar 
    Rating:
    100%
    from S$29.99
    Min. 3 days
  10. World Ductor (Rubber sheet for basic formwork)
    NEGUROSU DENKO World Ductor (Rubber sheet for basic formwork)
    Please use it when the gantry cannot be directly installed, such as when the paint film waterproofing method is used. Please use it when constructing a pedestal on the expansion joint of the cinder method. With a marking line for easy positioning. The formwork MK □ is concave so that it does not ... Read More
    Color  Black  Material  Ethylene propylene rubber 
    from S$6.19
    Min. 6 days
  11. Rubber base for day block
    NEGUROSU DENKO Rubber base for day block
    Please use it on the rooftop with a waterproof coating that cannot be installed directly on the Day One block. It is concave so that the day one block does not shift. It can also be used when using Day One blocks side by side in series. * The black color of the rubber base may transfer depending ... Read More
    Color  Black  Material  Ethylene propylene rubber 
    from S$12.99
    Min. 6 days
  12. D1 block floor fixing bracket
    NEGUROSU DENKO D1 block floor fixing bracket
    * Do not use for day one blocks with a rubber base.
    from S$11.99
    Min. 6 days
  13. Base block for Dactor channel mount
    NEGUROSU DENKO Base block for Dactor channel mount
    It can be easily used by inserting the ductor channel as the foundation of the piping stand. The attached L bracket can securely fix the ductor channel. Since it has drain holes and grooves, rainwater does not collect in the ductor channel insertion part. The block is waterproof and has excellent... Read More
    Suitable for  Ductor channel / D2 type  Mass (kg)  About 3.0 
    from S$36.99
    Min. 6 days
  14. Tire regeneration block
    NEGUROSU DENKO Tire regeneration block
    This product is made by recycling used tires and reprocessing them. It will not crack or chip even if dropped like a mortar block. The main body is made of rubber, so there is no risk of damaging the waterproof coating surface on the roof. Lightweight and easy to carry. The main body is made of r... Read More
    from S$27.99
    Min. 2 days
  15. Day One Block (Pull Box Fixing Bracket for Day One Block)
    NEGUROSU DENKO Day One Block (Pull Box Fixing Bracket for Day One Block)
    Suitable for  MKB□07 MKB□10 MKB□13 
    from S$8.49
    Min. 6 days
  16. D-One block (block adhesive)
    NEGUROSU DENKO D-One block (block adhesive)
    Suitable for  MKB□、MKBH□N MKBA□ 
    from S$27.99
    Min. 5 days
  17. Day One Block (Pull Box Fixing Bracket for Day One Block)
    NEGUROSU DENKO Day One Block (Pull Box Fixing Bracket for Day One Block)
    Suitable for  MKB□10 MKB□13  Surface Treatment  Hot-dip galvanized finish 
    from S$8.99
    Min. 6 days
  18. Foundation block for Dacter mount (with rubber base)
    NEGUROSU DENKO Foundation block for Dacter mount (with rubber base)
    The rubber base is attached directly to the bottom of the block using adhesive. Please use it when the block cannot be installed directly because the paint film is waterproofed. It can be easily used by inserting the ductor channel as the foundation of the piping stand. The attached L bracket can... Read More
    Suitable for  (Ductor channel) D1, D20 type  Dimension (mm)  (Rubber base) 50 × 110 × 3t  Color  (Rubber base) Black  Maximum Loading Capacity (kg)  250  Mass (kg)  About 3.1 
    from S$35.99
    Min. 3 days
  19. Rooftop exposed piping block
    NEGUROSU DENKO Rooftop exposed piping block
    MKB □ uses a hot dip galvanized ductor channel. S-MKB □ uses a stainless steel ductor channel. The block is waterproof and has excellent water repellency and is less likely to deteriorate. By extending the channel 3 mm from the top of the block and improving drainage, the piping material is less ... Read More
    Material  (Block part) Mortar  Dimension H (mm)  100  Maximum Loading Capacity (kg)  200 
    from S$58.99
    Min. 6 days
  20. World Ductor (base block for mount)
    NEGUROSU DENKO World Ductor (base block for mount)
    The block is waterproof and has excellent water repellency and is less likely to deteriorate. At the bottom of the block, there are notches on all sides for marking positioning. There are recesses on both sides for easy portability. * Do not use the foundation block for the construction of a stan... Read More
    Material  Block part: Concrete  Mass (kg)  19.5 
    from S$139.90
    Min. 7 days
  21. Day One Block (Equipment installation material for Day One Block)
    NEGUROSU DENKO Day One Block (Equipment installation material for Day One Block)
    Various devices can be installed using the Day One block as an installation stand. Please use it when installing the air conditioner outdoor unit etc. in the day one block.
    Suitable for  MKB□ 
    from S$6.49
    Min. 3 days
  22. Day one block (rubber base for block)
    NEGUROSU DENKO Day one block (rubber base for block)
    Please use it on the rooftop with a waterproof coating that cannot be installed directly on the block. Since it has an adhesive tape on one side, you can easily attach it to the bottom of the block by peeling off the release paper. * Please use by pasting at least two places on the bottom of the ... Read More
    Wall Thickness (mm)  Color  Black  Material  Chloroprene rubber  Suitable for  MKB□、MKBH□N MKBA1 
    from S$1.59
    Min. 5 days
  23. D-One block (Connecting bracket for D-One block)
    NEGUROSU DENKO D-One block (Connecting bracket for D-One block)
    Day One Block You can combine existing sizes and easily connect them. The ductor clip can also be used within the mounting range of the connecting bracket.
    Material  stainless steel 
    from S$3.99
    Min. 5 days
  24. Foundation block for Dactor channel mount (with rubber base)
    NEGUROSU DENKO Foundation block for Dactor channel mount (with rubber base)
    The rubber base is attached directly to the bottom of the block using adhesive. Please use it when the block cannot be installed directly because the paint film is waterproofed. It can be easily used by inserting the ductor channel as the foundation of the piping stand. The attached L bracket can... Read More
    Suitable for  Ductor channel / D2 type  Mass (kg)  About 3.1 
    from S$39.99
    Min. 6 days
  25. D-One block (rubber base for gantry base block)
    NEGUROSU DENKO D-One block (rubber base for gantry base block)
    Please use it on the rooftop with a waterproof coating that cannot be installed directly on the foundation block. It is concave so that the foundation block does not shift.
    Color  Black  Material  Ethylene propylene rubber  Suitable for  MKBS1-M10 MKBS1C-M10 
    from S$26.99
    Min. 6 days
  26. Base block for pedestal (product against frost damage)
    NEGUROSU DENKO Base block for pedestal (product against frost damage)
    At the bottom of the block, there are notches for marking on all sides. Recesses are provided on both sides of the side for easy portability. Since it does not absorb water and does not freeze and thaw, it is ideal as a countermeasure against frost damage. It is a block that can be used as the fo... Read More
    Depth (mm)  (Insert) 25  Applicable bolt diameter  M10  Mass (kg)  About 17  Material  (Block part) Resin concrete 
    from S$499.90
    Min. 6 days
  27. Foundation block for gantry (with rubber base)
    NEGUROSU DENKO Foundation block for gantry (with rubber base)
    A foundation block for fixing the base metal fittings for the gate-shaped mount and the telescopic base metal fittings. The height of the telescopic base bracket can be adjusted after fixing. It has a low center of gravity and excellent stability. It is a bolt-embedded type block. The base bracke... Read More
    Dimension (mm)  (Rubber base) 30 × 230 × 3t  Color  (Rubber base) Black  Suitable for  (Stand) SD-GSC  Maximum Loading Capacity (kg)  200  Mass (kg)  About 4 
    from S$46.99
    Min. 6 days
  28. Tire regeneration block  MKBM1RG
    NEGUROSU DENKO Tire regeneration block MKBM1RG
    This product is made by recycling used tires and reprocessing them. It will not crack or chip even if dropped like a mortar block. Since the main body is made of rubber, there is no risk of damaging the waterproof coating surface on the roof. Lightweight and easy to carry. The main body is made o... Read More
    Maximum Loading Capacity (kg)  100  Mass (kg)  About 0.68 
    from S$39.99
    Min. 6 days
  29. Foundation block (with rubber base)
    NEGUROSU DENKO Foundation block (with rubber base)
    A foundation block for fixing the base metal fittings for the gate-shaped mount and the telescopic base metal fittings. The height of the telescopic base bracket can be adjusted after fixing. It has a low center of gravity and excellent stability. It is a bolt-embedded type block. The base bracke... Read More
    Stand  SD-GSC□  Mass (kg)  About 4.0 
    from S$29.99
    Min. 7 days
  30. Base block for Dactor mount
    NEGUROSU DENKO Base block for Dactor mount
    It can be easily used by inserting the ductor channel as the foundation of the piping stand. The attached L bracket can securely fix the ductor channel. Since it has drain holes and grooves, rainwater does not collect in the ductor channel insertion part. The block is waterproof and has excellent... Read More
    Suitable for  (Ductor channel) D1, D20 type  Maximum Loading Capacity (kg)  250 
    from S$29.99
    Min. 2 days
  31. Piping support bracket for ground boundary block
    NEGUROSU DENKO Piping support bracket for ground boundary block
    You can fix the ductor to the ground boundary block. It can also be used as an installation stand for cable racks, etc. * Please refrain from carrying the ductor after assembly. The ductor may come off and the block may fall. * Z-MKBD1F is sold only as metal fittings. Please prepare the land boun... Read More
    Suitable for  Land boundary block 
    from S$22.99
    Min. 6 days
  32. D-One block (rubber base for block temporarily fixing type)
    NEGUROSU DENKO D-One block (rubber base for block temporarily fixing type)
    Please use it on the rooftop with a waterproof coating that cannot be installed directly on the Day One block. Since it is only attached to the bottom of the block using the elasticity of rubber, the attachment position can be adjusted freely. * Please use by pasting at least two places on the bo... Read More
    Wall Thickness (mm)  Color  Black  Material  Chloroprene rubber  Suitable for  MKB□ 
    from S$3.29
    Min. 6 days
View : Grid List
Filter

32 Item(s)

Set Ascending Direction