[Pressure resistance 140 kg] A furniture fall prevention telescopic rod that prevents furniture from tipping over in the event of an earthquake. Seismic goods recommended for offices with many bookshelves and cabinets. You don't need nails or tools because you just stick it to the ceiling wit... Read More
It is firmly fixed even at a seismic intensity of 7. It is an adhesive mat that prevents falls and falls due to an earthquake by simply sticking it on the bottom of furniture due to its excellent adhesiveness. Since it can be peeled off cleanly, it does not damage the adhesive surface and can be ... Read More
A step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read More
Included Accessories Connecting bolt Material Polypropylene Color Gray Load capacity (t) 10
[Pressure resistance 150 kg] A telescopic type furniture fall prevention rod that stretches between the furniture and the ceiling to fix the furniture and prevent the furniture from tipping over in the event of an earthquake. With the H-shaped structure and jack method, the ceiling and furniture ... Read More
Type Refill stick Material PVC pipe coated steel pipe, ABS resin Color White
A step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with the attached bolts. The height can be adjusted in 3 steps.
* P... Read More
A rubber step plate that softens the impact and makes it easier to get in. It is made of rubber and has a non-slip surface treatment, and the sound is quiet. It is a design that harmonizes with the exterior.
A step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read More
Included Accessories Connecting bolt Material Polypropylene Color Gray
It is a furniture fall prevention plate that makes it difficult to fall down just by laying it under a bookshelf or cabinet. Since it can be cut with scissors or a cutter, the length can be adjusted freely. Since it is a translucent synthetic resin, it is less noticeable.
To prevent the cabinet f... Read More
It is a furniture fall prevention metal fitting that can fix bookshelves and cabinets. Secure the furniture and walls with wood screws. The metal fittings rotate according to the position of the wall surface.
For preventing bookshelves, cabinets, etc. from tipping over.
* Please attach it to a so... Read More
Included Accessories With 8 wood screws Type L-shaped bracket Material Steel (black zinc plating)
It is a door opening prevention stopper that locks the door by detecting the shaking of the earthquake. Prevents stored items such as documents from popping out due to shaking. After an earthquake, you can easily release the stopper by pushing the door.
For preventing stored items from popping ou... Read More
A double-sized simple air bed that can be used as disaster prevention supplies and leisure supplies. Easy installation, compact storage, ready to use in case of emergency. With a soft surface treatment and a volume of 22 cm, you can sleep on a hard floor without feeling the bottom. The air plug i... Read More
[One size fits all] A disaster prevention hood that is useful in the event of a disaster. Protects your head from falling objects. As it can be folded and stored, it is safe to prepare as a stockpile for disaster prevention!
A cot that can be used during disasters and leisure. The maximum thickness of the bed is 22 cm, so you won't feel the bottom even on a hard floor. Because it is space-saving, it can be used in cars and shelters. The pump is a double action type that supplies air even if it is pushed or pulled... Read More
Due to the special wave shape, the body does not sink easily and it is a comfortable air bed. Comes with pillows and a dedicated pump. The tops of the beds and pillows have a smooth, flocking finish. The attached pump adopts a double action type that sends air even if it is pushed or pulled. Sinc... Read More
Set Contents Air bed body, pillow, pump body, hose Color Beige Mass (g) 1460
Ideal for cold weather measures in the event of a disaster. Two types to choose from, a blanket type and a sleeping bag type. As it can be folded compactly, it is convenient to carry.
For protection against the cold when evacuating.
A lightweight and thick aluminum blanket that is useful in an emergency. It plays three roles: hanging, rolling, and wearing. It has a double structure consisting of an aluminum-deposited film that reflects body temperature and does not escape, and a foamed polyethylene sheet that blocks the temp... Read More
It is a fall prevention wire that prevents the fall of the LCD TV. Prevents falls and falls due to earthquakes, etc., and prevents injuries. Load capacity: Supports TVs up to 50Kg
A multifunctional blanket that can be used as a sleeping bag, a blanket, or a blanket by fastening the buttons. We use coral Meyer fabric with excellent heat retention.
For protection against the cold when evacuating.
A set of a blanket that can be used in 3 roles (sleeping bag, cover, blanket) and a simple air bed that can be easily set up and stored compactly! Great for sleeping at evacuation shelters in the event of a disaster!
It is a security system that "directly notifies the phone" of the intrusion of a suspicious person. Since it is a wireless system, it is easy to install. A set of dial-up main unit, sensor, and remote control key. The motion sensor responds to the movement of people (intruders / suspici... Read More
Easy to install without tools. The installation surface is a foamed polyethylene material that does not easily damage the ceiling or furniture.
Prevents furniture and fixtures from tipping over.
It is a security system that "directly notifies the phone" of the intrusion of a suspicious person. Since it is a wireless system, it is easy to install. A set of dial-up main unit, sensor, and remote control key. The motion sensor responds to the movement of people (intruders / suspici... Read More
A set of 5 simple air beds that can be used as disaster prevention products and leisure products. Easy installation, compact storage, ready to use in case of emergency. With a soft surface treatment and a 22 cm thick volume, you can sleep on a hard floor without feeling the bottom. Even women can... Read More
The fall prevention effect has been proven in a vibration test (equivalent to a seismic intensity of 7). The area of the installation surface is large, and the ceiling and furniture are firmly fixed even if it shakes. The installation surface is a foamed polyethylene material that does not easily... Read More
A step plate that prevents pedestrians from tripping and bicycles and motorcycles from tipping over. Since the surface is stepped, you can get in the car smoothly. The bottom shape makes it easy for water to escape, making it difficult for rain to wash away. Horizontal connection is possible with... Read More
Included Accessories Connecting bolt Material Polypropylene (PP) Color Black Allowable Load 10t or less
A loud 90dB doorknob alarm installed inside the door. A suspicious person is detected with a two-stage stance of an electrostatic sensor and a vibration sensor. (The electrostatic sensor reacts to materials where the doorknob is metal and the door plate does not conduct electricity.) Since it has... Read More
Mass (g) About 206 Power Input (V) DC4.5 (alkaline battery size AA x 3) Sound Pressure (dB/m) About 90
Since it uses a translucent synthetic resin, it is less noticeable. Since it can be cut with scissors, a cutter, etc., the length can be adjusted freely.
The slope shape eliminates steps and prevents pedestrians from tripping and bicycles and motorcycles from tipping over. You can get in the car smoothly without the car body jumping up. It is a non-slip surface step processing. Bottom shape that makes it easy for water to escape so that it will no... Read More
It is an adhesive mat that prevents falls and falls due to an earthquake by simply sticking it on the bottom of LCD TVs and furniture due to its excellent adhesiveness. Durability has been improved by using a material that does not easily deteriorate. It can be used repeatedly by washing it with ... Read More
It is a furniture fall prevention metal fitting that can fix furniture such as tons and cupboards. You can change the length of the chain according to the furniture and location.
* Please attach it to a solid part such as a wall core, pillar, camouflage, or crosspiece. It cannot be attached to pl... Read More
Included Accessories With 16 wood screws Material Steel (black zinc plating)
It is a security system that "directly notifies the phone" of the intrusion of a suspicious person. Since it is a wireless system, it is easy to install. It is a set product of dial UP body, vibration sensor, and remote control key. The vibration sensor responds to the opening and closi... Read More
It is inconspicuous because it can be mounted close to the wall. The installation surface is a foamed polyethylene material that does not easily damage the ceiling or furniture. The furniture and ceiling are firmly fixed by the jack method.
Prevents furniture from tipping over due to earthquakes,... Read More
It is a tension type furniture fall prevention telescopic rod that prevents furniture from falling in the event of an earthquake. The fall prevention effect has been proven in a vibration test (equivalent to a seismic intensity of 7). The area of the installation surface is large, and the ceiling... Read More
It is a security system that "directly notifies the phone" of the intrusion of a suspicious person. Since it is a wireless system, it is easy to install. A set of dial-up main unit, sensor, and remote control key. The motion sensor responds to the movement of people (intruders / suspici... Read More
Compared to the plastic step plate, it is more stable and less slippery due to the weight of rubber. The sound when getting over is also quieter than that made of plastic. Since it is a corner integrated type, it is a shape that makes it difficult for wheelchairs and automobiles to enter from the... Read More
If you breathe in, it becomes an air mat. It protects you from the coldness and humidity of the ground during sleep, which was often dissatisfied with life in a shelter.
Since it uses a translucent synthetic resin, it does not stand out. Since it can be cut with scissors, a cutter, etc., the length can be adjusted freely.