Scientific Research & Development Products / Cleanroom Equipment
Other Related Pages
- SIBATA SCIENTIFIC TECHNOLOGY Stirring Blade Set for M Type・It is an optional replacement blade for the propeller type dedicated to the stirrer M series.・If it is a Φ8mm shaft, it can be fixed at any position and used.・It is used for stirring general-purpose liquids. - Since it has a boss, it can be fixed at any position on the stirring bar with a set... Read MoreBlade Diameter (mm) (F-40)Φ40、(P-60)Φ60、(DF-70)Φ70、(T-80)Φ80from S$38.99Min. 33 days
- SIBATA SCIENTIFIC TECHNOLOGY SPC Midget Impinger D-2Capacity (mL) 30 Type D-2 typefrom S$119.90Min. 5 days
- SIBATA SCIENTIFIC TECHNOLOGY Safety coated screw mouth bottleThe outside of the "screw cap bottle", which is superior in terms of material, is coated with polyurethane. It helps prevent damage due to impact from the outside and prevents scattering in the unlikely event of damage. Alkalinity class DIN ISO 695, class2.from S$49.99Min. 4 days
- SIBATA SCIENTIFIC TECHNOLOGY Dispenser Handy Petter IThe EIA method using a microplate is very useful for tissue culture. By combining with 6 types of dedicated syringes, 22 types of dispensing volumes from 10 μL to 5 mL can be selected. You can select the number of dispensing in 5 steps with the variable knob. The syringe can be easily replaced. T... Read MoreDispensing Range (μL) 10~5000 Autoclave availability Impossible Pattern Setting Push button switching type Included Accessories Syringe 0.6, 1.5, 6mL x 1 each Specification With tresabifrom S$559.90Min. 5 days
- SIBATA SCIENTIFIC TECHNOLOGY Filter paper clip・Replacement option for A type/B type/C30 type/NW354 type. For low volume *Please select according to the filter paper size.from S$649.90Min. 5 days
- SIBATA SCIENTIFIC TECHNOLOGY Powder Reagent for Residual Chlorine Measuring Instrument DPD Method・Reagent used for residual chlorine measuring device DPD method, handy water quality meter residual chlorine AQ-201/101, effective chlorine concentration measuring kit AQ-201P.・When this reagent is added to test water containing free residual chlorine, it turns pale reddish purple to reddish pu... Read More
- SIBATA SCIENTIFIC TECHNOLOGY Residual Chlorine Measuring Instrument Potassium Iodide ReagentThis measuring instrument is a simple measurement method based on the reaction that causes a specific reaction when the DPD reagent is added to water containing residual chlorine, and exhibits a pale reddish purple color depending on the amount of residual chlorine. The reagent addition operation... Read MoreMeasuring Range (mg/L) 0.05~2.0 Mass of Main Unit (g) 300 (including case) Main Unit Dimensions (mm) 67×34×157 Measurement Method DPD method
- SIBATA SCIENTIFIC TECHNOLOGY Powder Reagent High Concentration of Residual Chlorine・A reagent used for the handy water quality meter Aquab Residual Chlorine High Concentration and Effective Chlorine Concentration Measurement Kit.・It uses the same coloring principle as the iodine titration method of the water supply test method, which turns pale yellow to dark yellow.As ONE Part Number 2-7323-02
- SIBATA SCIENTIFIC TECHNOLOGY Simple Water Quality Test Kit Simple Pack (Economical)At the site of process control and actual water measurement, it is required to judge how much water is contained, whether it contains more than a certain amount, and whether it is necessary to collect water and bring it back to the laboratory. There are many. In such a case, it is desirable to ha... Read More
- SIBATA SCIENTIFIC TECHNOLOGY General bacteria test paperThis general bacteria test paper is a simple test method using a test paper containing TTC as a coloring agent. It is a simple operation of dropping 1 mL of the test solution onto the test paper, or immersing it in the test solution and culturing it in a thermostatic chamber (35-37°C), then judgi... Read More
- SIBATA SCIENTIFIC TECHNOLOGY Square test tube for residual chlorine measuring instrument・Square test tube spare parts for residual chlorine measuring instrument DPD method.As ONE Part Number 6-9785-11 Type Square test tube Specification With vinyl cap
- SIBATA SCIENTIFIC TECHNOLOGY Coliform test paperA simple test method for bacteria using specially treated test paper, which is as simple as dropping 1 mL of the test solution onto the test paper or immersing it in the test paper and determining the average number of spots after culturing in an incubator (35 to 37 ° C). It is an operation. In a... Read More
- SIBATA SCIENTIFIC TECHNOLOGY Suction Filtration BottleIt is a filter bottle for suction that is generally used.Material Borosilicate glass
- SIBATA SCIENTIFIC TECHNOLOGY POV test paper (peroxide value test paper)You can directly inspect the peroxide value of edible vegetable oils that are liquid at room temperature, such as the fats and oils used and salad oils. It is very effective for checking the product at the manufacturing stage and grasping the distribution status. Immerse the test paper in the fat... Read MoreAs ONE Part Number 6-9632-01 Specification Color samples (0, 10, 30-50)
- SIBATA SCIENTIFIC TECHNOLOGY Stirring Blade for Tornado Fan (M Type Series)・It is an optional replacement blade for the propeller type dedicated to the stirrer M series.・If it is a Φ8mm shaft, it can be fixed at any position and used.・It is used for stirring general-purpose liquids. - Since it has a boss, it can be fixed at any position on the stirring bar with a set... Read MoreMaterial Stainless steel (SUS316)
- SIBATA SCIENTIFIC TECHNOLOGY Simple Pack Mini (Simple Water Quality Inspection Kit)・It is a small box type simple water quality test kit "simple pack" containing 6 pieces.・Packs contain individual desiccants, making them easy to carry as individual packs.・By purchasing additional color samples, multiple people can easily perform distributed simultaneous measurement... Read MoreSpecification 1 standard color chart included Number of Measurements 6
- SIBATA SCIENTIFIC TECHNOLOGY Square test tube with silicon cap・Spare parts for residual chlorine measuring instrument DPD method.・Used for colorimetric measurement with sample water.
- SIBATA SCIENTIFIC TECHNOLOGY Sample cell・A glass container for measuring water exclusively for the handy water quality meter "Aquab" AQ-201/-202/-101/-102.Capacity (mL) 10 Suitable for For AQ-201 / 202/101/102 Material Glass
- SIBATA SCIENTIFIC TECHNOLOGY Water check team Tap water・It is a simple water quality test kit "simple pack" for environmental education. An easy-to-understand explanation of the item is written in a story format. In addition, it is a convenient package that can be carried outdoors as it is.・There are 5 items for tap water and 5 items for ... Read MoreSet Contents 2 packs each TGK Part No. 371-80-30-61from S$29.99Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY Common sliding flat plugIt is a glass stopper for the same common female shape.
- SIBATA SCIENTIFIC TECHNOLOGY Separable Screw Clamp 3 pcsIt is a clamp for flat ground type separable flask. The maximum opening diameter is 20 mm with a screw type.from S$58.99Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY Nitrite Tester (for Food)The nitrite tester detects nitrite in food by the Griess reaction. Judgment is made by comparing with the colorimetric table exactly 1 minute after soaking in food. Suitable for inspection of ham, sausage, pickles, etc.Measuring Range (mg/kg) 0 5 10 30 50 100 TGK Part No. 371-80-81-06 As ONE Part Number 6-9634-01
- SIBATA SCIENTIFIC TECHNOLOGY Graduated cylinder with super grade bumperWith a bumper, it prevents rolling and damage if it falls over. Compared to a volumetric flask, the accuracy (margin of error) becomes rougher due to the larger body diameter. Higher accuracy than JIS R 3505 Class A accuracy. For adjusting reagent concentration, etc.Material Hard glass Specification With bumper to prevent falling Scale Yes
- SIBATA SCIENTIFIC TECHNOLOGY Common eggplant shaped flaskMaterial Borosilicate glassfrom S$48.99Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY Common Jim Roth coolerThe inside is a cooler that can efficiently cool the steam from the bottom by passing cooling water through the spirally wound glass tube.from S$299.90Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY FunnelIt is a funnel (spare part) that comes standard with the Φ47mm set of filter holders.Capacity (mL) 80 Suitable for For Φ25mmfrom S$89.99Min. 4 days
- SIBATA SCIENTIFIC TECHNOLOGY Perspective meter (standard type) with acrylic standA fluorometer is a device for measuring the degree of transparency of various types of water. The height (cm) of the water column when the sign sunk on the bottom can be clearly recognized for the first time is used as the frequency.Material (Stand) acrylic Mass (g) 250 Inner Diameter x Total Length (mm) 31×320 TGK Part No. 371-80-61-02 Outer Dimensions, Width W x Depth D x Height H (mm) 70×60×335 Specification Scale height 300mm
- SIBATA SCIENTIFIC TECHNOLOGY Pettenkoher water thermometer + alcohol thermometer typeIt is also used to measure the water temperature at the water sampling position prior to the water quality inspection. Submerge it in water, soak it in the measurement position for a few minutes, then pull it up to read the thermometer reading.Temperature Range (℃) -10~+50 Mass (kg) 0.3 Scale 1/2℃ Dimension (mm) Φ55×335from S$179.90Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY Glass Filtering Funnel Cylindrical TypeCylindrical funnel with a capacity of 140 mL and a glass filter.Material Borosilicate glassfrom S$67.99Min. 5 days
- SIBATA SCIENTIFIC TECHNOLOGY Resin color plate for DPD method・A spare part for comparing the coloring of the residual chlorine measuring instrument DPD method.・It can be replaced by sliding it up and down from the main body of the measuring instrument.from S$79.99Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY Ostwald Viscometer・A viscometer used for comparative measurement.・From No.1 to No.6 depending on the capillary diameter.・A relative viscometer for comparative measurements. The volume of the bulb is about 3mL.from S$129.90Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY Automatic Burette with PTFE Cock Body OnlySpecification Flat sliding connection. With PTFE cock. Color Transparentfrom S$539.90Min. 5 days
- SIBATA SCIENTIFIC TECHNOLOGY Volumetric flask + super gradeUsed to measure a certain volume. Also called a volumetric flask. It is a flat-bottomed flask with an elongated neck, usually with a line at the neck. Since the diameter of the neck part with the scale is thin, the accuracy of the scale is higher than that of a graduated cylinder of the same capa... Read MoreMaterial Borosilicate glass Color Transparentfrom S$38.99Min. 2 days
- SIBATA SCIENTIFIC TECHNOLOGY Handy Water Quality Meter Aquab・The AQ-201 model is a residual chlorine measuring instrument that uses this DPD method, and can measure residual chlorine concentrations up to 2.00 mg/L. It can be used for measuring residual chlorine in water in water.・The AQ-202 model uses the iodine method and can measure high-concentration... Read MoreTesting Capacity 10mL Measurement Wavelength 511±2nm Dimensions, Width W x Depth D x Height H (mm) 70×142×63 Memory Capacity 99 points Mass (g) About 250 Power Supply Alkaline batteries AAA x 4 Display Format Digital numbers Light Source LED Measurement Method Transmission absorption measurement Measurement cell Vials bottle with Φ24mm cap
- SIBATA SCIENTIFIC TECHNOLOGY Peroxide Value Measurement Kit POV Tester Type 5When oil-treated foods and nuts and seeds with a high oil content are stored for a long period of time, the action of enzymes in the air, humidity, heat, light, etc. gives off an unpleasant odor, which deteriorates the taste and reduces the commercial value. .. This product simply measures the pe... Read MoreScale of Color Chart 5、10、20、30 Measuring Range 5、10、20、30meq/kg Measurement Principle Iodine starch reaction Type Type 5
- SIBATA SCIENTIFIC TECHNOLOGY Bio Pipette (Short)It is used for biotechnology, tissue culture, and microbial culture, and has a shape suitable for transferring cells suspended in a medium like protoplasts. Since it is shorter than a normal measuring pipette, it is easy to operate, and since the hole diameter at the tip is large, it is also suit... Read MoreOverall Length (mm) 205 Top Outer Diameter (Φmm) 8 Pipette Type Biopipette Material DUROBAX (borosilicate glass-2) Specification With short cotton stopper
Filter by categories