Engine Related
Engine-related is a general maintenance tool for engine production and maintenance or its storage equipment. It is used for maintenance and repairs in automobile factories and can improve work efficiency. In order to quickly loosen the inside of the engine that has been tightly tightened, the material is often made of durable steel or steel. Concerning oil filters and oil elements that are often removed, convenience is emphasized, such as those that can be adjusted in length or directly gripped with oil filters.
Other Related Pages
- MonotaRO Tensioner wrench For Suzuki light S energy charge vehicles onlyThis is an auto tensioner compression / release tool exclusively for Suzuki mini vehicles S energy charge vehicles. When replacing the drive belt, auto tensioner, and ISG. * Please read the maintenance manual of each vehicle carefully before starting work, and be sure to follow the procedure. * N... Read MoreMaterial S45Cfrom S$299.90Min. 2 days
- JTC Oil filter wrench Cup typeRoHS directive (corresponding to 10 substances) Correspondence
- JTC Seal pullerTake it so that the seal is rolled up with a unique shape.RoHS directive (corresponding to 10 substances) Correspondencefrom S$47.99Min. 7 days
- MonotaRO Oil Filter Wrench Cup TypeAs it is a cup type, it is easy to hold and use! For removing the oil filter. *The product number has been changed to the size across flats, but the old product number is printed on the package. Current COFW63→Old COFW64・Current COFW64→Old COFW65 *Depending on the manufacturer and shape of the o... Read MoreShape 14 square
- KTC Cup Type Oil Filter Wrench* The compatibility of the main engine used may vary depending on the model, model year, and engine model, so check the outer diameter of the oil filter. * This product is for manual use. Do not use power tools such as impact wrenches. * Do not use anything other than a filter paper replacement o... Read More
- MonotaRO Oil Filter Wrench for Toyota, Compatible for Filter Paper Replacing TypeThis is a special tool for attaching and detaching aluminum and resin filter paper replacement type oil filters used in Toyota vehicles. Detachment of oil filter * Some models may not be available depending on the model year. Carefully check the shape and mounting position of the filter. When tig... Read MoreShape 14P Outer Diameter (Φmm) 79
- MonotaRO Oil Filter Wrench Pliers TypeSince it can be adjusted in 3 steps, it can be used for oil filters of various sizes. With a grip, the handle is easy to grip, and you can remove the hardened filter. For removing the oil filter. * Since the grip does not have an insulating function, never use it for things where electricity is f... Read MoreMaterial S45C
- MonotaRO Hoose Remover PullerA special tool for pulling out the hose from the pipe. At the connection part of the fuel hose or vacuum hose, insert the tip between the pipe and the hose (border) (silver on the hose side, black on the pipe side), and you can remove the hose from the pipe simply by grasping the main body. is. W... Read More
- MonotaRO Oil filter wrench Swing Grip Band typeAn oil filter wrench that adjusts and holds the length of the band. Since the angle of the handle can be adjusted (180 °), it can be used in various situations. Attach a wrench to the oil filter, hold the band by hand, and turn it in the loosening direction to tighten the band. There is a protrus... Read More
- MonotaRO Seal puller setA special spiral shape can be used to wind up the seal or ring. Anyone can remove the oil or ring simply by inserting the tip under the oil seal, fixing the shaft with the left hand, and then rotating the handle with the right hand. It is possible to easily pull out an O-ring that is hard to come... Read More
- MonotaRO Oil filter wrench AdjustableIt can be used for both tightening and loosening according to the size of the oil filter. For tightening and loosening the oil filter * Do not use if there are any abnormalities such as cracks, chips, wear, or deformation. * Since it is a general-purpose product that fits a wide range of sizes, w... Read MoreIncluded Accessories Plug-in angle conversion adapter Suitable Diameter (Φmm) 63~102
- MonotaRO Line hose clamp set straight typeIt is used when you want to temporarily stop the flow of radiator hoses, heater hoses, etc. Made of plastic that is lightweight, easy to use, and does not damage the hose. It also has a lock function, and it is possible to maintain the blocked state even if you release your hand. The large one ca... Read MoreMass (g) (Large) 120 ・ (Medium) 70 ・ (Small) 40
- MonotaRO With seal puller 7-stage adjustment functionIt is a convenient puller that can remove the oil seal by the principle of leverage just by inserting the tip of the nail into the back side of the oil seal and pushing it. Since the angle can be adjusted in 7 steps, it can be used according to the oil seal. It is very convenient because you can ... Read MoreSpecification 7-step angle adjustment
- Griffin Cup type oil filter wrenchA must-have for professionals and Sunday mechanics No matter how tightly locked the oil filter element is, it can be easily loosened. * Since this product is manufactured for genuine oil elements, it may not be possible to use it if the oil elements are not genuine parts. Be sure to stop the engi... Read Moreplating Chrome plating
- MonotaRO Hose Pincher SetA tool used to stop fuel lines and vacuum lines. It can be easily used by simply pinching the hose and tightening the thumbscrew during the time. Since the main body is small, it is convenient in narrow places and complicated places such as motorcycles. Suitable for use in fuel hoses and vacuum h... Read MoreSuitable Diameter (Φmm) 0~20
- MonotaRO Piston Ring CompressorWhen assembling the piston to the cylinder, the ring part is wrapped around and the tightening ring is compressed for smooth insertion. When inserting the piston ring into the cylinder in a compressed state * Please do not use it for any purpose other than its intended purpose.
- MonotaRO Oil filter wrench For Toyota cars Lexus Filter paper replacement typeThis is a special tool for attaching and detaching aluminum and resin filter paper replacement type oil filters used in Toyota vehicles including Lexus. * Some models may not be available depending on the model year. Carefully check the shape and mounting position of the filter. When tightening, ... Read MoreShape 14P Inner Diameter (Φmm) 64.5 Outer Diameter (Φmm) 90
- MonotaRO Exhaust muffler hanger pliersWhen removing the muffler ・ It is a plier that allows you to easily remove the muffler hanger with a stopper that is difficult to remove even if you pull it. (If you apply a lubricant, it will come off more easily than usual.) For removing the muffler hanger * Please do not use it for any purpos... Read More
- MonotaRO Lock Ring (C-Type Ring) PlierA special tool for attaching and detaching lock rings (C-shaped rings) that do not have holes. It can be used with the lock ring (C-shaped ring) that does not get caught and is used in missions and transfers. Since the tip is non-slip processed, you can work safely. For shafts that open when gras... Read More
- MonotaRO Damper stopper clampIt is a tool to fix to prevent free fall due to the weight of the damper and bonnet weakened by oil leakage and gas release. It can also be used to fix the damper of a vehicle equipped with a large spoiler that is retrofitted. It becomes a stopper by attaching it to the shock rod part of the bump... Read More
- MonotaRO hose clamp pliersA universal tool for removing clamps. Since the teeth are latticed, it does not slip and is difficult to come off from the gripped hose clip. It can also be used in narrow places and deep situations. It can be used from various directions and is convenient. Detachment of the spring type hose clip... Read More
- MonotaRO Oil filter wrench Detachable for both use Slide typeIt is a convenient dual-purpose type that can be loosened as well as retightened. A slide type oil filter of various sizes can be attached and detached. For attaching and detaching the oil filter * Never work with the oil filter heated as it may cause burns. * Allow the oil filter to cool complet... Read MoreMaterial Steel Gripping Size (Depth) 18mm
- MonotaRO Locking pinch-off pliersIt blocks the flow of liquid by sandwiching a radiator hose or fuel hose. Since it is a vise pliers type, you do not need to hold it once you pinch it. It can also be used to prevent leakage of copper pipes in the event of a leak. Suitable for use in radiator hoses and brake hoses. * Please do no... Read More
- TOP KOGYO Filter chain wrenchUsed to remove the oil filter. It is strong and has a good bite. TW-230 has a chain drop prevention. Even large vehicles are possible.
- MonotaRO Oil filter cutterThe oil element can be disassembled into an inner filter paper and an outer case. Since it can be sorted, it helps to reduce disposal costs. With the oil element set, turn it with an oil filter wrench to cut the bottom edge. * Do not use for anything other than its intended purpose.Filter Diameter (Φmm) 60~140 Material (Blade) HSS
- MonotaRO Vice pliers type oil filter wrenchSince it is a vise pliers type, you do not need to hold it once you pinch it. If you grip it, all you have to do is turn it easily! For removing the oil filter * Please do not use it for any purpose other than its intended purpose. * Do not use for tightening as it may damage the oil filter.Material Chrome vanadium Suitable Diameter (Φmm) 55~118
- MonotaRO Oil filter wrench for truckCan be used according to size For installing and removing oil filters for large vehicles such as trucks and buses * Ratchet wrench is not included
- KTC Large diameter cup type oil filter wrenchBy adopting the insert manufacturing method, iron (steel material) is used for the drive corners, and the aluminum part is also thickened to improve proof stress. Detachment work of engine oil filter cartridges for 2-4t class trucks, buses, etc. * Even if the engine type is the same, the size may... Read MoreSpecification For large vehicles
- MonotaRO Belt hook toolA dedicated auxiliary tool used when attaching drive belts for automobiles and machinery. If you use this belt hooking tool, you can easily attach and detach the single drive belt, so you can shorten the work time. You can also inspect the V-belt and timing belt in the engine room. Since the shap... Read MoreShank Diameter (Φmm) 6.5 Handle Diameter (Φmm) 30
- MonotaRO Oil pan separatorThis is convenient when removing the oil pan that is stopped by seal packing. After removing the bolt of the oil pan, hit the blade of this product against the gap between the main body and the oil pan with a hammer or the like. * Please note that hitting too hard may damage the main body, blade,... Read MoreMaterial SK-5
- MonotaRO Oil Filter Wrench Adjustable ExclusiveSince it is an adjustable type, it can be used for oil filters of 60 mm to 80 mm. Detachable only * Please do not use it for any purpose other than its intended purpose.
- MonotaRO Pulley Hold Wrench V Belt TypeIt is a tool for fixing pulleys and circular parts so that they do not rotate together when they are attached or detached. For attaching / detaching pulleys and circular parts * The belt cannot be replaced. * Cannot be used when using an impact wrench together. * Due to the structure, it cannot b... Read MoreMaximum Operation Load 130N・m
- MonotaRO Piston ring pliers with safety stopperComes with an adjustable safety stopper. A tool for expanding the piston ring when removing or attaching the piston ring to the piston. This will make your work easier. It is also convenient with an adjustable safety stopper. For removing and installing piston rings * Please do not use it for any... Read MoreSuitable for (Ring thickness) 1.2 ~ 6.3mm
- MonotaRO Radiator leak & cap tester for domestic carsBy attaching an adapter compatible with the radiator and pressurizing the cooling water channel through the radiator, damage and leakage of the cooling system can be inspected. By exchanging the attachment, it can be used for all domestic cars. You can also check the valve opening pressure of the... Read More
- MonotaRO Hose clamp pliers for CLICK-R onlyA reusable CLICK / CLICK-R standard one-touch hose clamp that is often used in European cars. It is a plier that can be attached and detached. CLICK / CLICK-R standard one-touch hose clamp compatible * Do not use for any other purpose.Material Resin, iron Mass (g) 300
- SIGNET 2WAY oil filter wrenchSuitable Size (Φmm) 63-102 Drive angle (DR) For both 3/8 ”and 1/2”
- MonotaRO Oil Filter Wrench for Imported CarsIdeal for imported cars! Aluminum die-cast oil filter wrench. * Please check the size as it may not be available depending on the model and engine shape.Mass (g) 150 Cup size 74mm (14 square)
- MonotaRO Line hose clamp set vent nose typeThe bent nose type is very convenient because it allows you to grab the hose even through gaps that the straight type could not enter. Also, like the straight type, it is used when you want to temporarily stop the flow of radiator hoses, heater hoses, etc. Made of plastic that is lightweight, eas... Read MoreMass (g) (Large) 130 ・ (Medium) 90 ・ (Small) 50
- Lisle Stretch belt removal toolCombination removal and installation tools for most stretch belt applications used in many accessory drive systems. A unique magnetic surface holds the tool in place on the pulley. Helps prevent damage to the belt and pulley during removal and installation. You can use a compact one-piece tool on... Read MoreRoHS directive (corresponding to 10 substances) Correspondence
Filter by categories