Tire & Wheel Cleaning
Tires and wheels are easily damaged by oil stains from brake dust and asphalt and are difficult to remove. For cleaning tires, the lineup includes products that remove dirt without degrading the rubber and retain the gloss for a long time. Since it is difficult to remove dirt from brake dust for wheels, dirt that cannot be removed by washing with water can be easily removed by using a special brush or cleaning agent.
Other Related Pages
- SOFT99 Corporation Fukupika wheel dedicated wipe sheetSimply wipe to remove brake dust and persistent oil stains on the wheels. Unlike the spray type, there is no need to worry about it splashing on the tires, and the finish is surprisingly quick and shiny. It can be used for a wide range of materials such as aluminum wheels, steel wheels, and resin... Read MoreClassification of the Hazardous Non-dangerous goods
- VOODOORIDE Metal polish Metal polishing & protection cream (compound & protection agent for metal material)A compound exclusively for bare metal (metal that has not been surface treated). Metal parts that have lost their original brilliance and attractiveness due to discoloration due to aging and surface oxidation (rust), such as stainless mufflers, old aluminum wheels, and rusted plated parts, can be... Read MoreClassification of the Hazardous Non-dangerous goods
- VOODOORIDE Chrome cleaner (compound & protective agent for metal materials)It not only removes dirt, but also forms an oil-based protective film to protect the chrome plating from dirt (dust, fingerprints, rain stains) that can cloud the chrome plating for two months. * Cannot be used on painted surfaces or resin products (Car grills and wheels may be painted in a plati... Read MoreSuitable Material Chrome plating products Classification of the Hazardous Non-dangerous goods
- SOFT99 Corporation 99 workshop Modoshi Corps wheel iron powder melting cleanerA powerful acid-based cleaner that can easily remove brake dust that has been seized and stuck due to aging, which cannot be completely removed by the wheel cleaner used for car washing. The strong acid cleaner liquid dissolves the iron powder that sticks to the surface of the wheel paint without... Read MoreClassification of the Hazardous Non-dangerous goods
- SUZUKI MOTOR Aluminum Clean Spray BottleCapacity (L) 1 Classification of the Hazardous Non-dangerous goodsfrom S$9.69Min. 5 days
- GYEON Q2M Tire Express Part No. (Q2M-TE100) 1000 mlIt is a tire protectant that keeps the natural black color like a new tire. It spreads well and is easy to spread and can be used on both tires, whether wet or dry. As it is a water-based type, it is gentle on tires and is easy and beautiful. * Please refrain from using the product in direct sunl... Read MoreClassification of the Hazardous Non-dangerous goodsfrom S$119.90Min. 11 days
- AUTOGLYM Polishing Cleaner Metal Cleaner Metal PolishMetal Polish is a cleaner for polishing metals (aluminum, chrome, brass, stainless steel, etc.). It can polish metal surfaces safely and quickly, is very easy to control, and you can adjust the degree of polishing by adjusting the amount of force. For chrome-plated plastic parts and smooth metal ... Read MoreClassification For tires and wheels Classification of the Hazardous Non-dangerous goodsfrom S$59.99Min. 10 days
- BLUE MAGIC BLUE MAGIC Metal Polish CreamRemoves oxidation, rust, dirt, etc. on the metal surface and coats with silicon. It can be used for aluminum, magnesium, gold, silver, copper, stainless steel, etc. For glossing aluminum foil. * Be sure to use a soft cloth to polish. It cannot be used for painting. * It may be separated, but ther... Read MoreClassification of the Hazardous Non-dangerous goods
- SOFT99 Corporation Wheel CleanerIt cleans the wheels that cannot be removed by car wash and restores the brilliance of new products. Wheel-friendly cream type.Classification of the Hazardous Designated combustibles Name of The Hazardous Flammable solids Quantity of the Hazardous 0.065kg
- Asahi Metal Polish Metal Polish MPAluminum, plating, stainless steel, and other metals have a wonderful luster as if they were chrome-plated. Mirror finish can be achieved even faster by using a machine such as a polisher or a drill. Ultra-fine particle paste type (oil-based) wheel with little scattering Approximately 30 Approxi... Read MoreAbrasive Grain Size 1 micron on average Color White Mass (g) 200 Capacity (g) 200 Classification of the Hazardous Non-dangerous goods
- 3M Magnetium & Aluminum Polish 38529A cleaner and polish that removes oxide film, rain stains, dirt, brake dust and other debris from magnesium and aluminum wheels that have not been treated with a clear coat, and restores brilliance. (Silicon / wax component combination) * Cannot be used for clear coat processed items.Type Blistering Classification of the Hazardous Designated combustibles Name of The Hazardous Flammable liquids Quantity of the Hazardous 0.283kg
- GYEON Q2M Tire Express Part No. (Q2M-TE40) 400 mlIt is a tire protectant that keeps the natural black color like a new tire. It spreads well and is easy to spread and can be used on both tires, whether wet or dry. As it is a water-based type, it is gentle on tires and is easy and beautiful. * Please refrain from using the product in direct sunl... Read MoreClassification of the Hazardous Non-dangerous goodsfrom S$57.99Min. 11 days
- UNiCON Tire & Leather Wax 248SBNo need to treat with containers that deal with industrial waste problems This price is 18L!Discontinued
- Ichinen Chemicals (Former Taiho Kohzai) Metal polish + L-27Removes rust and dirt from metal and restores the original beauty of metal. Prevents discoloration of metal. Metal polish, cleaning, stain removerMain Application Metal Classification of the Hazardous Non-dangerous goods Feature PolishDiscontinued
- Red Sun Aluminum foil coatingIt provides outstanding durability by forming a polymer film on the surface while penetrating the aluminum itself. In addition to abrasion resistance, impact resistance, heat resistance, and rust resistance, this coating has excellent features on metal parts and FRP parts of cars.Discontinued
- Musashi Holt Motantan Aluminum Wheel Stain Removal KitIdeal for cleaning aluminum wheels. With a glossy protective ingredient, it coats the surface after wiping it off. With compoundContainer Laminated tubeDiscontinued
- Red Sun Aluminum foil cleanerAmazing finish recognized by the pro shop! Oxidized brake dust is removed by a newly developed liquid reaction! Apply cleaner solution for 5 minutes. After that, all the dirt on the brake dust will be removed just by washing with water. A newly developed cleaner with a new concept that is friendl... Read MoreAcidic / Alkaline Weakly alkalineDiscontinued
- SOFT99 Corporation Shampoo for exclusive use of aluminum wheelA shampoo for aluminum wheels that has an alkaline liquid effect that effectively removes dirt from the wheels. The surface of the attached sponge uses microfiber that can gently wash delicate wheels and a special mesh sheet to scrape off dirt. It is thin and can effectively wash curved surfaces ... Read MoreSet Contents This agent, special sponge Acidic / Alkaline alkalinityDiscontinued
Filter by categories