All Category

Car Window Cleaning

Use a washer fluid or wind cleaner to clean the window. Although it is a part where oil film and scales are easily attached, if it contains a surfactant, stubborn dirt can be removed quickly. In cold regions and in winter, using a window washer solution that can withstand temperatures up to -40 ° C and -50 ° C is effective in preventing freezing. The glass on the inside of the car is often stained with dirt or dirt, but use ethanol or other volatile interior window cleaners.
View : Grid List
Filter

21 Item(s)

Set Ascending Direction
  1. Window fukupika
    SOFT99 Corporation Window fukupika
    A semi-dry type glass cleaning sheet with a special 3-layer structure that does not leave after wiping or uneven wiping. The upper and lower sweeping layers scrape off dirt, and the middle hold layer adsorbs and holds it. Achieves a clear finish without having to wipe it twice. It can also be use... Read More
    Sheet Size (mm)  265×300  Trusco Part No.  479-3889  Mass (g)  50  Ingredient  Alcohol  Classification of the Hazardous  Non-dangerous goods  Material  Synthetic fibers 
    Rating:
    90%
    from S$4.79
    Min. 2 days
  2. Good cloud stop
    Prostaff Good cloud stop
    It is a wet sheet that stops the cloudiness of the inside of the glass and the mirror. Just wipe the cloudy glass to remove dirt and ensure a clear view. Also, if you wipe it in advance, it will have a strong "anti-fog effect". Uses hand-friendly vegetable alcohol.
    Sheet Size (mm)  About 220 × 330  Feature  Cloudy stop  Classification of the Hazardous  Non-dangerous goods 
    from S$4.49
    Min. 2 days
  3. FUKUPIKA Window Anti-Fog Reinforced Type
    SOFT99 Corporation FUKUPIKA Window Anti-Fog Reinforced Type
    Just by wiping it quickly, it has a strong anti-fog effect at the same time as cleaning the glass. It removes not only dirt on the outside of the window, but also sebum dirt such as hand stains that are difficult to remove on the inside and sticky tobacco tar. It doesn't take up much space, s... Read More
    Sheet Size (mm)  265×300  Classification of the Hazardous  Non-dangerous goods 
    Rating:
    83%
    from S$4.19
    Min. 2 days
  4. Window Fukupica Handy Wiper
    SOFT99 Corporation Window Fukupica Handy Wiper
    A handy wiper that can be easily wiped from corner to corner of the windshield while sitting on the seat. Easy and easy cleaning of the narrow inside of the windshield! Even the steep slopes and curves inside the windshield, and the narrow gaps in the back, which you had a hard time with, can be ... Read More
    Included Accessories  10 windows fukupica  Sheet Size (mm)  265×300  Overall Length (cm)  About 35  Classification of the Hazardous  Non-dangerous goods 
    Rating:
    90%
    from S$14.99
    Min. 2 days
  5. Garaco compound cloth
    SOFT99 Corporation Garaco compound cloth
    Uses an abrasive that is also used to polish optical lenses! It can strongly clean the oil film and old coating agent remaining on the glass without scratching the glass surface. After work, the finish is neat without leaving an oil film or dirt on the glass surface, making it ideal for base trea... Read More
    Sheet Size (mm)  200×300  Trusco Part No.  835-6668  Feature  Oil film removal 
    Rating:
    86%
    from S$6.39
    Min. 2 days
  6. Window Clean Window Cleaning Cloth Prestige
    Prestige Window Clean Window Cleaning Cloth Prestige
    Clean windows! Good visibility and no haze! Removes tobacco tar, hand stains, and dust adhering to the inside of the window glass. Removes oil film and dirt adhering to the outside of the window glass. Removes dust and oil from the dashboard, steering wheel, and rearview mirror in the car. Remove... Read More
    Other  10 sheets  Sheet Size (mm)  225×300  Size (mm)  225×300  Classification of the Hazardous  Non-dangerous goods  Material  Rayon nonwoven fabric  Feature  Yani, hand red, dust, oil film remover 
    Rating:
    100%
    from S$4.39
    Min. 2 days
  7. Glass cleaner
    Kyowa Shiko Glass cleaner
    Quickly wipe off dirt and oil slicks! The dirt and oil film that cause cloudiness are removed, and the visibility is clear. Thick type and soft to use.
    Size Per Sheet (mm)  About 300 × 200  RoHS directive (corresponding to 10 substances)  Correspondence  Feature  Dirt, dirt, oil film removal  Classification of the Hazardous  Non-dangerous goods  Material  Polyester, rayon 
    Rating:
    40%
    from S$1.99
    Min. 2 days
  8. Cloudy cleaner
    Kyowa Shiko Cloudy cleaner
    With a single wipe, the visibility is refreshing! Thick sheet that can be used on both sides. Since it is a wet type, the solvent does not scatter like the spray type.
    Size Per Sheet (mm)  About 300 × 200  Feature  Cloudy stop  RoHS directive (corresponding to 10 substances)  Correspondence  Classification of the Hazardous  Non-dangerous goods  Material  Rayon non-woven fabric 
    from S$2.09
    Min. 2 days
  9. A good window cleaner
    Prostaff A good window cleaner
    A wet cloth that cleans your car from the window to the room with a quick wipe. The double effect of 3D mesh structure + large size (sheet size about 225 x 299) catches dirt without letting it escape, and uses DuPont's non-woven fabric that is durable and excellent in wiping. It also cleans g... Read More
    Mass (g)  124  Dimensions (H x W x D) (mm)  215×135×15  Sheet Size (mm)  220×330  Feature  Hand red / crab removal  Classification of the Hazardous  Non-dangerous goods 
    from S$4.79
    Min. 2 days
  10. Water spot cleaner for glass
    CAR MATE Water spot cleaner for glass
    The synergistic effect of triple abrasive particles and special fiber pad removes water spots (rain stains and scales) on the glass surface, stubborn oil film, and old glass coat film, and restores transparent glass. Three types of abrasive particles "crush, peel, and remove" oil slicks... Read More
    Capacity (mL)  100  RoHS directive (corresponding to 10 substances)  Correspondence  Classification of the Hazardous  Non-dangerous goods  Feature  Oil film / coating agent removal  Included Accessories  Special fiber pad  Ingredient  Water-soluble solvent, abrasive  Acidic / Alkaline  Weakly alkaline  Type  liquid 
    Rating:
    53%
    from S$14.99
    Min. 2 days
  11. Clean view cloudy weather stopping sheet A-67
    Ichinen Chemicals (Former Taiho Kohzai) Clean view cloudy weather stopping sheet A-67
    Eliminate "cloudiness" with a quick wipe. If you wipe the areas that are prone to cloudiness in advance, you can prevent "cloudiness". It also cleans the glass. It's refreshing after wiping. A neutral type that is gentle on the hands. Removes oil film from automobile glass... Read More
    Feature  Cloudy stop  Classification of the Hazardous  Non-dangerous goods 
    from S$2.99
    Min. 2 days
  12. Dunk water-repellent wet cloth
    Prostaff Dunk water-repellent wet cloth
    A new wet cloth from the "Dunk Series" that repels water droplets and improves visibility on rainy days just by wiping the window glass! You can remove dirt and apply a water-repellent coating at the same time by simply wiping it. Easily removes dirt after rain, bird droppings, insect d... Read More
    Mass (g)  132  Dimensions (H x W x D) (mm)  230×145×22  Classification of the Hazardous  Non-dangerous goods 
    Rating:
    80%
    from S$6.59
    Min. 5 days
  13. B & Y + Clear view cross + For outer window
    Handy Crown B & Y + Clear view cross + For outer window
    Ideal for outer window glass! Hyper microfiber + special honeycomb weave processing & PP pile fabric adopted! 2WAY specification with soft and hard double face processing! Cleanly scrapes stubborn dirt on the outer window! Chuck case convenient for storage For wiping insects and dirt on the o... Read More
    Mass (g)  28  Dimension (mm)  300×350  RoHS directive (corresponding to 10 substances)  Correspondence  Classification of the Hazardous  Designated combustibles  Material  Polyester nylon  Name of The Hazardous  Threads 
    from S$12.99
    Min. 7 days
  14. Window fluffy anti-fog dry
    SOFT99 Corporation Window fluffy anti-fog dry
    A dry sheet type anti-fog sheet in a car that instantly eliminates cloudiness by simply wiping the cloudy glass. The strong anti-fog effect that lasts for about one month prevents the recurrence of cloudiness. The sheet with excellent scraping performance cleans fingerprints and sebum stains and ... Read More
    Dimensions, H x W (mm)  350×300  Feature  Cloudy stop  Classification of the Hazardous  Non-dangerous goods  Ingredient  Nonionic surfactant / preservative  Material  Synthetic fibers 
    from S$7.19
    Min. 6 days
  15. Glass compound cloth
    CCI Glass compound cloth
    Easy work just by wetting and polishing the glass. The stubborn oil film and fluorine-based water repellent also fall off. Ideal for pretreatment of glass water repellent.
    Classification of the Hazardous  Non-dangerous goods  Feature  Oil film and water repellent drop 
    Discontinued
  16. Beautiful window glass
    AUG Beautiful window glass
    Reliable domestic product, deodorant Epolion combination
    Discontinued
  17. Window cloudy swiss soft pack
    AUG Window cloudy swiss soft pack
    Dimensions (H x W x D) (mm)  225×130×15  Mass (g)  80  Feature  Cloudy stop 
    Discontinued
  18. For car cleaning windows
    Papertec For car cleaning windows
    It removes dirt that cannot be removed by wiping the window glass of a car or the inside of a car, and even glare of an oil film.
    Feature  Dirt, oil film removal  Classification of the Hazardous  Non-dangerous goods 
    Discontinued
  19. Globe Penguin Hand for Inner Window
    Prostaff Globe Penguin Hand for Inner Window
    An inner window glove made of double-sided microfiber material that eliminates cloudiness by simply wiping it. The black cloth surface of ultra-fine fibers with long hair quickly absorbs fine water droplets that cause cloudiness and clears the field of vision. The uneven waffle woven gray cloth s... Read More
    Dimensions (H x W x D) (mm)  285×190×30  Mass (g)  54  Feature  Cloudy stop 
    Discontinued
  20. Cloudy cloth cross X clear
    CAR MATE Cloudy cloth cross X clear
    Just by wiping the cloudy glass directly, the "anti-fog component" enclosed in the microcapsules on the surface of the cloth reacts with the moisture on the glass surface to stop the cloudiness.The "anti-fog component" gradually exudes. Can be used repeatedly (for about 12 win... Read More
    Size  120×200mm  Material  Acrylic, nylon  Shape  Bag type  Feature  Cloudy stop  Classification of the Hazardous  Non-dangerous goods  Ingredient  Surfactant 
    Discontinued
  21. Anti-fog cloth
    SO UP Anti-fog cloth
    A magical cloth that strongly removes dust and dirt adhering to the glass surface that causes cloudiness with special structural fibers to create a glass surface that does not become cloudy. Easy without the need for chemical agents. Gather weave processing strongly removes dust and dirt. Comes w... Read More
    Material  80% polyester, 20% nylon  Dimension (mm)  About 350 × 300  Feature  Cloudy stop  Classification of the Hazardous  Designated combustibles  Name of The Hazardous  Threads 
    Discontinued
View : Grid List
Filter

21 Item(s)

Set Ascending Direction