It is a waterproof remote controller for daily life that is safe even if it gets wet. Zoom operation is also possible with compatible compact digital cameras. Comes with a strap loop.
* Batteries cannot be replaced or used underwater. * Not compatible with compact digital cameras released before ... Read More
This remote code is ideal when you want to avoid camera shake, such as in close-up photography, or when you want to perform release operations away from the camera. Since it can be fixed while pressing the shutter button, it is also convenient for long-exposure (bulb) shooting. MC-DC2 can also be... Read More
AF lock is possible like the shutter button on the body. The total length of the cord is 60 cm. Lightweight and compact design with excellent portability. Release is possible without pressing the shutter button on the camera body. This is convenient for nighttime shooting where camera shake is li... Read More
Remote controller for EOS. Shutter operation is possible at a distance of about 5 m. Two modes can be selected: immediate release and release after 2 seconds.
A conversion adapter for connecting the timer remote controller TC-80N3 to an EOS digital camera equipped with an E3 type remote control terminal. It can be used only with EOS digital cameras equipped with an E3 type remote control terminal released after 2010.
* Cannot be used with the PowerShot... Read More
Use this to determine the exposure when you cannot obtain the proper exposure by TTL metering of the camera, such as when copying a subject with high contrast such as printed matter with black characters on a white background.
* Not suitable for white balance presets.
You can press the camera halfway and remotely control the release. If you want to prevent camera shake even a little in close-up photography, or if you want to operate the shutter button away from the camera within the range of the cord length, fix it with the shutter button pressed and expose fo... Read More
You can get a softer and lighter release feeling by screwing it into the release socket of the shutter button. The main body is made of brass and has the "Nikon" engraving on it, and the upper surface is made of ebonite resin, which has a soft feel and feels good to the touch, and the u... Read More
Wired remote controller with built-in timer function. The self-timer, interval timer, and long-exposure timer can be set every second from 1 second to 99 hours 59 minutes 59 seconds. In addition, the number of shots can be set from 1 to 99. Compatible with new remote control sockets. The cord len... Read More
It is a wireless remote controller (transmitter) that uses radio waves in the 2.4 GHz band and enables comfortable remote control shooting even if there is a shield between transmission and reception. You can use various functions such as autofocus and continuous shooting by pressing halfway, mov... Read More
By connecting to the camera via Bluetooth (R), you can start / stop zoom operation, still image shooting, and movie shooting. In addition, you can adjust the manual focus and select items with the multi-selector. It also has Fn1 / Fn2 buttons to which functions can be assigned from the camera.
* ... Read More
You can set an interval timer that shoots at set time intervals and expose for a long time. The display panel is illuminated. It also has a shutter button lock for long-time exposure (bulb) shooting and a function to notify you with an electronic sound every second during release. (About 0.85 m)
Power Supply 1.5V LR03 alkaline AAA battery x 2 Cable Length (m) About 0.85 Color Black
One set of transmitter and receiver. The power of the receiver is supplied from the 10-pin terminal of the camera body. Equipped with 2 channels, such as a delay mode that can be released after 3 seconds. It also has an auto-trigger mode that releases the shutter when an object crosses between th... Read More
You can release the shutter of the camera wirelessly. Zoom operation is also possible with some cameras. You can also release the camera shutter wirelessly. In addition, compact digital cameras allow zoom operation and image feed during playback. The K-5 / K-7 / K20D / K10D can be used from the b... Read More
A remote release with a Φ2.5mm terminal. As with the camera, pressing the shutter button halfway will bring it into focus, and then pressing it all the way in will take a picture. You can lock the shutter button by sliding it during bulb shooting or continuous shooting. The L-shaped conversion ca... Read More
A remote switch with an interval timer. The setting items are delay termer, exposure time, interval, number of shots, alarm ON / OFF. Set with an interactive menu, just like a typical digital clock. Built-in LED light for LCD screen, easy to use for long-exposure photography at night. Easy-to-obt... Read More
Main Unit Dimensions (mm) 110×45×22 Mass (g) About 72 Cable Length (cm) About 90
Remote switch with a cord length of 80 cm compatible with the new remote control socket
* When using with EOS60Da, the remote controller adapter RA-E3 included with EOS60Da is required.
A soft shutter button that is screwed onto the shutter button of the camera. By increasing the area and height of the shutter button, it is easier to release the shutter, which helps to suppress camera shake and improve quick shooting. The dent in the center fits your fingers. It can be used with... Read More
Diameter (Φmm) (Approx.) 10 Main Materials Made of brass Type Screw-in type
It can be attached to the 10-pin terminal of a compatible camera and the wireless remote controller WR-T10 can be used to wirelessly release or simultaneously release multiple unmanned cameras. In addition, interlocking release of multiple cameras equipped with WR-R11a and WR-R11b, interval timer... Read More
Camera specifications Camera equipped with 10-pin terminal
You can wirelessly release or release multiple unmanned cameras at the same time by attaching it to the accessory terminal of a compatible camera and using the wireless remote controller WR-T10. In addition, interlocking release of multiple cameras equipped with WR-R11a and WR-R11b, interval time... Read More
Camera specifications Camera equipped with accessory terminal
A shooting accessory that can be attached to the remote terminal of the camera to release the shutter without pressing the shutter button directly. Prevents blurring during slow shutter shooting that expresses the movement of rivers and the sea, and bulb shooting that is often used for fireworks.... Read More
Mass (g) 50 Overall Length (cm) About 100 (cord length about 90) Type Canon RS-E3
A remote switch with an interval timer. The setting items are delay termer, exposure time, interval, number of shots, alarm ON / OFF. Set with an interactive menu, just like a typical digital clock. Built-in LED light for LCD screen, easy to use for long-exposure photography at night. Easy-to-obt... Read More
Main Unit Dimensions (mm) 110×45×22 Mass (g) About 72 Cable Length (cm) About 90
Multi-function wireless remote switch. "One-frame shooting" When you press the shutter button on the transmitter, only one frame is shot. "1 frame / second continuous shooting" While pressing the shutter button on the transmitter, continuous shooting is continued every second.... Read More
Modulation method (Digital) FSK Frequency (GHz) 2.4 tranmission distance (m) 100+ (depends on environment) Number of Channels 16 pieces
This is the transmitter side of the "Lumi Control Set ML-3" that can control compatible cameras wirelessly. It is used as a set of receiver and transmitter.
* Batteries are not included.
A remote code that is convenient when using a tripod, which is required for bulb shooting, such as deep shooting and close-up shooting with a deep depth of field, and long exposure during evening and night scene shooting.
Double release for remote terminal. When taking close-up shots using the bellows attachment PB-6, the automatic aperture mechanism of the lens can be used as it is by using the AR-10 together. Can be used with MC-25 for D3, D2 series, D1 series, D300, D200, D100 (with MB-D100), F6, F5, F100, F90X... Read More
Main features of "Remote Control TR-1" You can easily take remote shots without connecting to a smartphone wirelessly. Attached to the selfie stick "RICOH THETA Stick TM-2 / TM-3" with the attached holder. 12mm thick thin size drip-proof structure allows you to shoot outdo... Read More
Operating Temperature Range (℃) 0~40 Rated Voltage (V) 3 Rated Power Consumption (W) 3m Operating humidity (%) 85 (No condensation) Communication distance (m) About 10 Battery CR2032 Suitable Models THETA Z1/V/SC2
Compatible with IEEE 802.11ac (5GHz) standard. High-speed communication with 2x2 MIMO (at the time of IEEE 802.11ac) improves the stability of wireless communication. Although it is a compact and lightweight design, it has a dust-proof and drip-proof structure.
A must-have item when using a tripod. Renewal of electronic remote switch. The exterior is made of impact-resistant polycarbonate, and the surface has a piano black finish. It has basic functions such as a half-press release used for metering and AF, and a release lock for long exposures. Φ2.5mm ... Read More
Dimensions (H x W x D) (mm) About 105×34×23 Cable Length (cm) About 20-50 (spiral type) Mass (g) About 30 Specification With valve block mechanism
A set of wireless remote controller WR-R11b and wireless remote controller WR-T10. You can attach the WR-R11b to the accessory terminal of a compatible camera and use the WR-T10 to wirelessly release or release multiple unmanned cameras at the same time. In addition, interlocking release of multi... Read More
Camera specifications Camera equipped with accessory terminal
A remote grip that can be connected to a Z-series camera via a wired connection and can be operated remotely. Various functions of the camera can be operated and controlled by attaching it to the pan stick of a tripod or the handle of a shoulder rig. By attaching an adapter to the ARRI standard c... Read More
Mass (g) (main unit only) about 205 Operating Temperature Range (℃) -10~40 Operating Humidity (%) 85% or less *No condensation USB type Type-C terminal Compatible camera Z 9/Z 7II/Z 6II *As of November 2, 2022