Rice / Rice Cakes
Other Related Pages
- IRIS OHYAMA Rice wrapping of low-temperature process rice Individual packagingIt is a luxurious mochi made from high-quality domestically produced glutinous rice. It is chewy and fluffy. We value the deliciousness of each piece. As it is individually wrapped, it is delicious and convenient to store.Type MochiDiscontinued
- IRIS OHYAMA Low-temperature manufacturing rice Miyagi prefecture HitomeboreThe "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Lami bag specifications and deoxidizing material are included, so it keeps fresh until it is ope... Read MoreType Rice Material Miyagi Prefecture HitomeboreDiscontinued
- IRIS OHYAMA Fresh rice Koshihikari from NiigataWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreMaterial Koshihikari from NiigataDiscontinued
- IRIS OHYAMA Gift box 3 go x 4 kinds eat comparison set 4 bagsWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreType RiceDiscontinued
- IRIS OHYAMA Pack rice variety set 3P x 5 bag setIt is a variety pack that compares eating delicious rice 3P type 5 brands of low-temperature manufacturing rice.Type RiceDiscontinued
- IRIS OHYAMA Brown rice from HokkaidoThe "low temperature manufacturing method" that consistently manages storage and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Lami bag specifications and deoxidizing material are included, so it keeps fresh until it is opened at home.Material Hokkaido dream dreamDiscontinued
- IRIS OHYAMA Fresh rice Non-washed rice from Miyagi prefecture HitomeboreIt is a convenient wash-free rice that can be cooked without sharpening as it is delicious. We use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less prote... Read MoreType Rice Material Miyagi Prefecture HitomeboreDiscontinued
- IRIS OHYAMA Delicious rice made with low-temperature process rice Hitoshibore from Miyagi Prefecture 180g x 3PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Miyagi Prefecture HitomeboreDiscontinued
- IRIS OHYAMA Delicious rice with low-temperature process rice Koshihikari from Niigata 180g x 3PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Koshihikari from NiigataDiscontinued
- IRIS OHYAMA Rice flour cut rice cake rose squareA rice cake made from Thai rice flour. It is plump and chewy. Each piece is carefully packed with the deliciousness of the chewy texture.Type MochiDiscontinued
- IRIS OHYAMA Brown rice Hokkaido sevenThe "low temperature manufacturing method" that consistently manages storage and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Lami bag specifications and deoxidizing material are included, so it keeps fresh until it is opened at home.Material Nanatsuboshi from HokkaidoDiscontinued
- IRIS OHYAMA Small-sized rosesIt is a luxurious rice cake made from high-quality domestically produced glutinous rice. It is chewy and fluffy. We value the deliciousness of each piece. It is a small and easy-to-eat size.Type MochiDiscontinued
- IRIS OHYAMA Brown rice from Yamagata PrefectureThe "low temperature manufacturing method" that consistently manages storage and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Lami bag specifications and deoxidizing material are included, so it keeps fresh until it is opened at home.Material Tsuyahime from YamagataDiscontinued
- IRIS OHYAMA Delicious rice made with low-temperature process rice Natsushibo from Hokkaido 180g × 3PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Nanatsuboshi from HokkaidoDiscontinued
- IRIS OHYAMA Lifestyle of low temperature process rice Individual packagingIt is a luxurious rice cake made from high-quality domestically produced glutinous rice. It is chewy and fluffy. We value the deliciousness of each piece. As it is individually wrapped, it is delicious and convenient to store.Discontinued
- IRIS OHYAMA Fresh rice Hokkaido Yume PurikaWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreMaterial Hokkaido dream dreamDiscontinued
- IRIS OHYAMA Rice flour cut rice cake single pack square typeA rice cake made from Thai rice flour. It is plump and chewy. Each piece is carefully packed with the deliciousness of the chewy texture. As it is individually wrapped, it is delicious and convenient to store.Type MochiDiscontinued
- IRIS OHYAMA Fresh rice Koshihikari from Uonuma, NiigataWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreDiscontinued
- IRIS OHYAMA Delicious rice made with low-temperature process rice, Miyagi Hitomebore 180g × 5PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Miyagi Prefecture HitomeboreDiscontinued
- IRIS OHYAMA Delicious rice made with low-temperature process rice Yamagata Prefecture Tsuyahime 180g × 5PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Tsuyahime from YamagataDiscontinued
- IRIS OHYAMA Lifestyle of low temperature process rice Individual packagingIt is a luxurious rice cake made from high-quality domestically produced glutinous rice. It is chewy and fluffy. We value the deliciousness of each piece. As it is individually wrapped, it is delicious and convenient to store.Type MochiDiscontinued
- IRIS OHYAMA Mirror rice cake100% domestic paddy rice glutinous rice is used to prepare for the New Year. We welcome you to our home with delicious kagami mochi. Domestic paddy rice glutinous rice is stored and polished by the low temperature manufacturing method that is particular to iris. The grains are steamed in a steame... Read MoreCountry of Origin Japan Type Mochi Material Paddy rice sticky rice (domestic)Discontinued
- IRIS OHYAMA Delicious rice with low-temperature process rice Hokkaido Yume Purika 180g × 3PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreMaterial Hokkaido dream dream Type RiceDiscontinued
- IRIS OHYAMA 6 kinds of fresh rice set for comparison 2 go × 6 bagsWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 2 go (about 300g) in a fr... Read MoreType RiceDiscontinued
- IRIS OHYAMA Brown rice Koshihikari from NiigataThe "low temperature manufacturing method" that consistently manages storage and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Lami bag specifications and deoxidizing material are included, so it keeps fresh until it is opened at home.Material Koshihikari from NiigataDiscontinued
- IRIS OHYAMA Fresh rice eating comparison 1.8 3 bags setWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreDiscontinued
- IRIS OHYAMA Fresh rice Unwashed rice Koshihikari from NiigataIt is a convenient wash-free rice that can be cooked without sharpening as it is delicious. We use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less prote... Read MoreMaterial Koshihikari from NiigataDiscontinued
- IRIS OHYAMA Gift box 3 go x 6 kinds eating comparison set 6 bagsWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreType RiceDiscontinued
- IRIS OHYAMA Fresh rice 3 go × 5 species comparisonWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreDiscontinued
- IRIS OHYAMA Small-sized roses with low-temperature production riceIt is a luxurious mochi made from high-quality domestically produced glutinous rice. It is chewy and fluffy. We value the deliciousness of each piece. It is a small and easy-to-eat size.Type MochiDiscontinued
- IRIS OHYAMA Delicious rice made from low-temperature process rice Koshihikari from Niigata 180g x 5PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreMaterial Koshihikari from Niigata Type RiceDiscontinued
- IRIS OHYAMA Fresh rice Unwashed rice Miyagi SasanishikiIt is a convenient wash-free rice that can be cooked without sharpening as it is delicious. We use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less prote... Read MoreMaterial Sasanishiki from Miyagi Type RiceDiscontinued
- IRIS OHYAMA Lifestyle of low temperature process rice Individual packagingIt is a luxurious rice cake made from high-quality domestically produced glutinous rice. It is chewy and fluffy. We value the deliciousness of each piece. As it is individually wrapped, it is delicious and convenient to store.Type MochiDiscontinued
- IRIS OHYAMA Fresh Rice Hokkaido NatsunaboshiWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreMaterial Nanatsuboshi from HokkaidoDiscontinued
- IRIS OHYAMA Delicious rice with low-temperature process rice Yamagata Tsuyahime 180g × 3PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Tsuyahime from YamagataDiscontinued
- IRIS OHYAMA Fresh rice from Yamagata PrefectureWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Rice was divided into 3 go (about 450g) in a fr... Read MoreMaterial Tsuyahime from YamagataDiscontinued
- IRIS OHYAMA Delicious rice made with low-temperature process rice, Miyagi hitomebore 180g × 10PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Miyagi Prefecture HitomeboreDiscontinued
- IRIS OHYAMA Low-temperature-processed rice Non-washed rice Miyagi TsuyahimeThe "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Lami bag specifications and deoxidizing material are included, so it keeps fresh until it is ope... Read MoreMaterial Princess Miyatsuya from MiyagiDiscontinued
- IRIS OHYAMA Mirror rice cake mini with orange100% domestic paddy rice glutinous rice is used to prepare for the New Year. We welcome you to our home with delicious kagami mochi. Domestic paddy rice glutinous rice is stored and polished by the low temperature manufacturing method that is particular to iris. The grains are steamed in a steame... Read MoreDimensions, Width W x Depth D x Height H (cm) (Decoration size) 10.7 × 10.7 × 9.5 Country of Origin Japan Size Mini Included Accessories Mizuhiki Type Mochi Material Paddy rice sticky rice (domestic)Discontinued
- IRIS OHYAMA Delicious rice of low-temperature production rice Hokkaido Yume Purika 180g x 5PWe use only carefully selected first-class rice. The "low temperature manufacturing method" that consistently manages storage, rice polishing, and packaging in the factory at 15 ° C or less protects the freshness and deliciousness of rice. Easy cooking with chin in the microwave. You ca... Read MoreType Rice Material Hokkaido dream dreamDiscontinued