The blue light of the LED back monitor can cut the light with the main wavelength of 450 nm by about 26%. It concentrates the blue light that is not easily absorbed by the crystalline lens of the eye and may damage the retina. Recommended for eye strain measures. It has a structure that is easy o... Read More
Transmittance (%) 78.3 Reflectance (%) 1.69 Suitable Model Fujitsu ARROWS Tab Q509 (10.1 type wide) UV Shading Rate (%) 99.9 Mass (g) 14 Surface Hardness 2~3H Dimensions, Width W x Depth D x Height H (mm) 248.7×0.2×164.9
Antibacterial / antiviral peeping prevention filter Clean, safe and easy to put on and take off again. Lumiart antibacterial / antiviral film and peep prevention filter are attached. It has both security and security for terminals that are directly operated by hand or finger, such as touch panels... Read More
Easy fit antibacterial film. Just stick the four corners with the original triangle tape. It can be easily attached and detached without worrying about air bubbles. Smooth finger slip with reduced reflection and fingerprint prevention. Hard coat and resistant to scratches. A lineup that can be us... Read More
Easy fit antibacterial film. Just stick the four corners with the original triangle tape. It can be easily attached and detached without worrying about air bubbles. Smooth finger slip with reduced reflection and fingerprint prevention. Hard coat and resistant to scratches. A lineup that can be us... Read More
Approximately 26% cut at the blue light main wavelength 450 nm of the LED back monitor. Concentrated cut of blue light that is difficult to be absorbed by the crystalline lens of the eye and may damage the retina. Recommended for eye strain measures. It reduces blue light and absorbs it inside an... Read More
Thickness (mm) 0.2 External light reflectance (%) 1.69 Suitable Size 10.1 inches wide Dimensions, Width W x Depth D x Height H (mm) 252.4×0.2×158.7 Blue Light Blocking Rate 26% Surface Hardness 2~3H Visible Light Transmittance (%) 78.3 UV Protection 99.9% Touch panel method Correspondence Suitable Models Fujitsu ARROWS Tab Q5010
Approximately 26% cut at the blue light main wavelength 450 nm of the LED back monitor. Concentrated cut of blue light that is difficult to be absorbed by the crystalline lens of the eye and may damage the retina. Recommended for eye strain measures. It reduces blue light and absorbs it inside an... Read More
Reflectance (%) 0.0169 Thickness (mm) 0.2 UV Protection 0.999 Size 13.3 inches wide Surface Hardness 2~3H Transmittance (%) 78.3 Dimensions, Width W x Depth D x Height H (mm) Film: 309 x 0.2 x 194.8 Suitable Models Fujitsu ARROWS Tab Q7310
For physical security measures. 2way (left and right) peep prevention film. Measures for telework security guidelines (Ministry of Internal Affairs and Communications).
Suitable Models For FJ Q5010 / Q5011 only Feature Peep prevention
For physical security measures. 2way (left and right) peep prevention film. Measures for telework security guidelines (Ministry of Internal Affairs and Communications).
Suitable Models For FJ Q7310 / Q7311 only Feature Peep prevention
For physical security measures. 4way (up / down / left / right) Peep prevention film. Measures for telework security guidelines (Ministry of Internal Affairs and Communications).
Suitable Models For FJ Q7310 / Q7311 only Feature Peep prevention
For physical security measures. 4way (up / down / left / right) Peep prevention film. Measures for telework security guidelines (Ministry of Internal Affairs and Communications).
Suitable Models For FJ Q5010 / Q5011 only Feature Peep prevention
The world's only highly transparent film that has acquired the SIAA mark for antivirals. Antiviral function: High effect of reducing 99.99% of viruses that do not have cell membranes that alcohol preparations do not work. Antibacterial function: Suppresses the growth rate of bacteria on produ... Read More
The world's only highly transparent film that has acquired the SIAA mark for antivirals. Antiviral function: High effect of reducing 99.99% of viruses that do not have cell membranes that alcohol preparations do not work. Antibacterial function: Suppresses the growth rate of bacteria on produ... Read More
Antibacterial / antiviral peeping prevention filter Clean, safe and easy to put on and take off again. Lumiart antibacterial / antiviral film and peep prevention filter are attached. It has both security and security for terminals that are directly operated by hand or finger, such as touch panels... Read More
Airless processing that allows air bubbles to escape cleanly. Anti-fingerprint, high-gloss type LCD protective film for arrows Tab F-02K that protects the LCD screen from scratches and dirt.
Special processing prevents flicker peculiar to anti-reflection and reproduces images clearly. Airless processing that allows air bubbles to escape cleanly. Anti-fingerprint / anti-reflective type LCD protective film for arrows Tab F-02K that protects the LCD screen from scratches and dirt.
The blue light main wavelength (450nm) light generated from the LED back monitor can be cut by about 26%. It concentrates the blue light that is not easily absorbed by the crystalline lens of the eye and may damage the retina. Recommended for eye strain measures. It has a structure that is easy o... Read More
UV Protection 0.999 Surface Hardness 2~3H Dimensions, Width W x Depth D x Height H (mm) 309.3×0.2×195.3 Reflectance (%) 4.7 Transmittance (%) 80.1 Suitable Models Fujitsu ARROWS Tab Q738
The blue light main wavelength (450nm) light generated from the LED back monitor can be cut by about 26%. It concentrates the blue light that is not easily absorbed by the crystalline lens of the eye and may damage the retina. Recommended for eye strain measures. It has a structure that is easy o... Read More
UV Protection 0.999 Mass (g) 14 Dimensions, Width W x Depth D x Height H (mm) 248.1×0.2×164.4 Surface Hardness 2~3H Reflectance (%) 4.7 Transmittance (%) 80.1
Since the adhesive surface uses a silicon material, it sticks perfectly to the entire table including the LCD screen. (Excluding the camera part) * There is no hole in the sensor part, but there is no problem in use. No need for double-sided tape. As it is a dedicated type, it can be used as it i... Read More
Since the adhesive surface uses a silicon material, it sticks perfectly to the entire table including the LCD screen. (Excluding the camera part) * There is no hole in the sensor part, but there is no problem in use. No need for double-sided tape. As it is a dedicated type, it can be used as it i... Read More
Anti-reflection film for ARROWS Tab Q5010 / CE, ARROWS Tab Q5010 / CB, ARROWS Tab Q5010 / DEG, which is a shock absorbing, blue light cut type that the multi-pet layer absorbs shock.
Blue Light Blocking Rate About 45% Material Bonding surface: Silicone, outside: PET