It is a film that has the same high surface hardness (9H) as glass and is extremely resistant to scratches. Although it has high hardness, it is thin and flexible and does not scatter like glass. With a high transmittance of 91%, it is a clear screen that projects light beautifully. Also supports... Read More
Included Accessories Cleaning cloth x1, Spatula x1 Feature High hardness 9H Suitable Model Kobo Libra H2O / Rakuten Type of Terminal Fitting Silicon adsorption
It cuts about 32% or more of blue light, which is considered to be harmful to the eyes. Anti-reflection (non-glare, anti-glare) processing reduces the reflection of light from fluorescent lamps and makes the screen easier to see. Anti-fingerprint processing makes it difficult for fingerprints to ... Read More
Feature Blue light cut / anti-reflection Included Accessories Cleaning cloth x1, Spatula x1 Suitable Model Kobo Libra H2O / Rakuten Type of Terminal Fitting Silicon adsorption
It cuts about 32% or more of blue light, which is considered to be harmful to the eyes. Anti-reflection (non-glare, anti-glare) processing reduces the reflection of light from fluorescent lamps and makes the screen easier to see. Anti-fingerprint processing makes it difficult for fingerprints to ... Read More
Feature Blue light cut / anti-reflection Included Accessories Cleaning cloth x1, Spatula x1 Suitable Model Kobo Clara HD Type of Terminal Fitting Silicon adsorption
With a surface hardness (8-9H) equivalent to that of glass, it is not easily scratched and keeps the screen beautiful. It cuts about 30% of blue light, which is harmful to the eyes. With a high transmittance of about 90%, the screen is very clear and the characters are clearly visible.
* The size... Read More
Included Accessories Cleaning cloth x1, Spatula x1 Suitable Model Kobo Libra H2O / Rakuten Type of Terminal Fitting Silicon adsorption
Since the adhesive surface uses a silicon material, it sticks perfectly to the entire table including the LCD screen. (Excluding the home button, etc.) Double-sided tape is not required. As it is a dedicated type, it can be used as it is without cutting. * Slightly smaller than each part size to ... Read More
Thickness (mm) 0.2 Quantity 1 sheet Suitable Model Rakuten kobo mini
Since the adhesive surface uses a silicon material, it sticks perfectly to the entire table including the LCD screen. (Excluding camera and home button) Double-sided tape is not required. As it is a dedicated type, it can be used as it is without cutting. * The size is slightly smaller than the s... Read More
Since the adhesive surface uses a silicon material, it sticks perfectly to the entire table including the LCD screen. (Excluding the home button, etc.) Double-sided tape is not required. As it is a dedicated type, it can be used as it is without cutting. * Slightly smaller than each part size to ... Read More
Quantity 1 sheet Dimensions, Width W x Depth D x Height H (mm) 90×0.2×121.5 Suitable Model Rakuten ebook reader kobo glo