Business Software
Other Related Pages
- TB Print slip 12Reduced tax rate compatible version! Voucher issuance is decided by this! 10% consumption tax & 8% reduced tax rate has been set! Easier than anywhere else! Supports reduced tax rates! Classified invoices-qualified invoices can be created Hisago's reduced tax rate correspondence form is i... Read MoreApplicable Media CD-ROM Capacity HD free space: 250MB or more Type Supported images: JPG / BMP / GIFfrom S$249.90Min. 2 days
- NJK Easy character input to PDF PRO v.9.0 UPG 1 licenseSoftware that allows you to enter and print characters on a computer for business forms such as various PDF applications, slips, and reports issued by government offices and companies. 1) Supports PDF file import. Scan the paper format with a scanner and capture it. 2) Touch panel compatible. Sup... Read MoreSuitable Models IBM PC / AT compatible machine
- rolan QR code creation software Sakura Ver. 5.0It is software that can create QR code on Windows OS. You can easily create a QR code from Excel, Word, or Access. You can also use a DLL to incorporate the QR code creation function into development tools such as VB and VC. The label creation software "QR Labeler" with QR code and the ... Read MoreSuitable Models IBM PC / AT compatible machinefrom S$589.90Min. 2 days
- TB Designated slip 12 PC softwareinstalled drive CD-ROM drive Image compression method jpeg/bitmap/gif Other Pointing device such as mousefrom S$299.90Min. 2 days
- Social Survey Research Information Excel statistics Normal version 1 year 1 unitExcel Statistics is a statistical analysis software that adds statistical analysis methods to Excel menus. The data on Excel can be statistically analyzed as it is, and it can be used intuitively. No script or code input required. Even those who perform statistical analysis for the first time can... Read MoreSupported OS Windows10/8.1/8/7 Suitable Models IBM PC / AT compatible machinefrom S$339.90Min. 2 days
- DE-NET Construction digital camera photo management 2This software allows you to easily capture construction photos taken with a digital camera or tablet and manage them on your computer. In this version, the program has been significantly improved and renewed to be easier to use and rich in functions. You can easily import photos from a digital ca... Read MoreSuitable Models IBM PC / AT compatible machine Memory 2GB or morefrom S$76.99Min. 2 days
- NJK Easy text input to PDF PRO v.9.0 1 licenseSoftware that allows you to enter and print characters on a computer for business forms such as various PDF applications, slips, and reports issued by government offices and companies. 1) Supports PDF file import. Scan the paper format with a scanner and capture it. 2) Touch panel compatible. Sup... Read MoreDisc 110MB or more Suitable Models IBM PC / AT compatible machinefrom S$189.90Min. 2 days
- ESUMI Mac Multivariate Analysis Ver.3.0It is software that can easily perform advanced multivariate analysis with Excel on Mac. It is a data mining software with excellent operability that allows you to use the data on the Excel data file as it is. You can use it as if a statistical analysis command was added to Excel that you always ... Read MoreMemory 1GB or more Disc 50MB or more Supported OS Mac OS X 10.5.8 or later Suitable Models Intel-equipped Mac Suitable CPU intel CPUfrom S$559.90Min. 18 days
- ESUMI EXCEL multivariate analysis + Ver.8.0Multivariate analysis software that runs on Excel. It is software that can easily perform advanced multivariate analysis with Excel. It is a data mining software with excellent operability that allows you to use the data on the Excel data file as it is. You can use it as if a statistical analysis... Read Morefrom S$489.90Min. 2 days
- Antenna House Shunkan + PDF + Edit + 9Software that allows you to freely edit PDF with simple operations. It is software that allows you to freely edit PDF with simple operations. Advanced editing such as direct editing of the text, batch editing of multiple PDFs, combining PDFs and rearranging pages is possible with simple operations.from S$119.90Min. 12 days
- rolan SakuraBar PLUS for WindowsA plug-in that adds barcode creation capabilities to FileMaker Pro. Barcodes can be displayed and printed in fonts, and barcodes can be created by adding calculated fields to existing files. Compatible with JAN / EAN (standard), JAN / EAN (shortened), UPC-A, UPC-E, NW7 (CODABAR), CODE39, CODE128,... Read MoreSuitable Models IBM PC / AT compatible machine Supported OS Windows 7 compatible Operating Environment Windows OS with FileMaker Pro7 or laterfrom S$299.90Min. 12 days
- Nihon Poladigital DeltaGraph7J WinGraph creation software that has an interface that is familiar to beginners and has "more than 80 types of abundant graph types" and "abundant graph editing functions". It also supports professional needs such as equipment of data analysis functions used in various research fi... Read MoreDisc 200MB or more Memory 1GB or more Supported OS Windows XP (SP3 or later) Vista / 7/8 Suitable Models IBM PC / AT compatible machine Suitable CPU Pentium 1.5GHz or higherfrom S$599.90Min. 12 days
- Kodensha ChineseWriter11 StandardChinese input + font + dictionary tool software that is convenient for Chinese documents, email composition, chat, etc. It is equipped with a wealth of support tools for Japanese people, such as handwriting, pinyin with tone, and Japanese-Chinese translation input, as well as input of simplified ... Read MoreSupported OS Windows 10/8.1/8/7(32bit・64bit) Disc 2.4GB or more Suitable Models IBM PC / AT compatible machinefrom S$399.90Min. 6 days
- Cross Language PC-Transer Translation Studio V26 for WindowsTranslation software designed for use in business translation. The total number of recorded dictionaries is 8.387 million words (basic word dictionary 3.7 million words: English-Japanese 1.31 million words / Japanese-English 2.39 million words, specialized word dictionary 4.683 million words: Eng... Read Morefrom S$1,899.00Min. 6 days
- Cross Language PC-Transer Translation Studio V26 Academic Edition for WindowsTranslation software designed for use in business translation. The total number of recorded dictionaries is 8.387 million words (basic word dictionary 3.7 million words: English-Japanese 1.31 million words / Japanese-English 2.39 million words, specialized word dictionary 4.683 million words: Eng... Read Morefrom S$999.00Min. 13 days
- Antenna House Shunkan + PDF + Create + 9PDF conversion driver and software that can convert documents such as Office to PDF at once, combine / split created PDF files, set document information, set / cancel security, etc. PDF conversion driver and software that can convert documents such as Office to PDF at once, combine / split create... Read Morefrom S$49.99Min. 12 days
- JUNGLE Polaris OfficeDocument creation, spreadsheet, presentation, PDF editing, software that combines four software into one. Document creation "WORD" that can manage the change history. Spreadsheet "SHEET" that supports pivot tables and 330 functions. Presentation software "SLIDE" that... Read MoreSuitable Models IBM PC / AT compatible machine Memory 2GB or more Disc 1GB or morefrom S$55.99Min. 6 days
- rolan M.B.D V2.2(MAGAZINE BAR DESIGN)Adobe Illustrator plug-in software for Mac that can create JAN / add-on code for periodical code (magazine). Create a standard-compliant periodical code (magazine) with a simple operation. OCR characters are also created in outline, so there is no need to purchase OCR-B fonts separately. If you c... Read MoreSuitable Models Intel-equipped Mac Supported OS Macfrom S$1,099.00Min. 12 days
- ESUMI EXCEL Conjoint Analysis / AHP Ver.2.0 1 license packageIt is software that can analyze conjoint analysis and AHP (analytic hierarchy process) used in marketing and decision making with Excel. Conjoint cards and hierarchical diagrams can be easily created with an easy-to-understand menu structure that matches the order of thoughts of the analyst. Stat... Read MoreSupported OS Windows XP/Vista/7/8 Memory 128M or more Disc 50MB or more Suitable Models IBM PC / AT compatible machinefrom S$559.90Min. 13 days
- Social Survey Research Information Trend Search 2015 Academic EditionSoftware that allows you to easily text-mine Japanese text on an Excel sheet. No statistical knowledge is required for analysis. If you paste data into Excel, such as free answers to questionnaires, writing on SNS, and inquiries from customers, the software will extract important keywords and the... Read MoreSuitable Models IBM PC / AT compatible machine Supported OS Windows 7/8/8.1/10 (x64/x86)from S$1,399.00Min. 12 days
- Kodensha ChineseWriter11 Learning Premium AcademicChinese input + font + dictionary tool software that is convenient for Chinese documents, email composition, chat, etc. It is equipped with a wealth of support tools for Japanese people, such as handwriting, pinyin with tone, and Japanese-Chinese translation input, as well as input of simplified ... Read MoreDisc 2.8GB or more Supported OS Windows 10/8.1/8/7(32bit・64bit) Suitable Models IBM PC / AT compatible machinefrom S$389.90Min. 6 days
- ESUMI EXCEL Questionnaire Dazai Ver.5.5 [Total]This is software dedicated to questionnaire aggregation analysis that runs on the Windows version of Excel. Advanced aggregation analysis is possible with simple operations for inputting / aggregation / analysis of questionnaire data. Since the tabulation / graph / analysis results can be output ... Read MoreDisc 120MB or more Memory 1GB or more Supported OS Windows 7/8/10 Suitable CPU intel CPU Suitable Models IBM PC / AT compatible machinefrom S$769.90Min. 13 days
- ESUMI EXCEL prediction Ver.3.0 1 license packageMicrosoft Excel add-in software equipped with prediction methods such as EPA method, trend analysis, and factor analysis. You can make full-scale predictions while maintaining the operability of Microsoft Excel. For demand forecasts and sales forecasts, it is possible not only to make forecasts b... Read MoreSupported OS Windows XP/Vista/7/8 Memory 128MB or more Suitable Models IBM PC / AT compatible machine Disc 10MB or morefrom S$569.90Min. 13 days
- ESUMI EXCEL quantification theory Ver.4.0Statistical analysis software that runs on Excel. A statistical analysis menu is temporarily added only when using the software, and it can be used as if a statistical analysis command was added to Excel. In this version, data editing for data editing has become more convenient by adding a data p... Read MoreSuitable Models IBM PC / AT compatible machine Supported OS Windows XP/Vista/7/8 Memory 128MB or more Disc 20MB or morefrom S$479.90Min. 13 days
- ESUMI EXCEL Questionnaire Dazai Ver.5.5 [Total + Graph version]This is software dedicated to questionnaire aggregation analysis that runs on the Windows version of Excel. Advanced aggregation analysis is possible with simple operations for inputting / aggregation / analysis of questionnaire data. Since the tabulation / graph / analysis results can be output ... Read MoreSuitable Models IBM PC / AT compatible machine Memory 1GB or more Supported OS Windows 7/8/10 Suitable CPU intel CPU Disc 120MB or morefrom S$999.00Min. 13 days
- TB Payroll printing 11 PC softwareThis software allows you to quickly, easily, and safely create annual-related forms such as pay slips and withholding slips. Data can be created by (1) directly inputting to the form (2) reading external data (3) using the attached Excel workbook, and printing my number is also possible (with man... Read MoreType Supported images: JPG / BMP / GIF Capacity HD free space: 250MB or more Applicable Media CD-ROMfrom S$249.90Min. 5 days
- rolan Postal bar code creation software YuBar Ver4.0Software for easily creating postal customer barcodes for postage reduction. It can be used standalone or for development. A mailing label printing application that is convenient when sending DM is included as standard. You can easily create barcodes on Excel or Access. It comes with a developmen... Read MoreSuitable Models IBM PC / AT compatible machinefrom S$769.90Min. 12 days
- Cross Language Translation Pikaichi European V6 + OCRTranslation software for Japanese and English / French / German / Spanish / Italian / Portuguese. Includes a basic word dictionary (Japanese → English and European 2.418 million words, English and European → Japanese 1.639,000 words). The add-in translation function preserves and translates the o... Read MoreSupported OS Windows 10/8.1/8/7 SP1(32bit/64bit) Suitable Models IBM PC / AT compatible machine Disc 1.5GB or morefrom S$299.90Min. 13 days
- Cross Language Translation Pikaichi Medical V15 for WindowsTranslation software specializing in medical translation (English <=> Japanese) that provides a higher quality translation with a dictionary of "5.093 million words". The high-precision translation engine, basic word dictionary, specialized word dictionary, and "Nanzando Medi... Read MoreSupported OS Windows 7 SP1/8/8.1/10 (32bit/64bit) Suitable Models IBM PC / AT compatible machine Disc 1.2GB or morefrom S$569.90Min. 6 days
- Cross Language Translation Pikaichi V15 for WindowsTranslation software that provides higher quality translation (English <=> Japanese) with a high-speed translation engine and a dictionary of "7.51 million words". The high-precision translation engine of the high-end product "Transer Series", full-featured specialized w... Read MoreDisc 1.6GB or more Supported OS Windows 10/8.1/8/7 SP1 (32bit/64bit) Suitable Models IBM PC / AT compatible machinefrom S$389.90Min. 6 days
- ESUMI Mac statistical analysis Ver.3.0It is software that can easily perform advanced statistical analysis with Excel on Mac. It is a data mining software with excellent operability that allows you to use the data on the Excel data file as it is. You can use it as if a statistical analysis command was added to Excel that you always u... Read MoreSupported OS Mac OS X 10.5.8 or later Suitable Models Intel-equipped Mac Disc 50MB or more Suitable CPU intel CPU Memory 1GB or morefrom S$559.90Min. 13 days
- OMRON SOFTWARE Wnn8 for Linux/BSDJapanese input system compatible with Linux and FreeBSD. The "input prediction function", which was first installed in the previous version "Wnn7" and has improved input efficiency, has evolved further. It not only predicts input candidates based on the "standard predicti... Read MoreMemory 64MB or more Supported OS Linux Disc 65MB free space Suitable Models IBM PC/ATCompatifrom S$139.90Min. 12 days
- ESUMI Mac statistical analysis Ver.3.0 + Mac multivariate analysis Ver.3.0It is software that can easily perform advanced statistical analysis with Excel on Mac. It is a data mining software with excellent operability that allows you to use the data on the Excel data file as it is. You can use it as if a statistical analysis command was added to Excel that you always u... Read MoreSuitable CPU intel CPU Supported OS Mac OS X 10.5.8 or later Disc 50MB or more Suitable Models Intel-equipped Mac Memory 1GB or morefrom S$1,199.00Min. 12 days
- SilverStarJapan Anything PDF8You can convert Excel, Word, or any other file to PDF. The secret is that "Anything PDF" can be set as a printer. In other words, any software that can print can be converted to PDF. Simply select "Anything PDF8" in the printer selection field and print. You can easily create ... Read MoreSuitable Models IBM PC / AT compatible machine Supported OS Windows Vista/7/8/8.1 Disc 10MB or morefrom S$21.99Min. 12 days
- rolan Barcode Plot WJAN (standard), JAN (shortened), UPC-A, UPC-E, logistics product code standard version (ITF 14 digits), logistics product code extended version (ITF 16 digits), ITF (variable length), for charge proxy storage Adobe Illustrator (Windows version) plug-in software that can create (UCC / EAN128). Cre... Read MoreSuitable Models IBM PC / AT compatible machine Supported OS Windowsfrom S$389.90Min. 12 days
- NJK Easy text input to PDF PRO v.9.0 5 licenseSoftware that allows you to enter and print characters on a computer for business forms such as various PDF applications, slips, and reports issued by government offices and companies. 1) Supports PDF file import. Scan the paper format with a scanner and capture it. 2) Touch panel compatible. Sup... Read MoreSuitable Models IBM PC / AT compatible machinefrom S$589.90Min. 11 days
- PCA PCA legal statement DX+with+SQL+20CALPayment record / legal record creation system. Easy-to-understand input screens and abundant output forms make legal record-related work more efficient. Consistently create from each payment record to the total table. Data is smoothly linked with "PCA Salary DX" and "PCA Accounting... Read Morefrom S$18,990.00Min. 12 days
- rolan Postal customer barcode creation software YuBar Ver4.0 Site licenseSoftware for easily creating postal customer barcodes for postage reduction. It can be used standalone or for development. A mailing label printing application that is convenient when sending DM is included as standard. You can easily create barcodes on Excel or Access. It comes with a developmen... Read MoreSuitable Models IBM PC / AT compatible machinefrom S$5,599.00Min. 12 days
- PCA PCA legal record DXPayment record / legal record creation system. Easy-to-understand input screens and abundant output forms make legal record-related work more efficient. Consistently create from each payment record to the total table. Data is smoothly linked with "PCA Salary DX" and "PCA Accounting... Read Morefrom S$1,399.00Min. 12 days
- rolan Barcode / QR image batch output software Barcode Dotto imageIt is software that outputs a large amount of QR code, GS1 DataBar, and JAN code of thousands or tens of thousands to an image file at once. Converts a line of data into a single image file. The output file format can be selected from BMP, JPEG, PNG, TIFF, GIF, and EPS. * DVD-ROM drive requiredSuitable Models IBM PC / AT compatible machinefrom S$2,699.00Min. 12 days
Filter by categories