This software allows you to easily capture construction photos taken with a digital camera or tablet and manage them on your computer. In this version, the program has been significantly improved and renewed to be easier to use and rich in functions. You can easily import photos from a digital ca... Read More
Suitable Models IBM PC / AT compatible machine Memory 2GB or more
Construction site photo management software that fully supports XML. The efficiency of construction site photo management work has been dramatically improved, from the construction photo ledger to the creation of data required for electronic delivery, in three steps: [import], [management], and [... Read More
Latest OS Windows 11 compatible (NEW) Easy creation of construction photo ledger from 2 creation modes You can put 3 photos and text information on 1 page. A ledger can be created in conjunction with the attached software "Construction Digital Camera Photo Management 2" Construction Pho... Read More
Applicable Media CD-ROM[1A] Suitable Models WIN[MS26] Supported OS Windows 11 / 10 / 8.1 ( 64・32bit ) Suitable PC Windows PC with manufacturer support
Latest OS Windows 11 compatible (NEW) Easy creation of construction photo ledger from 2 creation modes You can put 3 photos and text information on 1 page. A ledger can be created in conjunction with the attached software "Construction Digital Camera Photo Management 2" Construction Pho... Read More
Applicable Media CD-ROM[1A] Suitable Models WIN[MS26] Supported OS Windows 11 / 10 / 8.1( 64bit・32bit ) Suitable PC Windows PC with manufacturer support
[Smooth cooperation between photo management and electronic delivery] "Kuraemon Purveyor" is a full-scale "construction photo management" software for utilizing construction photos, which has a sales record of 20 years. By simply registering photos and information according to... Read More
Memory 4.0GB or more recommended Printer Color printer recommended Suitable CPU Intel + Core + i3 or higher recommended OS Windows10 / Windows 8.1
"Kuraemon Purveyor 2020 Standard" is construction photo management software for general buildings and small-scale sites. Both digital camera and electronic small blackboards can be managed together in one construction photo ledger. Equipped with a construction work type master as standa... Read More
Supported browsers Internet Explorer 11、Microsoft Edge Memory 4GB or more recommended Suitable CPU Core i3 or higher recommended OS Windows10 / Windows8.1 / Windows7 SP1 Display 1024 x 768 or higher resolution
Software that can create a construction photo ledger of the construction process and progress. Compatible with the new era "Reiwa", even when the construction period spans "Heisei" and "Reiwa". You can create and print a construction photo ledger simply by dragging a... Read More
The time required for construction photo management has been reduced to 1/4 compared to digital cameras.In conventional construction photography, it is difficult to set up a blackboard in rainy weather, strong winds, or in places with narrow scaffolding. I had to get the staff to bring a blackboa... Read More
Included Accessories Shockproof case, shoulder strap Dust / Water Protection IPX5 / IPX8, IP5X storage 32GB Camera specifications 13 million pixels (CALS compatible) Operating Temperature (℃) 5~35 OS 8.1 Resolution 1920×1200 Cable USB TypeC Memory 3G
-Waterproof, dustproof, and shockproof, highly robust model "Kuraemon Pad Tough". -The time required for construction photo management has been reduced to 1/4 compared to digital cameras.・ In the past, it was difficult to set up a blackboard in rainy weather, strong winds, or in a plac... Read More
Memory Capacity 3GB Cable USB TypeC Mass (g) 520 Display 8 (inch) (gorilla glass 3) Conform to microSDHC 32GB recommended OS Android8.1 Dust / Water Protection IP67 Warranty Period One and a half years Camera specifications 16 million pixels (CALS compatible) Resolution 1280×800 processor (GHz) 8 core 2.0GHz Temperature Range (℃) -20~60 storage 32GB Dimensions, Width W x Height H x Depth D (mm) Approx. 235 x 146 x 13
-The "Kuraemon Pad mini" is 8 inches and easy to carry even in narrow sites. -The time required for construction photo management has been reduced to 1/4 compared to digital cameras.・ In the past, it was difficult to set up a blackboard in rainy weather, strong winds, or in a place wit... Read More
Display 8 (inch) Cable USB TypeC Mass (g) 325 Memory Capacity 3GB OS Android8.1 Dust / Water Protection IPX5/IPX8、IP5X Temperature Range (℃) 5~35 Resolution 1920×1200 storage 32GB Warranty Period 1 year Camera specifications 13 million pixels (CALS compatible) Dimensions, Width W x Height H x Depth D (mm) About 214 × 126 × 8.3 processor (GHz) 4-core 1.4GHz
・ Kuraemon Pad main unit and stand for exclusive use of “Kuraemon Pad” ・ Touch pen ・ LCD protective film (2 sheets) ・ microSD card 32GB ・ AC adapter ・ USB-Type C cable set. -"Kuraemon Pad" with a large 10-inch screen for easy character input. -The time required for construction ph... Read More
processor (GHz) 8 core 2.0GHz Resolution 1920×1200 Cable USB TypeC Warranty Period 1 year Dimensions, Width W x Height H x Depth D (mm) About 259 × 168 × 8.6 Temperature Range (℃) 5~35 Mass (g) 503 Display 10.1 (inch) Memory Capacity 3GB OS Android8.1 Camera specifications 13 million pixels (CALS compatible) Dust / Water Protection IPX5/IPX8、IP5X Included Accessories Shockproof case, shoulder strap storage 32GB
-"Kuraemon Pad" with a large 10-inch screen for easy character input. -The time required for construction photo management has been reduced to 1/4 compared to digital cameras.・ In the past, it was difficult to set up a blackboard in rainy weather, strong winds, or in a place with a nar... Read More
Cable USB TypeC Warranty Period 1 year Resolution 1920×1200 Memory Capacity 3GB OS Android8.1 Temperature Range (℃) 5~35 Mass (g) 503 Display 10.1 (inch) processor (GHz) 8 core 2.0GHz Dimensions, Width W x Height H x Depth D (mm) About 259 × 168 × 8.6 storage 32GB Camera specifications 13 million pixels (CALS compatible) Dust / Water Protection IPX5/IPX8、IP5X
"Kuraemon Pad" is a tablet terminal equipped with a large 10.1-inch LCD and an 8.1 megapixel camera. On the large screen, you can enter construction information by hand, just like a conventional blackboard. At the scene, a blackboard is displayed on the shooting preview screen of "... Read More
Memory Storage (GB) (Memory) 2, (Storage) 16 Main Unit Dimensions, Height H x Width W x Thickness (mm) 193×289×23 Operating Temperature / Humidity Range 5~35℃/20~80%RH Mass of Main Unit (g) 875 Battery operating time About 14.0 hours Suitable Models Android 4.4 Dust / Water Protection IPX5 / IPX8, IP5X
Kuraemon Purveyor 18 is a construction photo management software that complies with the guidelines / standards of the Ministry of Land, Infrastructure, Transport and Tourism, the Ministry of Agriculture, Forestry and Fisheries, NEXCO, and the Metropolitan Expressway.
Supported browsers Internet Explorer 11、Microsoft Edge Memory 1.5GB or more recommended Suitable CPU Intel CPU 1GHz or more Supported OS Windows 10、Windows 8.1、Windows 7 Printer Color printer recommended
"Digital construction photo management" software compatible with digital cameras and electronic small blackboards. Construction photo management software for general buildings and small-scale sites. You can manage both digital camera and electronic small blackboard photos in a construct... Read More
Software that can create a construction photo ledger of the construction process and progress. Compatible with the new era "Reiwa", even when the construction period spans "Heisei" and "Reiwa". You can create and print a construction photo ledger simply by dragging a... Read More
A 3-license version of software that allows you to create a construction photo ledger of construction processes and progress. You can create and print a construction photo ledger simply by dragging and dropping the photographed photo and entering a comment. There are two creation modes. In the co... Read More
Memory 2GB or more Suitable Models IBM PC / AT compatible machine
"Digital construction photo management" software (compatible with Windows) compatible with digital cameras and electronic small blackboards. By simply registering photos and information according to the interactive guide, you can create a construction photo ledger that feels like turnin... Read More
"Digital construction photo management" software compatible with digital cameras and electronic small blackboards. Construction photo management software for general buildings and small-scale sites. You can manage both digital camera and electronic small blackboard photos in a construct... Read More
"Digital construction photo management" software compatible with digital cameras and electronic small blackboards. Construction photo management software for general buildings and small-scale sites. You can manage both digital camera and electronic small blackboard photos in a construct... Read More
Software that can create a construction photo ledger of the construction process and progress. You can create and print a construction photo ledger simply by dragging and dropping the photographed photo and entering a comment. There are two creation modes. In the construction photo mode, you can ... Read More
Memory 2GB or more Suitable Models IBM PC / AT compatible machine
Construction photo management software for general buildings and small-scale sites. You can manage both digital camera and electronic small blackboard photos in a construction photo ledger.
"PowerKit" that further improves the operability of "Kuraemon Pad". A foldable tablet stand and LCD protective film, a touch pen that can be operated while wearing work gloves, a microSD card with a capacity of 32GB, an AC adapter that can be charged, and a USB-Type C cable th... Read More
The electronic small blackboard tablet "Kuraemon Pad", which has promoted construction DX, protects construction photo data that proves construction quality with a drop-resistant body specialized for the site. In addition, it is equipped with a glove mode that can be operated with work ... Read More
Warranty Period 1 year Display 10.1 (inch) Camera specifications 13 million pixels (CALS compatible) Resolution 1920×1200 storage 32GB Memory Capacity 3GB Mass (g) 503 Temperature Range (℃) 5~35 drop height (cm) 75 processor (GHz) 8 core 2.0GHz Dimensions, Width W x Height H x Depth D (mm) About 259 × 168 × 8.6 OS Android8.1 Operation Glove touch compatible Dust / Water Protection IPX5/IPX8、IP5X Cable USB TypeC
Construction photo management software for general buildings and small-scale sites. You can manage both digital camera and electronic small blackboard photos in a construction photo ledger.
"Kuraemon Pad Tough" is a model that is dustproof and waterproof, as well as drop and heat resistant and cold resistant. The second generation is equipped with a dual camera, which is the first robust tablet sold in Japan. The ultra-wide-angle lens allows you to photograph every corner ... Read More
Temperature Range (℃) -20~60 drop height (cm) 120 Resolution 1280×800 Camera specifications 16 million pixels (CALS compatible) storage 32GB Memory Capacity 4GB Mass (g) 520 Display 8 (inch) (gorilla glass 3) processor (GHz) 8 core 2.0GHz OS Android8.1 Dimensions, Width W x Height H x Depth D (mm) Approx. 235 x 146 x 13 Dust / Water Protection IP67 Warranty Period One and a half years Operation Physical button Cable USB TypeC Conform to microSDHC 32GB recommended
"Digital construction photo management" software compatible with digital cameras and electronic small blackboards. Construction photo management software for general buildings and small-scale sites. You can manage both digital camera and electronic small blackboard photos in a construct... Read More
Kuraemon Purveyor 17 is construction photo management software that complies with the guidelines / standards of the Ministry of Land, Infrastructure, Transport and Tourism, the Ministry of Agriculture, Forestry and Fisheries, NEXCO, and the Metropolitan Expressway.
* The major difference between ... Read More
Memory 1.5GB or more recommended Suitable CPU Intel CPU 1GHz or more Supported browsers Internet Explorer 11、Microsoft Edge Supported OS Windows 10、Windows 8.1、Windows 7 Printer Color printer recommended