Japanese Input Systems
- OMRON SOFTWARE Wnn8 for Linux/BSDJapanese input system compatible with Linux and FreeBSD. The "input prediction function", which was first installed in the previous version "Wnn7" and has improved input efficiency, has evolved further. It not only predicts input candidates based on the "standard predicti... Read MoreMemory 64MB or more Supported OS Linux Disc 65MB free space Suitable Models IBM PC/ATCompatifrom S$139.90Min. 7 days
- OMRON SOFTWARE Wnn7 Personal for Linux / BSD Academic versionJapanese input system compatible with Linux and FreeBSD. "Easy input" function that memorizes words entered once and predicts and converts the character string that the user will input next according to the frequency of use, reverse lookup function that examines the "reading" ... Read MoreDisc 60MB or more free space Supported OS Linux、FreeBSD Suitable Models IBM PC/ATCompatifrom S$99.90Min. 7 days
- OMRON SOFTWARE Wnn8 for Linux / BSD Academic versionJapanese input system compatible with Linux and FreeBSD. The "input prediction function", which was first installed in the previous version "Wnn7" and has improved input efficiency, has evolved further. It not only predicts input candidates based on the "standard predicti... Read MoreDisc 65MB free space Supported OS Linux Suitable Models IBM PC/ATCompati Memory 64MB or morefrom S$99.90Min. 7 days
- OMRON SOFTWARE Wnn7 Personal for Linux/BSDJapanese input system compatible with Linux and FreeBSD. "Easy input" function that memorizes words once entered and predicts and converts the character string that the user will input next according to the frequency of use, reverse lookup function that checks the "reading" of... Read MoreSuitable Models IBM PC/ATCompati Supported OS Linux、FreeBSD Disc 60MB or more free spacefrom S$139.90Min. 7 days
- Fujitsu Middleware Japanist 10Japanese input software compatible with Windows 10 UWP apps. Equipped with a new multi-board that realizes comfortable input not only from the keyboard but also from the touch operation of the tablet. In addition to using it daily as a soft keyboard, you can also search for obfuscated characters ... Read MoreSuitable CPU 1GHz or more Suitable Models IBM PC / AT compatible machine Memory 2GB or moreDiscontinued
- JustSystems ATOK 2017 for Windows [Premium] Normal versionA smart Japanese input system that realizes comfortable conversion. In this version, deep learning technology has been applied to renew the conversion engine, and the conversion accuracy, which is the basis of the Japanese variable input system, has been greatly improved. Furthermore, with the &q... Read MoreDisc 1.5GB or more Suitable Models IBM PC / AT compatible machineDiscontinued
- JustSystems Medical Dictionary 2020 + for + ATOK + Regular EditionATOK terminology conversion dictionary. ATOK terminology conversion dictionary. By adding to the Japanese input system "ATOK", we will support efficient input in the medical field where term standardization is advancing. We strongly support the creation of various documents and reports ... Read MoreDiscontinued