Universe / Astronomy
Other Related Pages
- Artec 100x handmade astronomical telescopeA handmade astronomical telescope with a magnification of 100 times! You can observe the craters of the moon and the rings of Saturn. Since it is a handmade type, you can learn the structure of the telescope. Tripod is not included. When observing, use a commercially available telescope or camera... Read MoreDimension (mm) 600 × 110 × 70 (completed) Material Paper, glass, wood
- Artec Paper craft globeScale 1/120000000 Ball Diameter (Φmm) About 106 Dimension (mm) About 106 × 115 × 160 (completed) Material PP, paperfrom S$4.49Min. 2 days
- Artec SP Astronomical Telescope Craft KitYou can freely draw pictures to create your own astronomical telescope! Magnification 17x Keplerian astronomical telescopeMaterial Paper, PPMA Overall Length (m) About 405 Mass (g) 114 Diameter (Φmm) Objective lens: 34, Eyepiece lens: 25from S$13.99Min. 2 days
- KENIS Transparent hemisphere● You can observe the sun's street.Dimension (Φmm) 200 Included Accessories 2 suction cups with rod
- KENIS Telescope assembly kit● An assembly kit that can easily make telescopes using two convex lenses. ● You can create a Kepler telescope in which you can see an inverted image by adjusting the focal point of the slide by simply bonding the lens to the attached paper cylinder and wrapping the outer side of the telescope w... Read More
- KENIS Student Constellation Quick-View Board● This is a low-cost constellation that each individual can observe. ● When observing the constellation, you can correctly understand the holding direction and direction of the constellation by placing your finger on the "finger" mark drawn on the constellation.Diameter (Φmm) About 140 Material Paperfrom S$4.89Min. 2 days
- KENIS Red LED light (for astronomical observation)It is a red LED light used for astronomical observation. The red light, which is easy on the eyes, is ideal for observing the stars in the night sky while checking the planisphere.Power Supply AA battery x 2 Diameter x Length (Φmm x mm) 39×153from S$29.99Min. 2 days
- Kenko Planetarium NEW Star Museum with AC AdapterIt is a home planetarium where you can easily appreciate the starry sky that fills the ceiling at home. It projects the main constellations in the Northern Hemisphere, or the stars in the Northern Hemisphere and the Southern Hemisphere. Also equipped with a shooting star function. An AC adapter i... Read MoreLight Source 1W white LED Projection distance (m) 2.7m distance / 1.8 × 2.2 Mass (g) 668 (including pedestal) Pattern Setting Display object: date, time Specification Observation point: 35 ° N / 35 ° S Projection method Optical Lens Optical lens Included Accessories Stand, AC adapter, 3 types of film
- Artec Space projectorAll 24 pictures of the universe! With 3 films With a booklet that you can enjoy learning about the universe! Built-in batteryMass (g) 51 Material ABS、PET Dimension (mm) Body: Φ40 × 150, Film: Φ32.6 × 4.5from S$8.79Min. 2 days
- NARIKA Small transparent hemisphere for studentsIt is used to observe and record the path of the sun. A small transparent hemisphere and a dedicated north, south, east, and west sheet are included in the set, making it ideal for group experiments. The small transparent hemisphere can also be used as a work material.from S$37.99Min. 6 days
- DBK Global Globe 20Sphere diameter 200 mm. A smart type that can be placed on a desk.Material Sphere: PS stand, Bow: ABS Scale About 1/63 million Sphere Diameter (Φmm) x Height H (mm) 200×235 Mass (g) 304from S$48.99Min. 21 days
- Watanabe Star diskSince the star color is yellow fluorescent color, it can be seen relatively clearly in dim light. The expression of the Milky Way has become more realistic with the feeling of a milky way. The stars below the horizon are covered in light gray, so you can see what stars will come up next from the ... Read MoreDiameter (Φmm) 220 Material Plasticfrom S$21.99Min. 6 days
- NARIKA BaMoonInvented by Takehiko Sato This balloon is made by printing a moon pattern on the surface and is ideal for experiments on the moon. By shining light on the inflated bamoon with air, you can reproduce what kind of positional relationship the crescent moon, half moon, full moon, etc. can be seen. * ... Read MoreBall Diameter (Φmm) 130 (Inflated state) Material Vinyl chloridefrom S$13.99Min. 6 days
- NARIKA Planetarium production kit "Etoile Plus"You can easily make a full-scale planetarium. If you use the mini dome of the set, you can reproduce it like a large planetarium. You can see the constellations all year round by adjusting the moon and time scales.Power Supply 4 AA batteries Diameter (Φmm) Mini dome: about 380from S$45.99Min. 8 days
- Showa Globes globeTopographic map / Japanese notation It is a topographic map color-coded according to altitude.Scale 1/60 million Ball Diameter (Φmm) 210 Height (mm) 335from S$65.99Min. 6 days
- Showa Globes Globe terrain map typeA globe made in Japan with a low reflection finish and large letters that is easy to read. This is a topographic map type in which changes in topography are color-coded according to climatic characteristics. It is a standard model with high practicality.Material Holder: Steel, Pedestal: ABS plastic Mass (g) 900 2018 Trusco page 10 0381 Trusco Part No. 856-0116from S$119.90Min. 3 days
- Watanabe Globe without frameIt is a frameless type of globe. It is ideal for investigating changes in the altitude of the sun depending on the season. The globes are color-coded by country in green and orange to make the letters easier to see, and the sea area is darkened along the coastline, so the land can be seen clearly.Mass (g) 525 Ball Diameter (Φmm) 230 Specification 1/55 million Material Sphere: paper, pedestal plastic Overall Height (mm) 300from S$139.90Min. 15 days
- Watanabe Constellation quick-view board (Star Harmony)A planisphere that is perfect for getting to know the starry sky. It is a planisphere made to make it easy to find the constellations in the south direction. Since the celestial sphere must be represented by a plane on the planisphere, the southern constellation expands horizontally. Therefore, o... Read MoreMaterial Plastic Diameter (Φmm) 220from S$24.99Min. 6 days
- NARIKA Large transparent hemisphereA large transparent hemisphere that can be used to observe diurnal motion and positional relationships by observing the sun, moon, and stars from inside the sphere.Dimension (Φmm) About 450 Mass (g) About 570 Material Transparent acrylic resinfrom S$299.90Min. 6 days
- KENIS Ocean type globeIt is a new type of globe that precisely depicts the state of the seabed by focusing on the ocean, which occupies 70% of the earth's surface. The land part is an image of the earth seen from space, and mountains and the like are drawn using a computer. You can also see interesting terrain suc... Read MoreScale 18.5 million Ball Diameter (Φmm) 260 Material Paper Material (Shorter Rule) metallicfrom S$179.90Min. 6 days
- NARIKA Child constellation quick-view board (1)The front side clearly states how to use the planisphere, and the back side describes the stars from 1.5 to 1.8 mag and the representative constellations of the season.Overall Length (mm) 224 Material Paperfrom S$6.19Min. 6 days
- KENIS Constellation quick-view boardStars from 1st to 4th magnitude are printed, and if you match the date and time scale, the constellation at that time will appear on the board. In addition to the constellations, the winter triangle and the summer triangle are displayed on the board. The positions of clusters and nebulae are also... Read MoreDimension (Φmm) 220 Material plasticfrom S$19.99Min. 4 days
- Raymay Fujii World globe with talking flagWhen you touch a country or national flag with a dedicated touch pen, the touch pen will tell you information about the countries of the world. globeDimensions, Width W x Height H x Depth D (mm) 320×350×250 Mass (kg) 1.1 Specification Full rotation Type Administrative type Ball Diameter (Φmm) 250 Power Supply 2 x AAA batteries (sold separately) Scale About 1/52000000from S$329.90Min. 7 days
- Watanabe Constellation quick-view board (for students)It is a convenient astronomical teaching tool that shows the starry sky of the day just by setting the time and date. This bowl shape is used in schools all over the country and has been trusted for a long time.Included Accessories Red vinyl bag Material Base metal, turntable resin Width (mm) 20 Diameter (Φmm) 210 Mass (g) 100
- KENIS Constellation quick-view boardBy matching the date and time scale, you can set the starry sky at that time and understand the constellations in an easy-to-understand manner. The attached red plastic bag illuminates the flashlight by putting it in a bag so that your eyes can get used to the starlight.Thickness (mm) 20 Diameter (Φmm) 210 (bowl type) Included Accessories Azimuth needle Red plastic bag Material Metalfrom S$29.99Min. 4 days
- NARIKA Transparent hemisphere B set (10 sets)It is used to measure the apparent position (passage) of the sun and moon. You can understand the state of diurnal motion well. By continuing to do this, you will be able to better understand the regularity of the annual movement. The transparent hemisphere is made of soft vinyl chloride, so it i... Read MoreSpecification 10 PVC sticks with suction cups Thickness (mm) Transparent hemisphere: 0.8 Base Paper 10 pieces with crosshairs Diameter (mm) Transparent hemisphere: 215from S$139.90Min. 6 days
- Watanabe globeAn administrative type globe with social and cultural color coding. Listed the most common place names of this size, which is about 4,000. No other model is so detailed and easy to read. It is the best globe for checking international events and interiors. Since it is a PVC sheet printing, you ca... Read MoreDimensions (H x W x D) (mm) 420×355×320 Mass (kg) 2 Ball Diameter (Φmm) 320 (1/40 million)from S$489.90Min. 6 days
- Raymay Fujii Globe with national flagShows national flag illustrations of about 195 countries around the world. You can learn the national flag along with the name of the country. globeScale About 1/42000000 Dimensions, Width W x Height H x Depth D (mm) 315×435×300 Mass (kg) 1.6 Ball Diameter (Φmm) 300
- Watanabe Constellation quick-view board (for teachers)The constellation map has been updated to include spectral data (color-coded according to the surface temperature of the stars). Contains Bayer designation, Flamsteed number, Messier catalog, and NGC catalog. You can use it as a guide for astronomical observation.Diameter (Φmm) 350 Included Accessories With stand for standingfrom S$169.90Min. 7 days
- NARIKA Venus Solid Paper CraftWe made a paper craft so that each student can easily learn about the phases of Venus. Assembling can be done in about 15 minutes, and you can enjoy making it as if you were working. By sliding the Venus model, you can easily learn how the shape and size of Venus seen from the earth changes.Diameter x Length (Φmm x mm) 130 × 30 (at the time of assembly)from S$29.99Min. 6 days
- KENIS Moon ballIt is a lunar ball made based on the latest survey data by the Japanese lunar explorer "Kaguya". You can learn the topography of the "moon", which is a mysterious celestial body with completely different facial expressions on the front and back, based on precise data.Included Accessories Table Manual Japan Gauge Diameter (Φmm) 305from S$249.90Min. 8 days