It has a fine mesh and is suitable for scooping up small fish and removing dust in the aquarium. The net is made of a soft material and does not easily damage the fish.
It quickly neutralizes chlorine and chloramine in tap water, which are harmful to medaka, goldfish, tropical fish, etc., and makes them harmless.
Descaling (for freshwater and seawater)
A breeding set of Artemia salina, a creature called Primitive Legs. You can observe from hatching to growth, mating, and spawning. When you put an egg in seawater, it hatches the next day and grows to a size of about 1 cm in about a month.
Dimension (mm) (Water tank) 162 x 93 x 137 Mass (g) (Water tank) 171 Material (Water tank) Plastic
It is a bait for small fish such as killifish, tanago, and crucian carp. For spawning and breeding, it is a high-protein, high-fat, high-calorie combination that allows female parent medaka to grow well.
A breeding mat made by finely crushing high-quality oak (Quercus acutissima). It can be used not only for adult breeding but also as a spawning bed and food for larvae. * Outgrown larvae may be undernourished.
* This product is made from the decayed wood used for shiitake cultivation. Due to the ... Read More
Dimensions, Width W x Height H x Depth D (mm) 280×380×60 Mass (g) 1170
● A pump that is convenient for water replacement in a water tank. ● Connect a commercially available hose to the tip of the pump and drain the water from the tank using the siphon principle. ● The tip of the suction port is designed so that it is difficult to suck fish and gravel.
It is a neutralizing agent that neutralizes chlorine, which is harmful to fish and aquatic plants, and optimizes the quality of breeding water for goldfish, killifish, and aquatic organisms.
● It contains all the nutrients needed by turtles and can be kept with this diet alone. ● Small grains should be given for small turtles, large grains should be given for turtles grown to about 10 cm, and oversized grains should be given for turtles 12 cm or more.
A convenient breeding case for raising insects. The design makes it easy to observe the inside even from the side. In addition, the lid has a hole through which the tube of the air pump can pass, so you can also breed aquatic organisms such as crayfish and killifish. The large transparent window ... Read More
● Plastic case suitable for breeding insects, fish, amphibians, etc. ● The use of special resins makes them light and difficult to crack. ●PW06FB has a wide skylight and is a flat type suitable for observation.
An outdoor aquarium fish tank. Embedded type. A luxurious design with a blackish shade. A nice garden pond can be installed in combination with a water cleaner.
As an aquarium, pond, plastic pond, gourd pond, molding pond, and garden pond. For pond making, aquarium fish, outdoors, goldfish, carp,... Read More
It is a carefully selected high quality Quercus serrata Kuchiki. Ideal for spawning trees such as Dorcus hopei binodum. After soaking it in water, it is used by embedding it in a breeding mat.
Dimensions, Diameter x Length (Φmm × mm) About 70 × 150 Material Kuchiki Mass (g) About 250
Uses a light aluminum handle, making it easy for children to carry. The length of the handle is telescopic, and the length can be easily adjusted.
Diameter x Length (Φmm x mm) 30×950~2450 Material (Handle) Aluminum, telescopic Type B36-245L Top Diameter x Depth (mm) Net: 360 × 550 Material (Net) Nylon
The frame of the net is thickened and strengthened to withstand the collection of river and sea creatures.
Diameter x Length (Φmm x mm) 25×1260~1960 Material (Handle) Aluminum, telescopic Type FN-196L Dimension (mm) Net: 355 x 385 x 300 depth Material (Net) Nylon
Mol Taro is a kit that allows you to naturally learn the three-dimensional structure of molecules while assembling simple molecules. The crystal structure can be expressed vividly, and touching the three-dimensional figure helps to understand the basic crystal structure. Different types of atoms ... Read More
● This is a thin water tank that restricts the orientation and movement of fish and makes it easy to observe living things in the water. ●[Use Example] Observation of male and female medaka: Observation of plant roots, etc.
● A special sealing structure that does not allow noise inside the air pump to escape. It is designed to be quieter than conventional pumps. ● A filter set that incorporates an air pump 2000SB, a special three-layer mat, and an activated carbon cartridge.
Dimension (mm) 103×62×160 Power Consumption, at 50/60Hz (W) 2.1/1.9 Opening Diameter (Φmm) 5 (for air hose) Power Supply AC100V(50/60)
A mix pack of insect jelly with high palatability. Recommended for multi-headed breeders and breeders.
* This product is an insect breeding product (food). Do not use it for any other purpose. * This product is harmless to the human body, but please be careful not to accidentally eat it by childr... Read More
Target Beetle insect Mass (g) 3000 Dimensions, Width W x Height H x Depth D (mm) 325×140×210
A filter that is easy to install and can be set in water. Shower method, aeration method, and normal discharge method can be selected according to the application (with flow rate adjustment function). If placed horizontally, it can be used even in shallow water.
Power Supply AC100V(50/60) Type of Filter Material Sponge mat + activated carbon (included)
The special stainless steel double frame makes it difficult to damage the net. Since the net is attached to the inner frame, the edge of the net does not wear out.
* Please check the regulations of each local government (each river) before using. * Head ○ mm is the width of the stainless steel fr... Read More
● Laboratory materials that can be used to rub and observe luminescence in the laboratory. ● 10 to 20 dried borehole tars are rubbed in a mortar, 1 to 2 mL of water is added, and the mixture is mixed in the dark to observe luminescence.