It is a dyeing solution that can change the color of flowers by letting plants such as cut flowers absorb it. Cut flowers that are sucking water can be easily dyed by simply removing them from the water for about an hour and immersing the tips of the stems in the stain solution for 10 to 60 minut... Read More
It is a dyeing solution that can be sucked by plants such as cut flowers to change the color of the flowers. Cut flowers that are sucking water can be easily dyed by simply removing them from the water for about an hour and immersing the tips of the stems in the stain solution for 10 to 60 minute... Read More
A kit that allows you to easily make postcards and bookmarks for pressed flowers. A handmade gift! A set that makes nice pressed flowers according to the season. Contains a dry sheet that allows you to easily press flowers.
It is a dyeing solution that can change the color of flowers by letting plants such as cut flowers absorb it. Cut flowers that are sucking water can be easily dyed by simply removing them from the water for about an hour and immersing the tips of the stems in the stain solution for 10 to 60 minut... Read More
Liquid Color Red, blue, yellow, green, orange Capacity (mL) 100
Convenient stain solution that can be used immediately in experiments All stain solutions are prepared Small amount type that is ideal for group experiments Easy-to-use eye drops
It is a soil for raising seedlings with excellent drainage, water retention, fertilizer retention, and breathability. Since it does not contain fertilizer, it is ideal for experiments to investigate the germination and growth conditions of plants. It can be used as a slow cooling agent for heated... Read More
You can write the scientific name, family name, Japanese name, collection place, and date. Five sheets are printed on one sheet, and it is a type that you can cut and use.
<< Guidance by Professor Yoshio Inoue, Senior High School Attached to Kyoto University of Education >> Pigments of different types of marine plants and land plants can be separated and compared by thin layer chromatography.
It is a "vegetable dyeing agent for cotton" that brings out the colors and features of plant dyeing experimental materials and plant dyeing solutions. Dyes that used to be poorly dyed in cotton can be dyed beautifully by pre-treating with a disposable dye, and dyes that have been dyed i... Read More
6th grade Plant nutrients and water passages When this agent is given to plants, it stains flowers, leaves and stems. Since it does not die easily even if it is given for a long time, it is easy to understand how to absorb water from the plant. When experimenting with wildflowers, flowers and lea... Read More
Capacity (mL) 100 each tolerance V Up to 2 times possible Color Red and blue (one each)
Used in combination with the vegetable dyeing experimental material, G40-5702 Dispon. If you dye the cloth pre-treated with Dispon with this "Suou", it will be dyed in a beautiful red color.
A convenient stain that can be used immediately in experiments. Concentration adjusted. A small amount type that is ideal for group experiments. Comes in an easy-to-use eye drop bottle.
A safe Tsurugren device that uses a disposable body warmer as a heat source. Since it does not require a power supply, there is no need to worry about securing a power supply or the location of the outlet.
It is a soil animal extraction device that utilizes the habit of small animals in the soil to avoid light and heat. Small animals in the soil can be efficiently extracted alive.
Tulip seeds for observation. It can be used when explaining asexual reproduction by bulbs and sexual reproduction by seeds, and for introducing classes.
* Seeds are sorted and manufactured for observation, so germination cannot be guaranteed. Also, if it germinates, it takes 5 years for the flowe... Read More
Acidic soil with excellent breathability and water retention. It turns yellow when it contains water and turns white when it dries, so it is easy to judge the dryness of the soil. Since it contains almost no germs, it is also suitable for cuttings.
Invented by Professor Emeritus Tadashi Ryokawa of Kyoto University It can be used for experiments to compare the germination conditions of plants in the fifth grade of elementary school. Since the bag can be sealed, it prevents water from evaporating, so the medium can be kept moist and the plant... Read More