3rd grade elementary school An experimental instrument with a solar cell and a propeller driven by a solar cell attached to the nature of light, which is ideal for experiments that collect light reflected by a mirror. When the light reflected by the mirror hits the solar cell, the solar cell gene... Read More
Motor 1.5V~3V、210~250mA Dimension (mm) 240×210×100 Type A set Battery Photocell: 1.7V, 450mA
It is a work kit to make a wind power generator using a PET bottle. Special specifications that rotate and generate electricity with a light force! LED shines!
* PET bottles are not included.
Conform Science Elementary School 6 years Material PP
Assembly kit for a miniature car that runs on a small solar battery You can see the internal structure with a transparent body. Lightweight design equipped with a micromotor By adjusting the angle of the rear wheels, you can freely change straight ahead, right turn, and left turn. The solar cell ... Read More
Battery 1V、100mA Dimension (mm) 74×30×36 Material ABS Conform Science Elementary School 4 years
This motor is suitable for wind power generation experiments. It is a high-performance power generation motor that rotates with a small amount of force and generates an electric current, making it ideal for wind power generation experiments.
Rotational Speed (min -1 [rpm]) 1050 Current (mA) 20 Voltage (V) 3 Subject Science Conform Science Elementary School 6 years Dimension (mm) Φ25×42
You can convert thermal energy into electrical energy and electrical energy into thermal energy.
Voltage (V) (Maximum) 15.4 Mass (g) 27 Dimension (mm) 40×40×3.8 Maximum Current (A) 6 Material Aluminum Specification Maximum temperature difference: 68 ° C
Assembly kit with electronic music box and LED! Because it is an assembly kit, you can understand the structure of the generator well! The tone of the electronic music box changes depending on the amount of power generation. Artec's multi-generator series Small and easy to handle, ideal as an... Read More
Cable Length (m) 1 (with Minomushi clip) Dimension (mm) 106×53×70 Maximum voltage (V) 7 Material ABS Conform Science Elementary School 6 years
A polycrystalline silicon type photovoltaic cell that is easy to use for experiments and crafts. High power up to 1.7V !!
Main Unit Dimensions (mm) 110×60×3 Maximum Output (W) 0.57 Short Circuit Current (mA) 415 Voltage (V) (Action) 1.44, (Release) 1.7 Mass (g) About 28 Current (mA) (Operation) 400
A mysterious pipe that moves the temperature of things quickly! A heat pipe has a highly volatile liquid sealed in a decompressed pipe. In the high temperature part, the liquid evaporates and takes heat away, and heat can be quickly transferred to the low temperature part.
* Be careful not to tou... Read More
It is a mechanical work kit that runs on solar cells. You can freely reassemble and enjoy 4 types of designs that are popular with kids. Designed like Solar Dynasaw T-REX. Walk forward on two legs. Jet drill Travels while rotating the front drill. Solar Hercules Walk while moving the corner up an... Read More
RoHS directive (corresponding to 10 substances) Correspondence Power Supply Solar cell (included)
● This is an inexpensive type of photovoltaic device. It is recommended for manufacturing processes in which an electronic organ is sounded or a motor is turned. ● Use sunlight or an incandescent lamp of 150 W or more as the light source.
Dimension (mm) 60×110 Included Accessories Caterpillar lead wire Output DC2V ・ 267mAh (sunlight)
6th grade Electricity utilization This is a hand-held hand-cranked DC generator that is very convenient as a power source for energy conversion experiments and water electrolysis experiments. By turning the handle, you can generate a DC voltage of 12V or more, and it is the definitive educational... Read More
Cable Length (m) 1 Dimension (mm) 115×140×43 Mass (g) 120 Material Made of polycarbonate Output Maximum DC about 12V
T-Rex, elephant, crocodile, monkey, ostrich, scorpion, pteranodon, dog walk, excavator, forklift, rover, buggy, etc. A robot work kit that transforms into 12 types of animals and mechas. The movement and shape of the robot resemble the characteristics of actual animals and mecha, and are carefull... Read More
RoHS directive (corresponding to 10 substances) Correspondence Battery Solar cell (included)
Open Voltage (V) 0.57 Outer Dimensions, Length x Width x Thickness (mm) 154.9×56×1.2 Maximum Output (W) 0.75 Short circuit current (A) 1.8 Maximum Output 0.45V
It is possible to compare the speed of heat energy transfer (heat conduction) with a set of a heat pipe with a reduced pressure inside and a copper pipe with an open pipe. Since the air pressure inside the heat pipe is low, the water that is trapped in it instantly boils and becomes steam, which ... Read More
You can see how you can use 6th grade electricity and turn the handle to generate a DC voltage of about 3V and make your own electricity. Since the generated voltage is about 3V, it is difficult to damage the miniature bulbs, LEDs, and electronic music boxes (electronic melody) used in elementary... Read More
Dimension (mm) 115×140×43 Mass (g) 120 Output Approx. 3 V DC Included Accessories Dedicated output code (red / black, 1m) Material Polica-Bonate
It is a power generation kit for both thermal power and hydraulic power that has a structure in which a motor for power generation is attached to a steam turbine and the turbine can be rotated even with hydraulic power. Water vapor generated by heating water is used for thermal power generation, ... Read More
This kit allows you to easily experiment with the principle of a heat pump that transfers heat by pressurizing and depressurizing the refrigerant (gas or liquid). By putting a liquid crystal thermometer in the PET bottle and pressurizing it with the attached pressurizing pump, you can check that ... Read More
An amorphous solar cell that can be bent lightly. It can be used for departments, experiments, and practical training related to the environment, energy, and power management, such as investigating the power generation principle and characteristics of solar cells.
It is an ultra-compact mini solar car that runs at high speed. The lightweight design with a micromotor allows it to run vigorously. It is a small size unit finished product. It cannot be disassembled.
Mass (g) (Body) 4 Dimension (mm) Body: 23 x 32 x 14 Storage Case Made of plastic (90 × 70 × 27mm)
A corrugated cardboard solar cooker with an aluminum reflective film attached. It weighs only 500g per unit and can be folded smaller than A3 paper. It is a single cardboard box and does not use any tools for assembly. There are two installation methods, summer specifications and winter specifica... Read More
Mass (g) 500 Highest Temperature (℃) With no calm weather: Approx. 150
You can observe that the LED lights up by electromagnetic induction when you attach a magnet to the buzzer, rotate it, and bring it closer to the coil. The effect of electromagnetic induction is enhanced by rotating the magnet at high speed. You can enjoy learning electromagnetic induction with a... Read More
A high-efficiency, maintenance-free small wind power generator that matches the Japanese wind environment. Power generation starts from the breeze speed where the leaves sway. In addition to deepening your understanding of wind power generation, it is also ideal as a theme for environmental learn... Read More
Body Length (mm) 130 (300 including tail) Material AES resin Mass of Main Unit (g) About 300 Structure Drip-proof
A work set that uses the power of a unit that has a power generation motor set to generate electricity by turning it by hand. The motor runs on electricity, but on the contrary, it has the property of generating electricity (generator) when the motor is turned by hand. It is this work that uses i... Read More
A large 70 mm square Peltier module for power generation. With the Peltier module, even a low-quality heat source (100 ° C or less) that cannot drive a steam turbine can obtain electrical energy immediately anywhere if there is a temperature difference. Since the upper and lower surfaces are made... Read More
Type (For power generation) Dimension (mm) 72×72×5 temperature difference (℃) 80~85 Output Voltage (V) Maximum: 4.8
It is an experimental device that uses the power of the wind to turn the propeller and experience power generation. You can check the power generation by sound and light by turning the propeller by blowing it with a fan or blowing it with your mouth.
A mysterious device that can generate high-voltage static electricity only by the force of falling water droplets. The generated static electricity can be confirmed by lighting the LED. Ideal for introducing electrostatic experiments and learning electrostatic induction.
Dimension (mm) 300×200×450 Mass (g) 850 Material Acrylic
An electromotive force is generated when a temperature difference is applied to both sides of the module, and conversely, when an electric current is applied, a thermoelectric semiconductor Peltier module that absorbs heat from one side and dissipates heat from the opposite side, usually sandwich... Read More
Main Unit 40-square Peltier module Dimension (mm) Cooling unit: 45 x 46 Type skeleton
It is a kit that makes it easy to make a car that runs on the electromotive force of a photovoltaic cell. It has a simple structure with a photovoltaic panel as the car body and can be assembled without the need for tools. With a total weight of 110g, it runs faster than conventional photovoltaic... Read More
Wheel Diameter (Φmm) 46 Dimension (mm) 90 × 150 × 100 (when completed) Specification Dedicated motor gear Dedicated lead wire
It is also easy to use for Joule heat experiments with electric current, and uses direct current or alternating current of about 6V for the power supply. The lid of the container is made of transparent plastic so that the inside can be seen.
Diameter x Length (Φmm x mm) Copper container: 75 x 75 design temperature (℃) -40 to +260 (probe thermometer) Material Lid: Transparent plastic (with terminal)
It is a kit that allows you to create an original solar car using empty containers such as PET bottles and milk cartons. Since the speed of the car changes when the light is applied differently, it is possible to investigate the function of the photovoltaic cell and the strength of the electric c... Read More
[No soldering required] The world's smallest miniature solar car equipped with a solar battery, based on the model that was active in the actual race. Easy to assemble, just fit and screw. Although it is about 10 cm in length and is palm-sized, it runs lightly in the sunlight.
This product is a fuel cell learning kit that uses magnesium and oxygen in the air to generate electricity. You can learn the fluctuation of energy generated by using saline solution as the electrolyte and changing its concentration and temperature.