Perfect for your first block! You can enjoy it from the beginning by shaking, stacking, and rolling. Fun to see, fun to shake, fun to stack. The large size makes it easy to pick up, and the beautiful color and pleasant sound that can be used as a rattle nurture your heart. The blocks with all-blo... Read More
Suitable age (years) 1 year old ~ Set Contents Tsumiki with sound x11, wooden box x1
A model that appeared to commemorate the 60th anniversary of the release of the BRIO Crown. In addition to the conventional shape matching elements, we have also incorporated elements that match patterns.
Suitable age (years) 12 months ~ Dimensions, Width W x Depth D x Height H (mm) Approximately 70 x 70 x 242 Material Wood
A lovely pull toy that comes with your hips shining when you pull the string. For toddlers. Uses 2 alkaline AAA batteries (sold separately)
Suitable age (years) 12 months ~ Dimensions, Width W x Depth D x Height H (mm) Approximately 112 x 110 x 106 Material Wood / ABS / PP / EVA / Polyester
This is a model made to commemorate the 60th anniversary of the release of BRIO's representative pull toy "Dutchie", which is familiar with its black body and red tires.
Suitable age (years) 12 months ~ Dimensions, Width W x Depth D x Height H (mm) Approximately 200 x 93 x 88 Material Wood / ABS / Polyester
A building block where you can experience the fun of imagining with your parent and child. Mickey wears hakama, and Chip and Dale wear Kintaro's costume. The compact size makes it easy to decorate, making it easy to create Children's Day! The carp streamers sway and can be played as a bal... Read More
BRIO's representative bestseller. A classic toy that has been loved all over the world since its launch in 1958, and learns assembly procedures and color identification by stacking eight wood pieces.
Suitable age (years) 12 months ~ Dimensions, Width W x Depth D x Height H (mm) Approximately 70 x 70 x 242 Material Wood
A high deluxe set of builders assembled from wood and plastic. What you make depends on your child. Let's get creative and make an original model. Includes hammer, screwdriver, pliers, spanner, and example collection. All 271 pieces.
Suitable age (years) 3~ Material Wood / ABS / PP / TPR
Colorful and washable building blocks "Biobro" The color that attracts children's interest, the shape that draws out new ideas, and the washable building block bioblo made from hygienic materials. The colors are not painted but are mixed in during manufacturing, so the colors will n... Read More
Suitable age (years) 3 or more Material Wood, plastic
A popular drop-in box that promotes the development of shape and color recognition ability. Align the building blocks with the shapes of the round, triangular and square holes and get them in the box well. If you pull the handle on the front of the main unit, the building blocks inserted from the... Read More
Suitable age (years) 12 months ~ Dimensions, Width W x Depth D x Height H (mm) Approximately 130 x 144 x 110 Material Wood
Come on, makeover !! Train blocks turn into crocodile !? Load the colorful blocks on the crocodile's dolly and leave! A cute toy with a crocodile's body made of blocks. If you change the stacking method, the crocodile will be transformed into a train. You can also play as a pull toy by pu... Read More
Suitable age (years) 3~ Dimensions (cm) 44 × 8 × 10, 4.2 × 4 × 2 (minimum parts) Set Contents Blocks x 19 and trolleys x 3
A giant jumbling tower with a refreshing sherbet color. Sunny Life balance jenga game. Pieces made of natural wood are lightweight and durable ◎ Not only as a game, there are various ways to play such as building blocks and playing dominoes.
*Because it is an overseas product, there may be indivi... Read More
Dimensions, Width W x Depth D x Height H (cm) 12×12×45 Mass (kg) 2.7 Suitable age (years) 6 years or older Material Wood
An introductory set of builders assembled from wood and plastic. Promote hand-visual coordination while playing. Comes in a toolbox with pliers, spanner and example collection. All 49 pieces.
A classic pull toy that has been enjoyed by children and their families around the world since its launch in 1958. When you pull the string, it will follow you while shaking its tail.
Suitable age (years) 12 months ~ Dimensions, Width W x Depth D x Height H (mm) Approximately 200 x 93 x 88 Material Wood / ABS / Polyester
67 pieces of parts come with a recording / playback device and easy-to-use tools. Expand the world of play with the recording / playback function. All 67 pieces. Uses 3 LR44. (Included for trial)
A set of 120-piece parts, battery-powered light parts, and tools. Each light part has four modes: on, off, blinking, and pulsating, and the transparent plastic gives it a variety of colors. All 120 pieces. Uses LR44 x 8 pieces. (Included for trial)
It comes with a battery-powered motor and easy-to-use tools. The battery-powered motor has forward, stop, and reverse modes. All 120 pieces. Uses 2 AAA batteries. (Sold separately)
Comes with a booklet with tips for watching over children's free play! A simple set of blocks that can be played for a long time under the supervision of an infant classroom. A gorgeous package with bold illustrations of blocks is perfect for gifts. Tsumiki is a simple design that brings out ... Read More
A cute wooden toy with a Scandinavian taste in gentle colors. A building block set containing 60 blocks of various shapes. Playing with building blocks develops your child's creativity.
As an educational toy, it can also be used as a baby gift or as a gift.
A standard set of builders assembled from wood and plastic. What you make depends on your child. Let's get creative and make an original model. Includes hammer, screwdriver, pliers, spanner, and example collection. All 136 pieces.
Suitable age (years) 3~ Material Wood / ABS / PP / TPR
A deluxe set of builders assembled from wood and plastic. What you make depends on your child. Let's get creative and make an original model. Includes hammer, screwdriver, pliers, spanner, and example collection. All 211 pieces.
Suitable age (years) 3~ Material Wood / ABS / PP / TPR
Biobro Fun Box Colorful and washable building blocks "Biobro" Biobro jointly developed with an Austrian educational institution. The secret is the color that attracts children's interest, the shape that brings out new ideas, and the material that considers hygiene. The biggest feat... Read More