Chainsaws
Other Related Pages
- Oregon Saw Chain 25APHigh-performance chain that is easy to maintain. It has a very light and smooth sharpness and has gained overwhelming support in the Japanese market for many years. In addition to the high performance of the chisel chain, the micro chisel cutter is also characterized by its ease of maintenance. T... Read More
- Nishigaki Industrial Chainsaw depth adjusterIt plays an important role in adjusting the bite of the blade and maintaining the optimum sharpness. Please use it when it does not slip even after sharpening. * The depth gauge adjuster is set to a general saw chain (0.025 inch) of about 0.6 mm.
- SAMURAI LEGEND Chainsaw file flat typeA hexagonal file suitable for chisel saw chains. Please use it for sharpening large chainsaws.RoHS directive (corresponding to 10 substances) Correspondence
- EARTH MAN Combination box spanner for engine chainsawFor attaching / detaching the plug (19 mm), for replacing the chain (replacement blade) (13 mm), for adjusting the tension of the chain (-6 mm)
- Oregon File Handle WoodenA handle designed for ease of grip and movement during sharpening work. Can be used with 4mm to 8mm Oregon files.
- Oregon Saw chain 91FFor bamboo cutting and hardwoodTeeth Spacing 0.375 Gauge 0.50(1.3mm)
- BOSCH Cordless Micro SawAdopting the world's first newly designed nano blade technology Smooth and smooth cutting in a cross section close to vertical is possible without tools Easy blade attachment / detachment SDS system Stable cutting with one hand is also possible Pruning of outdoor trees and cutting of wooden b... Read More
- Tsumura (Suehiro Seiko) Tip Replacement Harvester BarTeeth Spacing .404” Gauge .080”(2.0mm)from S$299.90Min. 2 days
- SUGIHARA Chain saw guide bar hard bar lightweightThe tip of the body carved from a single plate of extremely strong special steel has a cemented carbide welded structure. Suitable for use under harsh conditions such as cutting hard wood. There are few breakdowns (work is not interrupted). It can be corrected even if it is caught in a tree. The ... Read More
- BIG-M (Maruyama Mfg) Engine chainsawThe recirculator engine is fuel efficient and environmentally friendly. BIG-M R start that makes it easy to start the engine. High safety with large bumper guard and automatic inertia brake. Side access oil adjuster. Intes bar with easy chain tension. Power sharp compatible guide bar. * Dedicated... Read MoreSuitable for Chainsaw blade: 91PX-52E Fuel 2-cycle mixed fuel (25: 1 mixed) Fuel Tank Capacity (L) 0.34 Oil Tank (L) 0.3 Starting Method R start Spark Plug CJ-6Y
- BOSCH Cordless chainsaw body only UC18HEasy chain mounting and tension adjustment without tools, SDS system. Equipped with non-slip rubber grip, hand guard, side handle, and battery level indicator. Equipped with a tip guard that can be easily hooked and cut. ※only a main partConform to Powerful Li-ion18V Lubricating Automatic Chain type 90XP-033Efrom S$359.90Min. 5 days
- Marunaka Chainsaw with rechargeable batteryUnlike the engine type, there is less vibration and you can work easily. Uses power mode and eco mode switching. In power mode, the chain speed is 13.3m / s, which is comparable to the engine type. The guide bar and saw chain uses a thin blade with outstanding sharpness, so the work speed is so f... Read MoreVoltage (V) 36 Maximum Rotation Speed (min -1 [rpm]) (Power mode) 7,000, (Eco mode) 6,000 Motor Brushless motor Battery Capacity (Ah) 2.5 motor output (W) Maximum: 820from S$599.90Min. 8 days
- Shindaiwa Electric chain sawBoasts ease of use and sharpness. Please use it for home use as well.Included Accessories Standard tool set Type With chain brake Current (A) 14 Power Input (V) Single phase 100 Power Consumption (W) 1300 Oil Tank (L) 0.1 Chain type 91PX-52E
- Strong Tool Chainsaw sharpening guideEasy to install! Compact and convenient to carry! Just file with a file according to the guidelines!from S$19.99Min. 4 days
- SHINKO (Shinko MechatroTech) ChainsawAutomatic refueling type. The switch is double type and safe. Uses a sharp Oregon saw chain. Uses a rubber grip that is easy on the hands. For cutting logs (firewood), pruning, rough cutting of sculptures, etc.Frequency (Hz) 50/60 Current (A) 11 Power Input (V) Single phase 100 Power Consumption (W) 1050 Chain type Oregon 91VG-46from S$129.90Min. 5 days
- BAHCO Ergo Chainsoyas reset with guideMaterial High performance alloy steelfrom S$59.99Min. 3 days
- SHINKO (Shinko MechatroTech) Electric chainsawFor cutting logs (firewood), pruning, rough cutting of sculptures, etc. Automatic refueling type. The switch is double type and safe. Uses a sharp Oregon saw chain. Uses a rubber grip that is easy on the hands.Frequency (Hz) 50/60 Current (A) 13.9 Power Input (V) Single phase 100 Power Consumption (W) 1350 Chain type Oregon 91VG-52from S$139.90Min. 5 days
- Oregon Saw chain 91PXStandard type with sharp sharpness and little kickback. Cutting performance is further improved by eliminating the bumper tie strap that prevents kickback and improving the blade attachment method. The cutter is a chamfer chisel with a reputation for sharpness, and the two cutting corners make th... Read More
- Vallorbe Chainsaw FileRound file from Valorbe, Switzerland. Ideal for sharpening saw chains. It has excellent machinability and long-lasting sharpness.
- Tsubosan Chainsaw fileA file specializing in chainsaws. Since it uses a soft grip, it fits comfortably in your hand. Since the raw material is made in Switzerland, it has excellent grinding power. The sharpening angle is determined for each type of chain blade. Comes in a storage bag that is convenient to carry. Consp... Read More
- Oregon Round fileA round file for saw chain that is indispensable for accurate chain sharpening work. Heat treated steel with excellent durability is used. 4.0mm/4.5mm/4.8mm/5.5mm/files are now colored one by one so that the size can be easily identified.
- Oregon Saw Chain 91VXLKickback suppression function that is safe for professionals. The BPX type of micro chisel cutter is favored by many professionals due to its high cutting performance. Despite being for professional use, the newly designed drive link significantly reduces kickback. A chain that can be used with g... Read MoreTeeth Spacing 0.375 Gauge 0.50(1.3mm)
- Oregon Sharpening clampA clamp that is set on the guide bar to improve stability when sharpening the chain at the work site. It is one of the most convenient tools to have.
- Oregon Saw chain 90PXLightweight chain with the narrowest cutting width. The 90PX is a saw chain with a shorter profile (height) and a narrower drive link. The feature of this chain is the chamfer chisel cutter, which improves cutting efficiency and maintains sharpness at the same time. In addition to the vibe van th... Read MoreTeeth Spacing 0.375 Gauge 0.043"(1.1mm)
- Oregon Saw chain 25F For bamboo cuttingBy doubling the number of 25AP cutters, which have been overwhelmingly popular in the market for many years, it has become easier to cut dense fibers. The micro chisel cutter has slightly rounded corners for fast and smooth cutting. Since the cut surface is smooth due to the "Full House Cutt... Read MoreTeeth Spacing 0.25 Gauge 0.050(1.3mm)
- SAMURAI LEGEND 1411SP SochenSamurai Legend 1411 Low Kick Roller Bar Compatible Saw Chain. Slender, low blade height, bites smoothly, and cuts at high speed. Saw chain for chainsawSuitable for PFERD3.0mm round file Teeth Spacing 1/4inch Gauge 0.043inch RoHS directive (corresponding to 10 substances) Correspondence
- Oregon Sochen 95TXLIt is a chain that further enhances the effect of 95VPX, which has been highly evaluated for its excellent efficiency and weight reduction. With the introduction of a new cutter polishing process, it is designed to improve cutting performance and facilitate sharpening. In addition, by reviewing t... Read MoreTeeth Spacing 0.325 Gauge 0.50(1.3mm)
- SUGIHARA Chain Saw Guide Bar 3-pcs Sprocket Nose Bar LightweightThe body has a laminated structure in which three steel plates are welded together, and has a sprocket nose at the tip. The tip is composed of sprockets and bearings, so it does not come into contact with the side links of the chain and the power loss of the engine is small. * Please check the co... Read More
- SAMURAI LEGEND 1411 low kick roller barGuide bar for Samurai Legend 1411SP. The tip roller and 1411SP, which has a thin cutting width, suppress resistance and achieve excellent cutting speed and sharpness. Ideal for small engines and battery chainsaws. Chainsaw guide barTeeth Spacing 1/4inch mount For domestic chainsaws only Gauge 0.043inch RoHS directive (corresponding to 10 substances) Correspondence
- PFERD Round File for Saw ChainRound file from Ford of Germany, the blade shape is a traditional classic type. It boasts high machinability and long life. For saw chain blade grind.
- IWOOD Diamond chainsawBrightly polishes hard cutting edges in a short time
- YAMAGUCHI Chainsaw FileA file for chainsaws. For sharpening and regenerating chainsaw blades.
- Oregon Angle plateThe correct sharpening angle is displayed on the plate, and you can perform accurate sharpening by filing according to this angle. It is used by freely adsorbing it to the required part of the guide bar with two built-in magnets.dressing angle (°) For 25/30
- TRUSCO Chainsaw FilesA file specializing in chainsaws. Since it uses a soft grip, it fits comfortably in your hand. Conspicuous regeneration of chainsaw blades * If it is clogged, remove it with a brush etc. before use. * The sharpening angle is determined for each type of chainsaw blade.Abrasive Grit Size Second
- Ryuhomaru Chainsoya Sribit All sizes are sharedA diamond bit for sharpening the blade of a chainsaw. It is used by attaching it to an electric drill, impact driver, etc.Material Industrial electrodeposition diamond Size All sizes are shared Mass (g) 12
- BLACK&DECKER Cordless chainsaw spare bladeSuitable Model GKC1820L、GPC1820L、CCS818 Type 90SG-34 frames
Filter by categories