Drafting & Marking Tools
Other Related Pages
- KAWAGUCHI Sewing penIt is used for fixing patterns and cutting fabrics. The dents on the sides fit comfortably in your hand and are easy to hold.Mass (g) 370 Color Brown Material Iron
- Clover Mfg Hatron paper colorFor tracing and drafting patterns. It is a 3-color set. Many of the patterns for clothes have similar shapes, such as the front and back of the skirt, so it is convenient to color-code each part so that they can be easily distinguished. By making a pattern for small parts (such as collars and cuf... Read MoreColor Blue, pink, yellow Dimensions (cm) 78×109from S$9.99Min. 3 days
- Clover Mfg Hatron paper whiteFor making patterns by tracing actual large paper, or for drawing clothes. Easy-to-use roll type. You can cut only the amount you use without waste, and you can draw lines neatly because there are no folds. The transparent kraft paper makes it easy to trace the actual large size paper that is pri... Read MoreLength (m) 21 Width (mm) 60
- VANCO Light table plus LEDA comfortable operating environment is realized by separating the "ON / OFF" and "dimming" buttons made in Japan for peace of mind. We have realized a working environment. The brightness can be adjusted in 7 steps according to the work environment. Working in a comfortable amo... Read MoreThickness (mm) 7
- Clover Mfg Hatron paper roll typeIt is used when tracing a large size paper to make a pattern or drawing clothes. You can cut only the amount you use without waste, and you can draw lines neatly because there are no folds. The transparent kraft paper makes it easy to trace the actual large size paper that is printed on top of ea... Read MoreDimensions, W (mm) x L (m) 60×7
- Clover Mfg Iron Chaco Pen WhiteA white marker suitable for black and dark cloths. The mark disappears with the heat of the iron or washing with water. Since the ink develops white, the marks can be seen even with a black cloth or a dark cloth.
- Kawamura Seichu Royal powder chalkIt is a popular and easy-to-hold triangle for a wide range of people from beginners to advanced players. Can be replaced with one touch and does not stain your handsDimensions (H x W) (cm) 6.5×6
- Clover Mfg Fabric weightMaterial ABS resin, iron Dimensions (Vertical x Horizontal) (cm) About 16.3 × 6.3
- KAWAGUCHI Green Cut Drafting PaperIt can be used not only for dressmaking, but also for patchwork, handicrafts, and general handmade patterns. There are many advantages that paper patterns do not have.Material 100% pure pulp Width (mm) 950
- Clover Mfg Seam Allowance LinerThis is useful for copying patterns and templates such as appliqués and Hawaiian quilts.
- Clover Mfg Tracer twinA stylus that is ideal for copying designs using chacopies. A ball tip type that does not easily tear patterns and copy paper and allows smooth copying.
- Clover Mfg Eraser pen for chaco penA brush-shaped nib that can be used in two ways. It is a design that shows the features at a glance. You can cleanly erase only the part you want to erase the mark made with the water-based chaco pen. You can use it in two ways, using the tip to erase small parts and the side of the pen tip to er... Read More
- Kawamura Seichu Powder chalk for refillingPowder chalk replenishmentDimensions (H x W) (cm) 3×2.5
- Clover Mfg Iron Chacopen White 2 coresA convenient replacement core for ironing chaco pens. A replacement core has been added to the iron chaco pen, which is a standard marking for dark cloth. When the ink runs out, you can easily replace it with the replacement bracket.Included Accessories 1 replacement bracket
- Clover Mfg Water-based chacopen <purple thick>The sign lasts a long time. It disappears naturally over time. It is a design that shows the features at a glance. A marker-type chaco pen whose mark disappears naturally over time. If you want to erase the mark immediately, you can erase it with water or a special eraser pen. The pen tip is a th... Read MoreColor Purple Type Thick
- Sun Coccoh Dressmaking chalkA triangular dressmaking chalk that is easy to hold. Introducing a triangle that makes it easy to hold dressmaking chalk, which is indispensable for marking! You can use it with a smooth feel without damaging the fabric.Material Kaolin and oil pigment
- Clover Mfg Grid pattern sheetA plastic sheet for making pieces that can be drawn with a pencil. Since it is translucent, you can easily copy the design.from S$7.19Min. 2 days
- KAWAGUCHI Chaco Ace EWith a convenient eraser pen when you want to erase immediatelyfrom S$5.39Min. 2 days
- ADGER Chaco Ace White A Chaco PenWhite chaco marker for black fabricColor Whitefrom S$5.39Min. 2 days
- Clover Mfg ChacopyPaper chaco that is convenient for design and paper pattern copying. It has a dark and clear mark, and the mark is easy to erase by washing with water. Gray is a color that is easy to see even on light-colored fabrics.
- Clover Mfg Chaco liner penA powder type that allows you to play thin and clean lines.
- Nippon Chuko Patchwork spatulaDimensions, Width W x Depth D x Height H (cm) 11.5×0.2×2.5
- Chacopaper Chalk PaperSince it has the characteristic of disappearing with water, it is mainly used for handicrafts, sewing patterns, and copying patterns. Copy paper that can be used for various materials such as cloth, paper, wood, synthetic paper, synthetic leather, plastic, glass, ceramics, and metal.Size (cm) 28×23 Set Contents Blue, yellow, red, white, green x 1 each Type One side
- Clover Mfg Clover New Chacopy <5-color set on one side>The signs are clearly visible and easy to erase! Crovertia copy has a new package and contents! The single-sided type is for copying patterns such as handicrafts and for marking sewing. It can be marked clearly and can be removed by washing with water. The one-sided 5-color set contains 5 colors ... Read MoreDimensions (cm) 30×25
- Chacopaper Chakopa ThickA bold type chaco pen that is ideal for drawing lines such as handicrafts and sewing.Overall Length (cm) 14 Material Water-based ink, polypropylene
- Chacopaper Transfer paperUsed when transferring a design. Since it disappears with water, you can draw it as it is. You can also draw and rewrite on paper, cloth, wood, synthetic leather, plastic, glass, pottery, etc.Dimensions (cm) 44×30from S$7.49Min. 2 days
- KIYOHARA KIYOHARA hatron paperThin and durable kraft paper, which is a must-have item for making patterns. Because it is transparent, you can easily copy actual large-sized paper. Copy it on a rough surface with a pencil.Dimensions (cm) 77×108from S$4.89Min. 2 days
- Clover Mfg Iron Chaco PenA white marker suitable for black and dark cloths. The mark disappears with the heat of the iron or washing with water.Color White
- Chacopaper Super Chaco PaperIf you want to correct, correct or erase the copied lines, you can easily erase them with a cloth or brush soaked in water, or spray them, and the finish of the work will be beautiful.from S$7.89Min. 2 days
- KAWAGUCHI Chacopen 3 pcs set (with sharpener)Chaco Pen A set of 3 white, red, and blue.Act on Promoting Green Procurement Conformity Included Accessories Sharpener Color White / red / bluefrom S$8.39Min. 2 days
- Clover Mfg S rouletteWhen copying a pattern directly onto a thin cloth. Standard type with a focus on functionality. This is useful when you want to transfer a pattern on another piece of paper or mark a thin piece of cloth. While rolling the gear along the pattern, push it forward to make a mark (hole).from S$9.89Min. 2 days
- Clover Mfg S Soft RouletteThe tooth tips are round, and you can mark it without damaging the paper pattern or chacopies. Standard type with a focus on functionality. It is used when copying a pattern on fabric using Clovercha Copy (paper chaco).
- KAWAGUCHI Chalk Ace BA twin type with a thick core / thin core that is convenient for tole painting, embroidery, patchwork, etc. It can be erased with water.Color Blue